Synchrnonous enable/disable interrupts fucntion.
Synchronous enable/disable of WINC to host interrupts.
Functions | |
void | nm_bsp_interrupt_ctrl (uint8 u8Enable) |
Enable/Disable interrupts. More... | |
void nm_bsp_interrupt_ctrl | ( | uint8 | u8Enable | ) |
Enable/Disable interrupts.
Enable/Disable interrupts from the WINC.
[in] | u8Enable | '0' disable interrupts. '1' enable interrupts |
This function can be used to enable/disable the WINC to host interrupts, depending on how the driver is implemented. It is an internal driver function and shouldn't be called by the application.
[in] | u8Enable |
|