Heart Rate Sensor Application Declarations.
Copyright (c) 2017-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | ACTIVITY_BRISK_WALKING (2) |
#define | ACTIVITY_FAST_RUNNING (4) |
#define | ACTIVITY_NORMAL (0) |
Activities of user. More... | |
#define | ACTIVITY_RUNNING (3) |
#define | ACTIVITY_WALKING (1) |
#define | DEFAULT_ACTIVITY (0xFF) |
#define | END_OF_LAST_ACTIVITY (200) |
#define | ENERGY_EXP_BRISK_WALKING (20) |
#define | ENERGY_EXP_FAST_RUNNING (60) |
#define | ENERGY_EXP_NORMAL (3) |
energy expended for various activities More... | |
#define | ENERGY_EXP_RUNNING (40) |
#define | ENERGY_EXP_WALKING (10) |
#define | ENERGY_EXPENDED_FIELD_PRESENT (0x1 << 3) |
ENERGY_EXPENDED_FIELD_PRESENT represents energy expended inclusion. More... | |
#define | ENERGY_RESET (0) |
#define | HEART_RATE_MAX_BRISK_WALK (110) |
#define | HEART_RATE_MAX_FAST_RUNNING (151) |
#define | HEART_RATE_MAX_NORM (70) |
#define | HEART_RATE_MAX_RUNNING (130) |
#define | HEART_RATE_MAX_WALKING (90) |
#define | HEART_RATE_MIN_BRISK_WALK (91) |
#define | HEART_RATE_MIN_FAST_RUNNING (130) |
#define | HEART_RATE_MIN_NORM (50) |
Heart Rate maximum and minimum values for various activities. More... | |
#define | HEART_RATE_MIN_RUNNING (111) |
#define | HEART_RATE_MIN_WALKING (71) |
#define | HR_CHAR_VALUE_LEN (10) |
The maximum length of the hr measurement characteristic data. More... | |
#define | HR_VALUE_FORMAT_UINT16 (0x1 << 0) |
HR_VALUE_FORMAT_UINT16 the bit to represent hr value sent is 16 bit. More... | |
#define | NOTIFICATION_INTERVAL (1) |
Notification interval to determine the frequency of notifications. More... | |
#define | RR_INTERVAL_VALUE_PRESENT (0x1 << 4) |
RR_INTERVAL_VALUE_PRESENT represents the rr value inclusion. More... | |
#define | RR_VALUE_MAX (1000) |
RR interval maximum and minimum values for simulation of rr values. More... | |
#define | RR_VALUE_MIN (100) |
#define | SENSOR_CONTACT_FTR_NOT_SPRTD_CONTACT_DTD (0x3 << 1) |
SENSOR_CONTACT_FTR_NOT_SPRTD_NOT_CONTACT to represent the sensor contact info. More... | |
#define | SENSOR_CONTACT_FTR_NOT_SPRTD_NOT_CONTACT (0x1 << 2) |
SENSOR_CONTACT_FTR_NOT_SPRTD_NOT_CONTACT to represent the sensor contact info. More... | |
#define | START_OF_FIRST_ACTIVITY (0) |
time limit of last activity More... | |
#define | TIME_BRISK_WALK_LIMIT (120) |
#define | TIME_FAST_RUNNING_LIMIT (200) |
#define | TIME_NORMAL_LIMIT (40) |
Time counter for change of activities by user. More... | |
#define | TIME_RUNNING_LIMIT (160) |
#define | TIME_WALKING_LIMIT (80) |
Functions | |
static at_ble_status_t | app_connected_event_handler (void *params) |
connected state handler More... | |
static at_ble_status_t | app_disconnected_event_handler (void *params) |
disconnected state handler More... | |
at_ble_status_t | app_notification_cfm_handler (void *params) |
app_notification_cfm_handler called by ble manager to give the status of notification sent More... | |
#define ACTIVITY_BRISK_WALKING (2) |
#define ACTIVITY_FAST_RUNNING (4) |
#define ACTIVITY_NORMAL (0) |
Activities of user.
#define ACTIVITY_RUNNING (3) |
#define ACTIVITY_WALKING (1) |
#define DEFAULT_ACTIVITY (0xFF) |
#define END_OF_LAST_ACTIVITY (200) |
#define ENERGY_EXP_BRISK_WALKING (20) |
#define ENERGY_EXP_FAST_RUNNING (60) |
#define ENERGY_EXP_NORMAL (3) |
energy expended for various activities
#define ENERGY_EXP_RUNNING (40) |
#define ENERGY_EXP_WALKING (10) |
#define ENERGY_EXPENDED_FIELD_PRESENT (0x1 << 3) |
ENERGY_EXPENDED_FIELD_PRESENT represents energy expended inclusion.
#define ENERGY_RESET (0) |
#define HEART_RATE_MAX_BRISK_WALK (110) |
#define HEART_RATE_MAX_FAST_RUNNING (151) |
#define HEART_RATE_MAX_NORM (70) |
#define HEART_RATE_MAX_RUNNING (130) |
#define HEART_RATE_MAX_WALKING (90) |
#define HEART_RATE_MIN_BRISK_WALK (91) |
#define HEART_RATE_MIN_FAST_RUNNING (130) |
#define HEART_RATE_MIN_NORM (50) |
Heart Rate maximum and minimum values for various activities.
#define HEART_RATE_MIN_RUNNING (111) |
#define HEART_RATE_MIN_WALKING (71) |
#define HR_CHAR_VALUE_LEN (10) |
The maximum length of the hr measurement characteristic data.
#define HR_VALUE_FORMAT_UINT16 (0x1 << 0) |
HR_VALUE_FORMAT_UINT16 the bit to represent hr value sent is 16 bit.
#define NOTIFICATION_INTERVAL (1) |
Notification interval to determine the frequency of notifications.
#define RR_INTERVAL_VALUE_PRESENT (0x1 << 4) |
RR_INTERVAL_VALUE_PRESENT represents the rr value inclusion.
#define RR_VALUE_MAX (1000) |
RR interval maximum and minimum values for simulation of rr values.
#define RR_VALUE_MIN (100) |
#define SENSOR_CONTACT_FTR_NOT_SPRTD_CONTACT_DTD (0x3 << 1) |
SENSOR_CONTACT_FTR_NOT_SPRTD_NOT_CONTACT to represent the sensor contact info.
#define SENSOR_CONTACT_FTR_NOT_SPRTD_NOT_CONTACT (0x1 << 2) |
SENSOR_CONTACT_FTR_NOT_SPRTD_NOT_CONTACT to represent the sensor contact info.
#define START_OF_FIRST_ACTIVITY (0) |
time limit of last activity
#define TIME_BRISK_WALK_LIMIT (120) |
#define TIME_FAST_RUNNING_LIMIT (200) |
#define TIME_NORMAL_LIMIT (40) |
Time counter for change of activities by user.
#define TIME_RUNNING_LIMIT (160) |
#define TIME_WALKING_LIMIT (80) |
|
static |
connected state handler
[in] | status | of the application |
|
static |
disconnected state handler
[in] | status | of the application |
at_ble_status_t app_notification_cfm_handler | ( | void * | params | ) |
app_notification_cfm_handler called by ble manager to give the status of notification sent
[in] | at_ble_cmd_complete_event_t | address of the cmd completion |
app_notification_cfm_handler called by ble manager to give the status of notification sent
[in] | at_ble_cmd_complete_event_t | address of the cmd completion |
References AT_BLE_SUCCESS, DBG_LOG_DEV, notification_sent, and at_ble_cmd_complete_event_t::status.