API driver for OV7740 CMOS image sensor.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
uint32_t | ov_configure (Twi *const p_twi, const e_ov7740_format format) |
Configure the OV7740 sensor for a specified image size (pixel format). More... | |
uint32_t | ov_configure_finish (Twi *const p_twi) |
Complete the OV7740 sensor configuration. More... | |
uint32_t | ov_configure_manual (Twi *const p_twi) |
Configure the OV7740 sensor manually. More... | |
void | ov_dump_registers (Twi *const p_twi, ov_reg *p_regs) |
Dump all registers. More... | |
static uint32_t | ov_id (Twi *const p_twi) |
Read PID and VER. More... | |
uint32_t | ov_init (Twi *const p_twi) |
Initialize the OV7740 sensor. More... | |
static uint32_t | ov_manufacturer (Twi *const p_twi) |
Read Manufacturer. More... | |
void | ov_power (uint32_t ul_on_off, Pio *const p_pio, const uint32_t ul_mask) |
Turn OV7740 sensor on/off using power pin. More... | |
uint32_t | ov_read_reg (Twi *const p_twi, twi_packet_t *const p_packet) |
Read a value from a register in an OV7740 sensor device. More... | |
void | ov_reset (Pio *const p_pio, const uint32_t ul_mask) |
Reset OV7740 sensor using power pin. More... | |
uint32_t | ov_restore_manual (volatile uint32_t *p_backup_addr, uint32_t ul_size) |
Restore backup register manually. More... | |
static void | ov_retrieve_manual (Twi *const p_twi) |
Retrieve register manually. More... | |
uint32_t | ov_store_manual (Twi *const p_twi, volatile uint32_t *p_backup_addr, uint32_t ul_size) |
Store back up register manually. More... | |
static uint32_t | ov_test_write (Twi *const p_twi) |
OV7740 test write. More... | |
uint32_t | ov_write_reg (Twi *const p_twi, twi_packet_t *const p_packet) |
Write a specified value to a register of the OV7740 sensor. More... | |
uint32_t | ov_write_regs (Twi *const p_twi, const ov_reg *p_reg_list) |
Initialize a list of OV7740 registers. More... | |
Variables | |
static ov_reg | regs_manual [] |
Register array for manual operation (given by OmniVision toolkit). More... | |