Common User Interface for USB application.
Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | ui_com_close (uint8_t port) |
Called when communication port is closed. More... | |
void | ui_com_error (void) |
Called when a communication error occur. More... | |
void | ui_com_open (uint8_t port) |
Called when communication port is opened. More... | |
void | ui_com_overflow (void) |
Called when a overflow occur. More... | |
void | ui_com_rx_start (void) |
Called when a data is received on CDC. More... | |
void | ui_com_rx_stop (void) |
Called when all data pending are sent on port com. More... | |
void | ui_com_tx_start (void) |
Called when a data is received on port com. More... | |
void | ui_com_tx_stop (void) |
Called when all data pending are sent on CDC. More... | |
void | ui_init (void) |
Initializes the user interface. More... | |
void | ui_kbd_led (uint8_t value) |
Turn on or off the keyboard LEDs. More... | |
void | ui_powerdown (void) |
Enters the user interface in power down mode. More... | |
void | ui_process (uint16_t framenumber) |
This process is called each 1ms It is called only if the USB interface is enabled. More... | |
void | ui_wakeup (void) |
Exits the user interface of power down mode. More... | |
void | ui_wakeup_disable (void) |
Disables the asynchronous interrupts of the user interface. More... | |
void | ui_wakeup_enable (void) |
Enables the asynchronous interrupts of the user interface. More... | |
Callback to show the MSC read and write access | |
void | ui_start_read (void) |
void | ui_stop_read (void) |
void | ui_start_write (void) |
void | ui_stop_write (void) |
void ui_com_close | ( | uint8_t | port | ) |
Called when communication port is closed.
void ui_com_error | ( | void | ) |
Called when a communication error occur.
void ui_com_open | ( | uint8_t | port | ) |
Called when communication port is opened.
void ui_com_overflow | ( | void | ) |
Called when a overflow occur.
void ui_com_rx_start | ( | void | ) |
Called when a data is received on CDC.
void ui_com_rx_stop | ( | void | ) |
Called when all data pending are sent on port com.
void ui_com_tx_start | ( | void | ) |
Called when a data is received on port com.
void ui_com_tx_stop | ( | void | ) |
Called when all data pending are sent on CDC.
void ui_init | ( | void | ) |
Initializes the user interface.
Called at firmware startup.
Initializes the user interface.
void ui_kbd_led | ( | uint8_t | value | ) |
Turn on or off the keyboard LEDs.
void ui_powerdown | ( | void | ) |
Enters the user interface in power down mode.
Called before enter in powerdown mode.
Enters the user interface in power down mode.
Sets the user interface in power down mode.
void ui_process | ( | uint16_t | framenumber | ) |
This process is called each 1ms It is called only if the USB interface is enabled.
framenumber | Current frame number |
This process is called each 1ms It is called only if the USB interface is enabled.
This function processes user touch events and updates the display.
The first registered touch is used to control the cursor. Its presence is indicated with a red frame around the display. When the cursor touch moves, its movement is visualized with a trace on the display.
The second registered touch is used to control mouse buttons, and is indicated with an inner frame of which the color depends on which side the touch is for: blue for left and green for right button click. The frame is shown until the touch is released. To detect which side click it is, the position relative to the cursor touch is used, i.e., a touch to the left of the first touch will cause a left mouse click.
framenumber | Current USB frame number |
void ui_start_read | ( | void | ) |
void ui_start_write | ( | void | ) |
void ui_stop_read | ( | void | ) |
void ui_stop_write | ( | void | ) |
void ui_wakeup | ( | void | ) |
Exits the user interface of power down mode.
Called when CPU exit of powerdown mode.
Exits the user interface of power down mode.
void ui_wakeup_disable | ( | void | ) |
Disables the asynchronous interrupts of the user interface.
Disables the asynchronous interrupts of the user interface.
void ui_wakeup_enable | ( | void | ) |
Enables the asynchronous interrupts of the user interface.
Enables the asynchronous interrupts of the user interface.