Microchip® Advanced Software Framework

at_ble_htpt_cfg_indntf_ind_t Struct Reference

Parameters of the AT_BLE_HTPT_CFG_INDNTF_IND message.

#include <at_ble_api.h>

Data Fields

uint8_t conhdl
 Connection handle. More...
 
uint8_t ntf_ind_cfg
 Stop/notify/indicate value to configure into the peer characteristic. More...
 

uint8_t at_ble_htpt_cfg_indntf_ind_t::conhdl

Connection handle.

uint8_t at_ble_htpt_cfg_indntf_ind_t::ntf_ind_cfg

Stop/notify/indicate value to configure into the peer characteristic.

Referenced by app_htpt_cfg_indntf_ind_handler().