Microchip® Advanced Software Framework

at_ble_lecb_add_credit_ind_t Struct Reference

Parameters of the AT_BLE_LECB_ADD_CREDIT_IND message.

#include <at_ble_api.h>

Data Fields

uint16_t dest_credit
 Destination Credit for the LE Credit Based Connection. More...
 
uint16_t le_psm
 LE Protocol/Service Multiplexer. More...
 
uint16_t src_credit
 Source Credit for the LE Credit Based Connection. More...
 

uint16_t at_ble_lecb_add_credit_ind_t::dest_credit

Destination Credit for the LE Credit Based Connection.

Referenced by l2cap_credit_indication().

uint16_t at_ble_lecb_add_credit_ind_t::le_psm

LE Protocol/Service Multiplexer.

uint16_t at_ble_lecb_add_credit_ind_t::src_credit

Source Credit for the LE Credit Based Connection.