Microchip® Advanced Software Framework

at_ble_user_desc_t Struct Reference

#include <at_ble_api.h>

Data Fields

at_ble_handle_t handle
 user descriptor handle More...
 
uint16_t len
 the user friendly description length, this value will be stored in the relevant descriptor, if no user description is desired set to 0 More...
 
at_ble_attr_permissions_t permissions
 user descriptor permissions More...
 
uint8_t * user_description
 a user friendly description, this value will be stored in the relevant descriptor, if no user description is desired set to NULL More...
 

at_ble_handle_t at_ble_user_desc_t::handle

user descriptor handle

Referenced by hid_serv_init().

uint16_t at_ble_user_desc_t::len

the user friendly description length, this value will be stored in the relevant descriptor, if no user description is desired set to 0

Referenced by hid_serv_init().

at_ble_attr_permissions_t at_ble_user_desc_t::permissions

user descriptor permissions

Referenced by hid_serv_init().

uint8_t* at_ble_user_desc_t::user_description

a user friendly description, this value will be stored in the relevant descriptor, if no user description is desired set to NULL

Referenced by hid_serv_init().