#include <at_cmd_Handler.h>
Data Fields | |
uint8 | u8Disaply_hint |
uint8 | u8Echo_status |
uint8 | u8Restart_app |
uint8 tstr_app_config::u8Disaply_hint |
If this variable has been set, this means if something wrong happened This will display a hint about the command
Referenced by atCmd_AppConfig_Handler(), init_m2m_app(), and start_m2m_app().
uint8 tstr_app_config::u8Echo_status |
Must be disabled if automated transfer is used
Referenced by atCmd_AppConfig_Handler(), init_m2m_app(), and start_m2m_app().
uint8 tstr_app_config::u8Restart_app |
Has the value of the application to restart or not when this variable will auto reset after execution
Referenced by atCmd_AppConfig_Handler().