M2M association information of the connected station in the AP mode.
#include <m2m_types.h>
Data Fields | |
uint8 | __PAD__ [PAD_SZ(1+(sizeof(tstrM2MAssocEntryInfo)*8))] |
tstrM2MAssocEntryInfo | astrM2MAssocEntryInfo [8] |
uint8 | u8NoConnSta |
uint8 tstrM2MAPAssocInfo::__PAD__[PAD_SZ(1+(sizeof(tstrM2MAssocEntryInfo)*8))] |
Padding bytes for forcing 4-byte alignment
tstrM2MAssocEntryInfo tstrM2MAPAssocInfo::astrM2MAssocEntryInfo[8] |
array of the associated stations
Referenced by http_request().
uint8 tstrM2MAPAssocInfo::u8NoConnSta |
No of connected stations
Referenced by http_request().