Microchip® Advanced Software Framework

tstrM2mAntDivParams Struct Reference

#include <m2m_types.h>

Data Fields

uint8 antenna1
 
uint8 antenna2
 
uint8 gpio_mode
 
uint8 mode
 

uint8 tstrM2mAntDivParams::antenna1

Antenna1 WILC GPIO number selection

Referenced by m2m_wifi_set_antenna_mode().

uint8 tstrM2mAntDivParams::antenna2

Antenna2 WILC GPIO number selection

Referenced by m2m_wifi_set_antenna_mode().

uint8 tstrM2mAntDivParams::gpio_mode

Antenna GPIO Switch mode - Single=1, Dual=2 or None=0

Referenced by m2m_wifi_set_antenna_mode().

uint8 tstrM2mAntDivParams::mode

Antenna Selection mode

Referenced by m2m_wifi_set_antenna_mode().