Wi-Fi Connection State.
This struct contains the Wi-Fi connection state.
#include <m2m_types.h>
Data Fields | |
uint8 | __PAD16__ [2] |
uint8 | __PAD__ [PAD_SZ(4+6)] |
uint8 | u8Ch |
uint8 | u8CurrState |
uint8 | u8ErrCode |
uint8 | u8IfcId |
uint8 | u8MAcAddr [6] |
uint8 tstrM2mWifiStateChanged::__PAD16__ |
Padding bytes for forcing 4-byte alignment
< Mac Address of the STA/AP involved in state changePadding bytes for forcing 4-byte alignment
uint8 tstrM2mWifiStateChanged::u8Ch |
< Interface on which state was changed
uint8 tstrM2mWifiStateChanged::u8CurrState |
Current Wi-Fi connection state
Referenced by app_wifi_handle_event(), iperf_wifi_cb(), m2m_wifi_cb(), prov_wifi_cb(), and wifi_cb().
uint8 tstrM2mWifiStateChanged::u8ErrCode |
Error type as in tenuM2mConnChangedErrcode
Error type review tenuM2mConnChangedErrcode
Error type
Referenced by wifi_cb().