Wi-Fi Scan Result.
This struct contains the information corresponding to an AP in the scan result list identified by its order (index) in the list.
Information corresponding to an AP in the Scan Result list identified by its order (index) in the list.
#include <m2m_types.h>
Data Fields | |
uint8 | __PAD__ [PAD_SZ(4+6+M2M_MAX_SSID_LEN+M2M_DEVICE_NAME_MAX)] |
uint8 | _PAD8_ |
uint8 | au8BSSID [6] |
uint8 | au8DeviceName [M2M_DEVICE_NAME_MAX] |
uint8 | au8SSID [M2M_MAX_SSID_LEN] |
sint8 | s8rssi |
uint8 | u8AuthType |
uint8 | u8ch |
uint8 | u8index |
uint8 tstrM2mWifiscanResult::__PAD__[PAD_SZ(4+6+M2M_MAX_SSID_LEN+M2M_DEVICE_NAME_MAX)] |
< P2P Device NamePadding bytes for forcing 4-byte alignment
uint8 tstrM2mWifiscanResult::_PAD8_ |
Padding bytes for forcing 4-byte alignment
uint8 tstrM2mWifiscanResult::au8DeviceName[M2M_DEVICE_NAME_MAX] |
uint8 tstrM2mWifiscanResult::au8SSID |
sint8 tstrM2mWifiscanResult::s8rssi |
AP signal strength.
Referenced by ble_prov_scan_result(), send_scan_result(), and wifi_cb().
uint8 tstrM2mWifiscanResult::u8AuthType |
AP authentication type.
Referenced by ble_prov_scan_result(), send_scan_result(), and wifi_cb().