Microchip® Advanced Software Framework

tstrOtaHostFileGetStatusResp Struct Reference

Host File OTA Information.

#include <m2m_types.h>

Data Fields

uint8 __PAD16__ [2]
 
uint32 u32OtaFileSize
 
uint8 u8CFHandler
 
uint8 u8OtaFileGetStatus
 

uint8 tstrOtaHostFileGetStatusResp::__PAD16__[2]

Padding byte for forcing 4-byte alignment

uint32 tstrOtaHostFileGetStatusResp::u32OtaFileSize

Reports the size of the downloaded file. Valid if u8OtaFileGetStatus=OTA_STATUS_SUCCESS.

Referenced by m2m_ota_cb().

uint8 tstrOtaHostFileGetStatusResp::u8CFHandler

The file handler stored in the WINC for a valid file. Valid if u8OtaFileGetStatus=OTA_STATUS_SUCCESS.

Referenced by m2m_ota_cb().

uint8 tstrOtaHostFileGetStatusResp::u8OtaFileGetStatus

The status of the File Get operation. See tenuOtaUpdateStatus.

Referenced by m2m_ota_cb().