Microchip® Advanced Software Framework

usb_phdc_classfnct_desc_t Struct Reference

PHDC Class Function Descriptor.

#include <usb_protocol_phdc.h>

Data Fields

uint8_t bDescriptorType
 PHDC descriptor type. More...
 
uint8_t bLength
 Size of this descriptor in bytes. More...
 
uint8_t bmCapability
 Features available in the interface. More...
 
uint8_t bPHDCDataCode
 Data/Messaging format code. More...
 

uint8_t usb_phdc_classfnct_desc_t::bDescriptorType

PHDC descriptor type.

uint8_t usb_phdc_classfnct_desc_t::bLength

Size of this descriptor in bytes.

uint8_t usb_phdc_classfnct_desc_t::bmCapability

Features available in the interface.

uint8_t usb_phdc_classfnct_desc_t::bPHDCDataCode

Data/Messaging format code.