This is the check box control struct.
It contains references to the windows composing the check box, as well as non-window information required.
Data Fields | |
char * | caption |
Copy of caption string. More... | |
win_command_t | command |
Command to send. More... | |
struct win_window * | container |
Container, ultimate widget parent. More... | |
bool | selected |
True if selected. More... | |
enum wtk_check_box_state | state |
Current state. More... | |
char* wtk_check_box::caption |
Copy of caption string.
Referenced by wtk_check_box_create(), and wtk_check_box_handler().
win_command_t wtk_check_box::command |
Command to send.
Must be non-zero to be enabled.
Referenced by wtk_check_box_create(), wtk_check_box_get_command(), and wtk_check_box_handler().
struct win_window* wtk_check_box::container |
Container, ultimate widget parent.
Referenced by wtk_check_box_as_child(), wtk_check_box_create(), wtk_check_box_handler(), wtk_check_box_set(), and wtk_check_box_toggle().
bool wtk_check_box::selected |
True if selected.
Referenced by wtk_check_box_create(), wtk_check_box_handler(), wtk_check_box_is_selected(), wtk_check_box_set(), and wtk_check_box_toggle().
enum wtk_check_box_state wtk_check_box::state |
Current state.
Referenced by wtk_check_box_create(), and wtk_check_box_handler().