HTTP Netconn Example.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
#include <FreeRTOS.h>
#include <StackMacros.h>
#include <croutine.h>
#include <list.h>
#include <mpu_wrappers.h>
#include <portable.h>
#include <projdefs.h>
#include <queue.h>
#include <semphr.h>
#include <task.h>
#include <timers.h>
#include <pmc.h>
#include <sysclk.h>
Macros | |
#define | mainGFX_TASK_PRIORITY (tskIDLE_PRIORITY + 1) |
The priorities at which various tasks will get created. More... | |
#define | mainGFX_TASK_STACK_SIZE (256) |
The stack sizes allocated to the DSP stack: (256 * 4) = 1024 bytes. More... | |
#define | mainHTTP_TASK_PRIORITY (tskIDLE_PRIORITY + 2) |
The priorities at which various tasks will get created. More... | |
#define | mainHTTP_TASK_STACK_SIZE (256) |
The stack sizes allocated to the DSP stack: (256 * 4) = 1024 bytes. More... | |
#define | WAIT_FOR_TOUCH_EVENT {while (app_hold) vTaskDelay(instructions_delay);} |
Wait for user to touch screen. More... | |
Functions | |
void | create_gfx_task (uint16_t stack_depth_words, unsigned portBASE_TYPE task_priority) |
Create the GFX task. More... | |
void | create_http_task (uint16_t stack_depth_words, unsigned portBASE_TYPE task_priority) |
Create the HTTP task. More... | |
Variables | |
uint32_t | app_hold |
Used to block the application on instruction screen. More... | |
const portTickType | instructions_delay |
Small delay to hold tasks, during instruction screen. More... | |
#define mainGFX_TASK_PRIORITY (tskIDLE_PRIORITY + 1) |
The priorities at which various tasks will get created.
Referenced by main().
#define mainGFX_TASK_STACK_SIZE (256) |
The stack sizes allocated to the DSP stack: (256 * 4) = 1024 bytes.
Referenced by main().
#define mainHTTP_TASK_PRIORITY (tskIDLE_PRIORITY + 2) |
The priorities at which various tasks will get created.
Referenced by http_task(), and main().
#define mainHTTP_TASK_STACK_SIZE (256) |
The stack sizes allocated to the DSP stack: (256 * 4) = 1024 bytes.
Referenced by http_task(), and main().
#define WAIT_FOR_TOUCH_EVENT {while (app_hold) vTaskDelay(instructions_delay);} |
Wait for user to touch screen.
Referenced by http_task().
void create_gfx_task | ( | uint16_t | stack_depth_words, |
unsigned portBASE_TYPE | task_priority | ||
) |
Create the GFX task.
stack_depth_words | Task stack size in 32 bits word. |
task_priority | Task priority. |
References gfx_init(), gfx_task(), NULL, and xTaskCreate.
Referenced by main().
void create_http_task | ( | uint16_t | stack_depth_words, |
unsigned portBASE_TYPE | task_priority | ||
) |
Create the HTTP task.
stack_depth_words | Task stack size in 32 bits word. |
task_priority | Task priority. |
References http_task(), NULL, and xTaskCreate.
Referenced by main().
uint32_t app_hold |
Used to block the application on instruction screen.
Referenced by gfx_task().
const portTickType instructions_delay |
Small delay to hold tasks, during instruction screen.