FreeRTOS configuration.
Copyright (c) 2012-2018 Microchip Technology Inc. and its subsidiaries.
Macros | |
#define | TASK_LED_STACK_PRIORITY (tskIDLE_PRIORITY) |
#define | TASK_LED_STACK_SIZE (1024/sizeof(portSTACK_TYPE)) |
#define | TASK_MONITOR_STACK_PRIORITY (tskIDLE_PRIORITY) |
#define | TASK_MONITOR_STACK_SIZE (2048/sizeof(portSTACK_TYPE)) |
Functions | |
static void | configure_console (void) |
Configure the console UART. More... | |
int | main (void) |
FreeRTOS Real Time Kernel example entry point. More... | |
static void | task_led (void *pvParameters) |
This task, when activated, make LED blink at a fixed rate. More... | |
static void | task_monitor (void *pvParameters) |
This task, when activated, send every ten seconds on debug UART the whole report of free heap and total tasks status. More... | |
void | vApplicationIdleHook (void) |
This function is called by FreeRTOS idle task. More... | |
void | vApplicationMallocFailedHook (void) |
void | vApplicationStackOverflowHook (xTaskHandle *pxTask, signed char *pcTaskName) |
Called if stack overflow during execution. More... | |
void | vApplicationTickHook (void) |
This function is called by FreeRTOS each tick. More... | |
void | xPortSysTickHandler (void) |
#define TASK_LED_STACK_PRIORITY (tskIDLE_PRIORITY) |
Referenced by main().
#define TASK_LED_STACK_SIZE (1024/sizeof(portSTACK_TYPE)) |
Referenced by main().
#define TASK_MONITOR_STACK_PRIORITY (tskIDLE_PRIORITY) |
Referenced by main().
#define TASK_MONITOR_STACK_SIZE (2048/sizeof(portSTACK_TYPE)) |
Referenced by main().
|
static |
Configure the console UART.
References uart_rs232_options::baudrate, CONF_UART, CONF_UART_BAUDRATE, CONF_UART_CHAR_LENGTH, CONF_UART_PARITY, CONF_UART_STOP_BITS, NULL, and stdio_serial_init().
Referenced by main().
int main | ( | void | ) |
FreeRTOS Real Time Kernel example entry point.
References board_init(), BOARD_NAME, configure_console(), NULL, pdPASS, sysclk_init(), task_led(), TASK_LED_STACK_PRIORITY, TASK_LED_STACK_SIZE, task_monitor(), TASK_MONITOR_STACK_PRIORITY, TASK_MONITOR_STACK_SIZE, vTaskStartScheduler(), and xTaskCreate.
|
static |
This task, when activated, make LED blink at a fixed rate.
References UNUSED, and vTaskDelay().
Referenced by main().
|
static |
This task, when activated, send every ten seconds on debug UART the whole report of free heap and total tasks status.
References UNUSED, uxTaskGetNumberOfTasks(), vTaskDelay(), and vTaskList().
Referenced by main().
void vApplicationIdleHook | ( | void | ) |
This function is called by FreeRTOS idle task.
vApplicationIdleHook() will only be called if configUSE_IDLE_HOOK is set to 1 in FreeRTOSConfig.h. It will be called on each iteration of the idle task. It is essential that code added to this hook function never attempts to block in any way (for example, call xQueueReceive() with a block time specified, or call vTaskDelay()). If the application makes use of the vTaskDelete() API function (as this demo application does) then it is also important that vApplicationIdleHook() is permitted to return to its calling function, because it is the responsibility of the idle task to clean up memory allocated by the kernel to any task that has since been deleted.
Referenced by portTASK_FUNCTION().
void vApplicationMallocFailedHook | ( | void | ) |
vApplicationMallocFailedHook() will only be called if configUSE_MALLOC_FAILED_HOOK is set to 1 in FreeRTOSConfig.h. It is a hook function that will get called if a call to pvPortMalloc() fails. pvPortMalloc() is called internally by the kernel whenever a task, queue, timer or semaphore is created. It is also called by various parts of the demo application. If heap_1.c or heap_2.c are used, then the size of the heap available to pvPortMalloc() is defined by configTOTAL_HEAP_SIZE in FreeRTOSConfig.h, and the xPortGetFreeHeapSize() API function can be used to query the size of free heap space that remains (although it does not provide information on how the remaining heap might be fragmented).
Referenced by pvPortMalloc().
void vApplicationStackOverflowHook | ( | xTaskHandle * | pxTask, |
signed char * | pcTaskName | ||
) |
Called if stack overflow during execution.
void vApplicationTickHook | ( | void | ) |
This function is called by FreeRTOS each tick.
This function will be called by each tick interrupt if configUSE_TICK_HOOK is set to 1 in FreeRTOSConfig.h. User code can be added here, but the tick hook is called from an interrupt context, so code must not attempt to block, and only the interrupt safe FreeRTOS API functions can be used (those that end in FromISR()).
Referenced by vTaskIncrementTick(), and xTaskIncrementTick().
void xPortSysTickHandler | ( | void | ) |