SW Timer component for the IoT(Internet of things) service.
Copyright (c) 2018 Microchip Technology Inc. and its subsidiaries.
#include <asf.h>
#include <stdint.h>
#include "conf_sw_timer.h"
Data Structures | |
struct | sw_timer_config |
SW timer configuration structure. More... | |
struct | sw_timer_handle |
SW timer handler structure. More... | |
struct | sw_timer_module |
SW timer module structure. More... | |
Typedefs | |
typedef void(* | sw_timer_callback_t )(struct sw_timer_module *const module, int timer_id, void *context, int period) |
Callback Function type of time out event in the timer. More... | |
Functions | |
void | sw_timer_disable (struct sw_timer_module *const module_inst) |
Stop the timer. More... | |
void | sw_timer_disable_callback (struct sw_timer_module *const module_inst, int timer_id) |
Disable callback. More... | |
void | sw_timer_enable (struct sw_timer_module *const module_inst) |
Start the timer. More... | |
void | sw_timer_enable_callback (struct sw_timer_module *const module_inst, int timer_id, uint32_t delay) |
Enables callback. More... | |
void | sw_timer_get_config_defaults (struct sw_timer_config *const config) |
Get default configuration of SW timer. More... | |
void | sw_timer_init (struct sw_timer_module *const module_inst, struct sw_timer_config *const config) |
Initialize the SW timer module. More... | |
int | sw_timer_register_callback (struct sw_timer_module *const module_inst, sw_timer_callback_t callback, void *context, uint32_t period) |
Register callback. More... | |
void | sw_timer_task (struct sw_timer_module *const module_inst) |
Checks the time out of each timer handlers. More... | |
void | sw_timer_unregister_callback (struct sw_timer_module *const module_inst, int timer_id) |
Unregister callback. More... | |
typedef void(* sw_timer_callback_t)(struct sw_timer_module *const module, int timer_id, void *context, int period) |
Callback Function type of time out event in the timer.
[in] | timer_id | ID of timer. |
[in] | context | Private data of timer. |
[in] | context | Period of timer handle. |
void sw_timer_disable | ( | struct sw_timer_module *const | module_inst | ) |
Stop the timer.
[in] | module_inst | Pointer of timer. |
void sw_timer_disable_callback | ( | struct sw_timer_module *const | module_inst, |
int | timer_id | ||
) |
Disable callback.
Disable the callback function registered by the sw_timer_register_callback.
[in] | module_inst | Pointer to USART software instance struct |
[in] | timer_id | Timer ID . |
void sw_timer_enable | ( | struct sw_timer_module *const | module_inst | ) |
Start the timer.
[in] | module_inst | Pointer of timer. |
void sw_timer_enable_callback | ( | struct sw_timer_module *const | module_inst, |
int | timer_id, | ||
uint32_t | delay | ||
) |
Enables callback.
Enables the callback function registered by the sw_timer_register_callback.
[in] | module_inst | Pointer to USART software instance struct |
[in] | timer_id | Timer ID . |
[in] | delay | Initialization value of timer. |
void sw_timer_get_config_defaults | ( | struct sw_timer_config *const | config | ) |
Get default configuration of SW timer.
[in] | config | Pointer of configuration structure which will be used in the timer. |
Get default configuration of SW timer.
This function performs to the increasing the tick count.
[in] | module | Instance of the TCC. |
void sw_timer_init | ( | struct sw_timer_module *const | module_inst, |
struct sw_timer_config *const | config | ||
) |
Initialize the SW timer module.
[in] | module_inst | Pointer of timer. |
[in] | config | Pointer of configuration structure which will be used in the timer. |
int sw_timer_register_callback | ( | struct sw_timer_module *const | module_inst, |
sw_timer_callback_t | callback, | ||
void * | context, | ||
uint32_t | period | ||
) |
Register callback.
[in] | module_inst | Pointer of timer. |
[in] | callback | Callback entry of time out. |
[in] | context | Private data of timer. |
[in] | period | Period of timer. |
void sw_timer_task | ( | struct sw_timer_module *const | module_inst | ) |
Checks the time out of each timer handlers.
This function must be called continuously for the checking the expiration of the timer handle.
[in] | module_inst | Pointer to USART software instance struct |
void sw_timer_unregister_callback | ( | struct sw_timer_module *const | module_inst, |
int | timer_id | ||
) |
Unregister callback.
[in] | module_inst | Pointer of timer. |
[in] | timer_id | Timer ID . |