WINC Crypto Application Interface.
Copyright (c) 2016-2018 Microchip Technology Inc. and its subsidiaries.
#include "common/include/nm_common.h"
#include "driver/include/m2m_types.h"
#include "driver/source/m2m_hif.h"
Data Structures | |
struct | sha256ctxt |
Macros | |
#define | M2M_MAX_RSA_LEN (256) |
#define | M2M_SHA256_DIGEST_LEN 32 |
#define | M2M_SHA256_MAX_DATA (M2M_BUFFER_MAX_SIZE - M2M_SHA256_CONTEXT_BUFF_LEN - M2M_HIF_HDR_OFFSET) |
Typedefs | |
typedef void(* | tpfAppCryproCb )(uint8 u8MsgType, void *pvResp, void *pvMsg) |
Crypto Callback function receiving the crypto related messages. More... | |
typedef struct sha256ctxt | tstrM2mSha256Ctxt |
Enumerations | |
enum | tenuRsaSignStatus { M2M_RSA_SIGN_OK, M2M_RSA_SIGN_FAIL, M2M_RSA_SIGN_OK, M2M_RSA_SIGN_FAIL } |
RSA Signature status: pass or fail. More... | |
Functions | |
sint8 | m2m_crypto_init (tpfAppCryproCb pfAppCryproCb) |
sint8 | m2m_crypto_rsa_sign_gen (uint8 *pu8N, uint16 u16NSize, uint8 *pu8d, uint16 u16dSize, uint8 *pu8SignedMsgHash, uint16 u16HashLength, uint8 *pu8RsaSignature) |
sint8 | m2m_crypto_rsa_sign_verify (uint8 *pu8N, uint16 u16NSize, uint8 *pu8E, uint16 u16ESize, uint8 *pu8SignedMsgHash, uint16 u16HashLength, uint8 *pu8RsaSignature) |
sint8 | m2m_crypto_sha256_hash_finish (tstrM2mSha256Ctxt *psha256Ctxt, uint8 *pu8Sha256Digest) |
sint8 | m2m_crypto_sha256_hash_init (tstrM2mSha256Ctxt *psha256Ctxt) |
sint8 | m2m_crypto_sha256_hash_update (tstrM2mSha256Ctxt *psha256Ctxt, uint8 *pu8Data, uint16 u16DataLength) |
#define M2M_MAX_RSA_LEN (256) |
#define M2M_SHA256_DIGEST_LEN 32 |
#define M2M_SHA256_MAX_DATA (M2M_BUFFER_MAX_SIZE - M2M_SHA256_CONTEXT_BUFF_LEN - M2M_HIF_HDR_OFFSET) |
tpfAppCryproCb |
Crypto Callback function receiving the crypto related messages.
[in] | u8MsgType | Crypto command about which the notification is received. |
[in] | pvResp | A pointer to the result associated with the notification. |
[in] | pvMsg | A pointer to a buffer containing the notification parameters (if any). It should be Casted to the correct data type corresponding to the notification type. |
typedef struct sha256ctxt tstrM2mSha256Ctxt |
enum tenuRsaSignStatus |
RSA Signature status: pass or fail.
Enumerator | |
---|---|
M2M_RSA_SIGN_OK | |
M2M_RSA_SIGN_FAIL | |
M2M_RSA_SIGN_OK | |
M2M_RSA_SIGN_FAIL |
sint8 m2m_crypto_init | ( | tpfAppCryproCb | pfAppCryproCb | ) |
sint8 m2m_crypto_rsa_sign_gen | ( | uint8 * | pu8N, |
uint16 | u16NSize, | ||
uint8 * | pu8d, | ||
uint16 | u16dSize, | ||
uint8 * | pu8SignedMsgHash, | ||
uint16 | u16HashLength, | ||
uint8 * | pu8RsaSignature | ||
) |
sint8 m2m_crypto_rsa_sign_verify | ( | uint8 * | pu8N, |
uint16 | u16NSize, | ||
uint8 * | pu8E, | ||
uint16 | u16ESize, | ||
uint8 * | pu8SignedMsgHash, | ||
uint16 | u16HashLength, | ||
uint8 * | pu8RsaSignature | ||
) |
sint8 m2m_crypto_sha256_hash_finish | ( | tstrM2mSha256Ctxt * | psha256Ctxt, |
uint8 * | pu8Sha256Digest | ||
) |
sint8 m2m_crypto_sha256_hash_init | ( | tstrM2mSha256Ctxt * | psha256Ctxt | ) |
sint8 m2m_crypto_sha256_hash_update | ( | tstrM2mSha256Ctxt * | psha256Ctxt, |
uint8 * | pu8Data, | ||
uint16 | u16DataLength | ||
) |