This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of internal software and hardware interrupts/exceptions.
The following peripheral is used by this module:
- NVIC (Nested Vector Interrupt Controller)
The following devices can use this module:
- Atmel | SMART SAM D20/D21
- Atmel | SMART SAM R21
- Atmel | SMART SAM D09/D10/D11
- Atmel | SMART SAM L21/L22
- Atmel | SMART SAM DA1
- Atmel | SMART SAM C20/C21
- Atmel | SMART SAM HA1
- Atmel | SMART SAM R30
- Atmel | SMART SAM R34
- Atmel | SMART SAM R35
The outline of this documentation is as follows:
Prerequisites
There are no prerequisites for this module.
Module Overview
The ARM® Cortex® M0+ core contains an interrupt and exception vector table, which can be used to configure the device's interrupt handlers; individual interrupts and exceptions can be enabled and disabled, as well as configured with a variable priority.
This driver provides a set of wrappers around the core interrupt functions, to expose a simple API for the management of global and individual interrupts within the device.
Critical Sections
In some applications it is important to ensure that no interrupts may be executed by the system whilst a critical portion of code is being run; for example, a buffer may be copied from one context to another - during which interrupts must be disabled to avoid corruption of the source buffer contents until the copy has completed. This driver provides a basic API to enter and exit nested critical sections, so that global interrupts can be kept disabled for as long as necessary to complete a critical application code section.
Software Interrupts
For some applications, it may be desirable to raise a module or core interrupt via software. For this reason, a set of APIs to set an interrupt or exception as pending are provided to the user application.
Special Considerations
Interrupts from peripherals in the SAM devices are on a per-module basis; an interrupt raised from any source within a module will cause a single, module-common handler to execute. It is the user application or driver's responsibility to de-multiplex the module-common interrupt to determine the exact interrupt cause.
Extra Information
For extra information, see Extra Information for SYSTEM INTERRUPT Driver. This includes:
Examples
For a list of examples related to this driver, see Examples for SYSTEM INTERRUPT Driver.
API Overview
|
enum | system_interrupt_priority_level {
SYSTEM_INTERRUPT_PRIORITY_LEVEL_0 = 0,
SYSTEM_INTERRUPT_PRIORITY_LEVEL_1 = 1,
SYSTEM_INTERRUPT_PRIORITY_LEVEL_2 = 2,
SYSTEM_INTERRUPT_PRIORITY_LEVEL_3 = 3
} |
| Table of possible system interrupt/exception vector priorities. More...
|
|
enum | system_interrupt_vector_samc21 {
SYSTEM_INTERRUPT_NON_MASKABLE = NonMaskableInt_IRQn,
SYSTEM_INTERRUPT_HARD_FAULT = HardFault_IRQn,
SYSTEM_INTERRUPT_SV_CALL = SVCall_IRQn,
SYSTEM_INTERRUPT_PENDING_SV = PendSV_IRQn,
SYSTEM_INTERRUPT_SYSTICK = SysTick_IRQn,
SYSTEM_INTERRUPT_MODULE_SYSTEM = SYSTEM_IRQn,
SYSTEM_INTERRUPT_MODULE_WDT = WDT_IRQn,
SYSTEM_INTERRUPT_MODULE_RTC = RTC_IRQn,
SYSTEM_INTERRUPT_MODULE_EIC = EIC_IRQn,
SYSTEM_INTERRUPT_MODULE_FREQM = FREQM_IRQn,
SYSTEM_INTERRUPT_MODULE_NVMCTRL = NVMCTRL_IRQn,
SYSTEM_INTERRUPT_MODULE_DMA = DMAC_IRQn,
SYSTEM_INTERRUPT_MODULE_EVSYS = EVSYS_IRQn,
SYSTEM_INTERRUPT_MODULE_SERCOMn = SERCOMn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCCn = TCCn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCn = TCn_IRQn
} |
| Table of possible system interrupt/exception vector numbers. More...
|
|
enum | system_interrupt_vector_samd09 {
SYSTEM_INTERRUPT_NON_MASKABLE = NonMaskableInt_IRQn,
SYSTEM_INTERRUPT_HARD_FAULT = HardFault_IRQn,
SYSTEM_INTERRUPT_SV_CALL = SVCall_IRQn,
SYSTEM_INTERRUPT_PENDING_SV = PendSV_IRQn,
SYSTEM_INTERRUPT_SYSTICK = SysTick_IRQn,
SYSTEM_INTERRUPT_MODULE_PM = PM_IRQn,
SYSTEM_INTERRUPT_MODULE_SYSCTRL = SYSCTRL_IRQn,
SYSTEM_INTERRUPT_MODULE_WDT = WDT_IRQn,
SYSTEM_INTERRUPT_MODULE_RTC = RTC_IRQn,
SYSTEM_INTERRUPT_MODULE_EIC = EIC_IRQn,
SYSTEM_INTERRUPT_MODULE_NVMCTRL = NVMCTRL_IRQn,
SYSTEM_INTERRUPT_MODULE_DMA = DMAC_IRQn,
SYSTEM_INTERRUPT_MODULE_EVSYS = EVSYS_IRQn,
SYSTEM_INTERRUPT_MODULE_SERCOMn = SERCOMn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCn = TCn_IRQn,
SYSTEM_INTERRUPT_MODULE_ADC = ADC_IRQn
} |
| Table of possible system interrupt/exception vector numbers. More...
|
|
enum | system_interrupt_vector_samd1x {
SYSTEM_INTERRUPT_NON_MASKABLE = NonMaskableInt_IRQn,
SYSTEM_INTERRUPT_HARD_FAULT = HardFault_IRQn,
SYSTEM_INTERRUPT_SV_CALL = SVCall_IRQn,
SYSTEM_INTERRUPT_PENDING_SV = PendSV_IRQn,
SYSTEM_INTERRUPT_SYSTICK = SysTick_IRQn,
SYSTEM_INTERRUPT_MODULE_PM = PM_IRQn,
SYSTEM_INTERRUPT_MODULE_SYSCTRL = SYSCTRL_IRQn,
SYSTEM_INTERRUPT_MODULE_WDT = WDT_IRQn,
SYSTEM_INTERRUPT_MODULE_RTC = RTC_IRQn,
SYSTEM_INTERRUPT_MODULE_EIC = EIC_IRQn,
SYSTEM_INTERRUPT_MODULE_NVMCTRL = NVMCTRL_IRQn,
SYSTEM_INTERRUPT_MODULE_DMA = DMAC_IRQn,
SYSTEM_INTERRUPT_MODULE_EVSYS = EVSYS_IRQn,
SYSTEM_INTERRUPT_MODULE_SERCOMn = SERCOMn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCCn = TCCn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCn = TCn_IRQn,
SYSTEM_INTERRUPT_MODULE_AC = AC_IRQn,
SYSTEM_INTERRUPT_MODULE_ADC = ADC_IRQn,
SYSTEM_INTERRUPT_MODULE_DAC = DAC_IRQn,
SYSTEM_INTERRUPT_MODULE_PTC = PTC_IRQn
} |
| Table of possible system interrupt/exception vector numbers. More...
|
|
enum | system_interrupt_vector_samd20 {
SYSTEM_INTERRUPT_NON_MASKABLE = NonMaskableInt_IRQn,
SYSTEM_INTERRUPT_HARD_FAULT = HardFault_IRQn,
SYSTEM_INTERRUPT_SV_CALL = SVCall_IRQn,
SYSTEM_INTERRUPT_PENDING_SV = PendSV_IRQn,
SYSTEM_INTERRUPT_SYSTICK = SysTick_IRQn,
SYSTEM_INTERRUPT_MODULE_PM = PM_IRQn,
SYSTEM_INTERRUPT_MODULE_SYSCTRL = SYSCTRL_IRQn,
SYSTEM_INTERRUPT_MODULE_WDT = WDT_IRQn,
SYSTEM_INTERRUPT_MODULE_RTC = RTC_IRQn,
SYSTEM_INTERRUPT_MODULE_EIC = EIC_IRQn,
SYSTEM_INTERRUPT_MODULE_NVMCTRL = NVMCTRL_IRQn,
SYSTEM_INTERRUPT_MODULE_EVSYS = EVSYS_IRQn,
SYSTEM_INTERRUPT_MODULE_SERCOMn = SERCOMn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCn = TCn_IRQn,
SYSTEM_INTERRUPT_MODULE_AC = AC_IRQn,
SYSTEM_INTERRUPT_MODULE_ADC = ADC_IRQn,
SYSTEM_INTERRUPT_MODULE_DAC = DAC_IRQn
} |
| Table of possible system interrupt/exception vector numbers. More...
|
|
enum | system_interrupt_vector_samd21 {
SYSTEM_INTERRUPT_NON_MASKABLE = NonMaskableInt_IRQn,
SYSTEM_INTERRUPT_HARD_FAULT = HardFault_IRQn,
SYSTEM_INTERRUPT_SV_CALL = SVCall_IRQn,
SYSTEM_INTERRUPT_PENDING_SV = PendSV_IRQn,
SYSTEM_INTERRUPT_SYSTICK = SysTick_IRQn,
SYSTEM_INTERRUPT_MODULE_PM = PM_IRQn,
SYSTEM_INTERRUPT_MODULE_SYSCTRL = SYSCTRL_IRQn,
SYSTEM_INTERRUPT_MODULE_WDT = WDT_IRQn,
SYSTEM_INTERRUPT_MODULE_RTC = RTC_IRQn,
SYSTEM_INTERRUPT_MODULE_EIC = EIC_IRQn,
SYSTEM_INTERRUPT_MODULE_NVMCTRL = NVMCTRL_IRQn,
SYSTEM_INTERRUPT_MODULE_DMA = DMAC_IRQn,
SYSTEM_INTERRUPT_MODULE_USB = USB_IRQn,
SYSTEM_INTERRUPT_MODULE_EVSYS = EVSYS_IRQn,
SYSTEM_INTERRUPT_MODULE_SERCOMn = SERCOMn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCCn = TCCn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCn = TCn_IRQn,
SYSTEM_INTERRUPT_MODULE_ADC = ADC_IRQn,
SYSTEM_INTERRUPT_MODULE_AC = AC_IRQn,
SYSTEM_INTERRUPT_MODULE_DAC = DAC_IRQn,
SYSTEM_INTERRUPT_MODULE_PTC = PTC_IRQn,
SYSTEM_INTERRUPT_MODULE_I2S = I2S_IRQn,
SYSTEM_INTERRUPT_MODULE_AC1 = AC1_IRQn
} |
| Table of possible system interrupt/exception vector numbers. More...
|
|
enum | system_interrupt_vector_samda1 {
SYSTEM_INTERRUPT_NON_MASKABLE = NonMaskableInt_IRQn,
SYSTEM_INTERRUPT_HARD_FAULT = HardFault_IRQn,
SYSTEM_INTERRUPT_SV_CALL = SVCall_IRQn,
SYSTEM_INTERRUPT_PENDING_SV = PendSV_IRQn,
SYSTEM_INTERRUPT_SYSTICK = SysTick_IRQn,
SYSTEM_INTERRUPT_MODULE_PM = PM_IRQn,
SYSTEM_INTERRUPT_MODULE_SYSCTRL = SYSCTRL_IRQn,
SYSTEM_INTERRUPT_MODULE_WDT = WDT_IRQn,
SYSTEM_INTERRUPT_MODULE_RTC = RTC_IRQn,
SYSTEM_INTERRUPT_MODULE_EIC = EIC_IRQn,
SYSTEM_INTERRUPT_MODULE_NVMCTRL = NVMCTRL_IRQn,
SYSTEM_INTERRUPT_MODULE_DMA = DMAC_IRQn,
SYSTEM_INTERRUPT_MODULE_USB = USB_IRQn,
SYSTEM_INTERRUPT_MODULE_EVSYS = EVSYS_IRQn,
SYSTEM_INTERRUPT_MODULE_SERCOMn = SERCOMn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCCn = TCCn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCn = TCn_IRQn,
SYSTEM_INTERRUPT_MODULE_ADC = ADC_IRQn,
SYSTEM_INTERRUPT_MODULE_AC = AC_IRQn,
SYSTEM_INTERRUPT_MODULE_DAC = DAC_IRQn,
SYSTEM_INTERRUPT_MODULE_PTC = PTC_IRQn,
SYSTEM_INTERRUPT_MODULE_I2S = I2S_IRQn,
SYSTEM_INTERRUPT_MODULE_AC1 = AC1_IRQn
} |
| Table of possible system interrupt/exception vector numbers. More...
|
|
enum | system_interrupt_vector_saml21 {
SYSTEM_INTERRUPT_NON_MASKABLE = NonMaskableInt_IRQn,
SYSTEM_INTERRUPT_HARD_FAULT = HardFault_IRQn,
SYSTEM_INTERRUPT_SV_CALL = SVCall_IRQn,
SYSTEM_INTERRUPT_PENDING_SV = PendSV_IRQn,
SYSTEM_INTERRUPT_SYSTICK = SysTick_IRQn,
SYSTEM_INTERRUPT_MODULE_SYSTEM = SYSTEM_IRQn,
SYSTEM_INTERRUPT_MODULE_WDT = WDT_IRQn,
SYSTEM_INTERRUPT_MODULE_RTC = RTC_IRQn,
SYSTEM_INTERRUPT_MODULE_EIC = EIC_IRQn,
SYSTEM_INTERRUPT_MODULE_NVMCTRL = NVMCTRL_IRQn,
SYSTEM_INTERRUPT_MODULE_DMA = DMAC_IRQn,
SYSTEM_INTERRUPT_MODULE_USB = USB_IRQn,
SYSTEM_INTERRUPT_MODULE_EVSYS = EVSYS_IRQn,
SYSTEM_INTERRUPT_MODULE_SERCOMn = SERCOMn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCCn = TCCn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCn = TCn_IRQn,
SYSTEM_INTERRUPT_MODULE_AC = AC_IRQn,
SYSTEM_INTERRUPT_MODULE_ADC = ADC_IRQn,
SYSTEM_INTERRUPT_MODULE_DAC = DAC_IRQn,
SYSTEM_INTERRUPT_MODULE_PTC = PTC_IRQn,
SYSTEM_INTERRUPT_MODULE_AES = AES_IRQn,
SYSTEM_INTERRUPT_MODULE_TRNG = TRNG_IRQn
} |
| Table of possible system interrupt/exception vector numbers. More...
|
|
enum | system_interrupt_vector_saml22 {
SYSTEM_INTERRUPT_NON_MASKABLE = NonMaskableInt_IRQn,
SYSTEM_INTERRUPT_HARD_FAULT = HardFault_IRQn,
SYSTEM_INTERRUPT_SV_CALL = SVCall_IRQn,
SYSTEM_INTERRUPT_PENDING_SV = PendSV_IRQn,
SYSTEM_INTERRUPT_SYSTICK = SysTick_IRQn,
SYSTEM_INTERRUPT_MODULE_SYSTEM = SYSTEM_IRQn,
SYSTEM_INTERRUPT_MODULE_WDT = WDT_IRQn,
SYSTEM_INTERRUPT_MODULE_RTC = RTC_IRQn,
SYSTEM_INTERRUPT_MODULE_EIC = EIC_IRQn,
SYSTEM_INTERRUPT_MODULE_FREQM = FREQM_IRQn,
SYSTEM_INTERRUPT_MODULE_NVMCTRL = NVMCTRL_IRQn,
SYSTEM_INTERRUPT_MODULE_DMA = DMAC_IRQn,
SYSTEM_INTERRUPT_MODULE_EVSYS = EVSYS_IRQn,
SYSTEM_INTERRUPT_MODULE_SERCOMn = SERCOMn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCn = TCn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCC0 = TCC0_IRQn,
SYSTEM_INTERRUPT_MODULE_AC = AC_IRQn,
SYSTEM_INTERRUPT_MODULE_ADC = ADC_IRQn,
SYSTEM_INTERRUPT_MODULE_SLCD = SLCD_IRQn
} |
| Table of possible system interrupt/exception vector numbers. More...
|
|
enum | system_interrupt_vector_samr21 {
SYSTEM_INTERRUPT_NON_MASKABLE = NonMaskableInt_IRQn,
SYSTEM_INTERRUPT_HARD_FAULT = HardFault_IRQn,
SYSTEM_INTERRUPT_SV_CALL = SVCall_IRQn,
SYSTEM_INTERRUPT_PENDING_SV = PendSV_IRQn,
SYSTEM_INTERRUPT_SYSTICK = SysTick_IRQn,
SYSTEM_INTERRUPT_MODULE_PM = PM_IRQn,
SYSTEM_INTERRUPT_MODULE_SYSCTRL = SYSCTRL_IRQn,
SYSTEM_INTERRUPT_MODULE_WDT = WDT_IRQn,
SYSTEM_INTERRUPT_MODULE_RTC = RTC_IRQn,
SYSTEM_INTERRUPT_MODULE_EIC = EIC_IRQn,
SYSTEM_INTERRUPT_MODULE_NVMCTRL = NVMCTRL_IRQn,
SYSTEM_INTERRUPT_MODULE_DMA = DMAC_IRQn,
SYSTEM_INTERRUPT_MODULE_USB = USB_IRQn,
SYSTEM_INTERRUPT_MODULE_EVSYS = EVSYS_IRQn,
SYSTEM_INTERRUPT_MODULE_SERCOMn = SERCOMn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCCn = TCCn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCn = TCn_IRQn,
SYSTEM_INTERRUPT_MODULE_AC = AC_IRQn,
SYSTEM_INTERRUPT_MODULE_ADC = ADC_IRQn,
SYSTEM_INTERRUPT_MODULE_PTC = PTC_IRQn
} |
| Table of possible system interrupt/exception vector numbers. More...
|
|
enum | system_interrupt_vector_samr30 {
SYSTEM_INTERRUPT_NON_MASKABLE = NonMaskableInt_IRQn,
SYSTEM_INTERRUPT_HARD_FAULT = HardFault_IRQn,
SYSTEM_INTERRUPT_SV_CALL = SVCall_IRQn,
SYSTEM_INTERRUPT_PENDING_SV = PendSV_IRQn,
SYSTEM_INTERRUPT_SYSTICK = SysTick_IRQn,
SYSTEM_INTERRUPT_MODULE_SYSTEM = SYSTEM_IRQn,
SYSTEM_INTERRUPT_MODULE_WDT = WDT_IRQn,
SYSTEM_INTERRUPT_MODULE_RTC = RTC_IRQn,
SYSTEM_INTERRUPT_MODULE_EIC = EIC_IRQn,
SYSTEM_INTERRUPT_MODULE_NVMCTRL = NVMCTRL_IRQn,
SYSTEM_INTERRUPT_MODULE_DMA = DMAC_IRQn,
SYSTEM_INTERRUPT_MODULE_USB = USB_IRQn,
SYSTEM_INTERRUPT_MODULE_EVSYS = EVSYS_IRQn,
SYSTEM_INTERRUPT_MODULE_SERCOMn = SERCOMn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCCn = TCCn_IRQn,
SYSTEM_INTERRUPT_MODULE_TCn = TCn_IRQn,
SYSTEM_INTERRUPT_MODULE_AC = AC_IRQn,
SYSTEM_INTERRUPT_MODULE_ADC = ADC_IRQn,
SYSTEM_INTERRUPT_MODULE_PTC = PTC_IRQn
} |
| Table of possible system interrupt/exception vector numbers. More...
|
|
Table of possible system interrupt/exception vector priorities.
Table of all possible interrupt and exception vector priorities within the device.
Enumerator |
---|
SYSTEM_INTERRUPT_PRIORITY_LEVEL_0 |
Priority level 0, the highest possible interrupt priority.
|
SYSTEM_INTERRUPT_PRIORITY_LEVEL_1 |
Priority level 1.
|
SYSTEM_INTERRUPT_PRIORITY_LEVEL_2 |
Priority level 2.
|
SYSTEM_INTERRUPT_PRIORITY_LEVEL_3 |
Priority level 3, the lowest possible interrupt priority.
|
Table of possible system interrupt/exception vector numbers.
Table of all possible interrupt and exception vector indexes within the SAM C20/C21 device.
- Note
- The actual enumeration name is "system_interrupt_vector".
Enumerator |
---|
SYSTEM_INTERRUPT_NON_MASKABLE |
Interrupt vector index for a NMI interrupt.
|
SYSTEM_INTERRUPT_HARD_FAULT |
Interrupt vector index for a Hard Fault memory access exception.
|
SYSTEM_INTERRUPT_SV_CALL |
Interrupt vector index for a Supervisor Call exception.
|
SYSTEM_INTERRUPT_PENDING_SV |
Interrupt vector index for a Pending Supervisor interrupt.
|
SYSTEM_INTERRUPT_SYSTICK |
Interrupt vector index for a System Tick interrupt.
|
SYSTEM_INTERRUPT_MODULE_SYSTEM |
Interrupt vector index for MCLK, OSCCTRL, OSC32KCTRL, PAC, PM, SUPC, TAL peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_WDT |
Interrupt vector index for a Watch Dog peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_RTC |
Interrupt vector index for a Real Time Clock peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_EIC |
Interrupt vector index for an External Interrupt peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_FREQM |
Interrupt vector index for Frequency Meter peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_NVMCTRL |
Interrupt vector index for a Non Volatile Memory Controller interrupt.
|
SYSTEM_INTERRUPT_MODULE_DMA |
Interrupt vector index for a Direct Memory Access interrupt.
|
SYSTEM_INTERRUPT_MODULE_EVSYS |
Interrupt vector index for an Event System interrupt.
|
SYSTEM_INTERRUPT_MODULE_SERCOMn |
Interrupt vector index for a SERCOM peripheral interrupt.
Each specific device may contain several SERCOM peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_SERCOM0 ).
|
SYSTEM_INTERRUPT_MODULE_TCCn |
Interrupt vector index for a Timer/Counter Control peripheral interrupt.
Each specific device may contain several TCC peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_TCC0 ).
|
SYSTEM_INTERRUPT_MODULE_TCn |
Interrupt vector index for a Timer/Counter peripheral interrupt.
Each specific device may contain several TC peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_TC3 ).
|
Table of possible system interrupt/exception vector numbers.
Table of all possible interrupt and exception vector indexes within the SAM D09 device.
- Note
- The actual enumeration name is "system_interrupt_vector".
Enumerator |
---|
SYSTEM_INTERRUPT_NON_MASKABLE |
Interrupt vector index for a NMI interrupt.
|
SYSTEM_INTERRUPT_HARD_FAULT |
Interrupt vector index for a Hard Fault memory access exception.
|
SYSTEM_INTERRUPT_SV_CALL |
Interrupt vector index for a Supervisor Call exception.
|
SYSTEM_INTERRUPT_PENDING_SV |
Interrupt vector index for a Pending Supervisor interrupt.
|
SYSTEM_INTERRUPT_SYSTICK |
Interrupt vector index for a System Tick interrupt.
|
SYSTEM_INTERRUPT_MODULE_PM |
Interrupt vector index for a Power Manager peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_SYSCTRL |
Interrupt vector index for a System Control peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_WDT |
Interrupt vector index for a Watch Dog peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_RTC |
Interrupt vector index for a Real Time Clock peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_EIC |
Interrupt vector index for an External Interrupt peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_NVMCTRL |
Interrupt vector index for a Non Volatile Memory Controller interrupt.
|
SYSTEM_INTERRUPT_MODULE_DMA |
Interrupt vector index for a Direct Memory Access interrupt.
|
SYSTEM_INTERRUPT_MODULE_EVSYS |
Interrupt vector index for an Event System interrupt.
|
SYSTEM_INTERRUPT_MODULE_SERCOMn |
Interrupt vector index for a SERCOM peripheral interrupt.
Each specific device may contain several SERCOM peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_SERCOM0 ).
|
SYSTEM_INTERRUPT_MODULE_TCn |
Interrupt vector index for a Timer/Counter peripheral interrupt.
Each specific device may contain several TC peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_TC3 ).
|
SYSTEM_INTERRUPT_MODULE_ADC |
Interrupt vector index for an Analog-to-Digital peripheral interrupt.
|
Table of possible system interrupt/exception vector numbers.
Table of all possible interrupt and exception vector indexes within the SAM D10/D11 device.
- Note
- The actual enumeration name is "system_interrupt_vector".
Enumerator |
---|
SYSTEM_INTERRUPT_NON_MASKABLE |
Interrupt vector index for a NMI interrupt.
|
SYSTEM_INTERRUPT_HARD_FAULT |
Interrupt vector index for a Hard Fault memory access exception.
|
SYSTEM_INTERRUPT_SV_CALL |
Interrupt vector index for a Supervisor Call exception.
|
SYSTEM_INTERRUPT_PENDING_SV |
Interrupt vector index for a Pending Supervisor interrupt.
|
SYSTEM_INTERRUPT_SYSTICK |
Interrupt vector index for a System Tick interrupt.
|
SYSTEM_INTERRUPT_MODULE_PM |
Interrupt vector index for a Power Manager peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_SYSCTRL |
Interrupt vector index for a System Control peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_WDT |
Interrupt vector index for a Watch Dog peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_RTC |
Interrupt vector index for a Real Time Clock peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_EIC |
Interrupt vector index for an External Interrupt peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_NVMCTRL |
Interrupt vector index for a Non Volatile Memory Controller interrupt.
|
SYSTEM_INTERRUPT_MODULE_DMA |
Interrupt vector index for a Direct Memory Access interrupt.
|
SYSTEM_INTERRUPT_MODULE_EVSYS |
Interrupt vector index for an Event System interrupt.
|
SYSTEM_INTERRUPT_MODULE_SERCOMn |
Interrupt vector index for a SERCOM peripheral interrupt.
Each specific device may contain several SERCOM peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_SERCOM0 ).
|
SYSTEM_INTERRUPT_MODULE_TCCn |
Interrupt vector index for a Timer/Counter Control peripheral interrupt.
Each specific device may contain several TCC peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_TCC0 ).
|
SYSTEM_INTERRUPT_MODULE_TCn |
Interrupt vector index for a Timer/Counter peripheral interrupt.
Each specific device may contain several TC peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_TC3 ).
|
SYSTEM_INTERRUPT_MODULE_AC |
Interrupt vector index for an Analog Comparator peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_ADC |
Interrupt vector index for an Analog-to-Digital peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_DAC |
Interrupt vector index for a Digital-to-Analog peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_PTC |
Interrupt vector index for a Peripheral Touch Controller peripheral interrupt.
|
Table of possible system interrupt/exception vector numbers.
Table of all possible interrupt and exception vector indexes within the SAM D20 device.
- Note
- The actual enumeration name is "system_interrupt_vector".
Enumerator |
---|
SYSTEM_INTERRUPT_NON_MASKABLE |
Interrupt vector index for a NMI interrupt.
|
SYSTEM_INTERRUPT_HARD_FAULT |
Interrupt vector index for a Hard Fault memory access exception.
|
SYSTEM_INTERRUPT_SV_CALL |
Interrupt vector index for a Supervisor Call exception.
|
SYSTEM_INTERRUPT_PENDING_SV |
Interrupt vector index for a Pending Supervisor interrupt.
|
SYSTEM_INTERRUPT_SYSTICK |
Interrupt vector index for a System Tick interrupt.
|
SYSTEM_INTERRUPT_MODULE_PM |
Interrupt vector index for a Power Manager peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_SYSCTRL |
Interrupt vector index for a System Control peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_WDT |
Interrupt vector index for a Watch Dog peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_RTC |
Interrupt vector index for a Real Time Clock peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_EIC |
Interrupt vector index for an External Interrupt peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_NVMCTRL |
Interrupt vector index for a Non Volatile Memory Controller interrupt.
|
SYSTEM_INTERRUPT_MODULE_EVSYS |
Interrupt vector index for an Event System interrupt.
|
SYSTEM_INTERRUPT_MODULE_SERCOMn |
Interrupt vector index for a SERCOM peripheral interrupt.
Each specific device may contain several SERCOM peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_SERCOM0 ).
|
SYSTEM_INTERRUPT_MODULE_TCn |
Interrupt vector index for a Timer/Counter peripheral interrupt.
Each specific device may contain several TC peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_TC0 ).
|
SYSTEM_INTERRUPT_MODULE_AC |
Interrupt vector index for an Analog Comparator peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_ADC |
Interrupt vector index for an Analog-to-Digital peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_DAC |
Interrupt vector index for a Digital-to-Analog peripheral interrupt.
|
Table of possible system interrupt/exception vector numbers.
Table of all possible interrupt and exception vector indexes within the SAM D21 device. Check peripherals configuration in SAM D21 datasheet for available vector index for specific device.
- Note
- The actual enumeration name is "system_interrupt_vector".
Enumerator |
---|
SYSTEM_INTERRUPT_NON_MASKABLE |
Interrupt vector index for a NMI interrupt.
|
SYSTEM_INTERRUPT_HARD_FAULT |
Interrupt vector index for a Hard Fault memory access exception.
|
SYSTEM_INTERRUPT_SV_CALL |
Interrupt vector index for a Supervisor Call exception.
|
SYSTEM_INTERRUPT_PENDING_SV |
Interrupt vector index for a Pending Supervisor interrupt.
|
SYSTEM_INTERRUPT_SYSTICK |
Interrupt vector index for a System Tick interrupt.
|
SYSTEM_INTERRUPT_MODULE_PM |
Interrupt vector index for a Power Manager peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_SYSCTRL |
Interrupt vector index for a System Control peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_WDT |
Interrupt vector index for a Watch Dog peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_RTC |
Interrupt vector index for a Real Time Clock peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_EIC |
Interrupt vector index for an External Interrupt peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_NVMCTRL |
Interrupt vector index for a Non Volatile Memory Controller interrupt.
|
SYSTEM_INTERRUPT_MODULE_DMA |
Interrupt vector index for a Direct Memory Access interrupt.
|
SYSTEM_INTERRUPT_MODULE_USB |
Interrupt vector index for a Universal Serial Bus interrupt.
|
SYSTEM_INTERRUPT_MODULE_EVSYS |
Interrupt vector index for an Event System interrupt.
|
SYSTEM_INTERRUPT_MODULE_SERCOMn |
Interrupt vector index for a SERCOM peripheral interrupt.
Each specific device may contain several SERCOM peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_SERCOM0 ).
|
SYSTEM_INTERRUPT_MODULE_TCCn |
Interrupt vector index for a Timer/Counter Control peripheral interrupt.
Each specific device may contain several TCC peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_TCC0 ).
|
SYSTEM_INTERRUPT_MODULE_TCn |
Interrupt vector index for a Timer/Counter peripheral interrupt.
Each specific device may contain several TC peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_TC3 ).
|
SYSTEM_INTERRUPT_MODULE_ADC |
Interrupt vector index for an Analog-to-Digital peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_AC |
Interrupt vector index for an Analog Comparator peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_DAC |
Interrupt vector index for a Digital-to-Analog peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_PTC |
Interrupt vector index for a Peripheral Touch Controller peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_I2S |
Interrupt vector index for a Inter-IC Sound Interface peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_AC1 |
Interrupt vector index for an Analog Comparator 1 peripheral interrupt.
|
Table of possible system interrupt/exception vector numbers.
Table of all possible interrupt and exception vector indexes within the SAM DA1 device. Check peripherals configuration in SAM DA1 datasheet for available vector index for specific device.
- Note
- The actual enumeration name is "system_interrupt_vector".
Enumerator |
---|
SYSTEM_INTERRUPT_NON_MASKABLE |
Interrupt vector index for a NMI interrupt.
|
SYSTEM_INTERRUPT_HARD_FAULT |
Interrupt vector index for a Hard Fault memory access exception.
|
SYSTEM_INTERRUPT_SV_CALL |
Interrupt vector index for a Supervisor Call exception.
|
SYSTEM_INTERRUPT_PENDING_SV |
Interrupt vector index for a Pending Supervisor interrupt.
|
SYSTEM_INTERRUPT_SYSTICK |
Interrupt vector index for a System Tick interrupt.
|
SYSTEM_INTERRUPT_MODULE_PM |
Interrupt vector index for a Power Manager peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_SYSCTRL |
Interrupt vector index for a System Control peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_WDT |
Interrupt vector index for a Watch Dog peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_RTC |
Interrupt vector index for a Real Time Clock peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_EIC |
Interrupt vector index for an External Interrupt peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_NVMCTRL |
Interrupt vector index for a Non Volatile Memory Controller interrupt.
|
SYSTEM_INTERRUPT_MODULE_DMA |
Interrupt vector index for a Direct Memory Access interrupt.
|
SYSTEM_INTERRUPT_MODULE_USB |
Interrupt vector index for a Universal Serial Bus interrupt.
|
SYSTEM_INTERRUPT_MODULE_EVSYS |
Interrupt vector index for an Event System interrupt.
|
SYSTEM_INTERRUPT_MODULE_SERCOMn |
Interrupt vector index for a SERCOM peripheral interrupt.
Each specific device may contain several SERCOM peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_SERCOM0 ).
|
SYSTEM_INTERRUPT_MODULE_TCCn |
Interrupt vector index for a Timer/Counter Control peripheral interrupt.
Each specific device may contain several TCC peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_TCC0 ).
|
SYSTEM_INTERRUPT_MODULE_TCn |
Interrupt vector index for a Timer/Counter peripheral interrupt.
Each specific device may contain several TC peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_TC3 ).
|
SYSTEM_INTERRUPT_MODULE_ADC |
Interrupt vector index for an Analog-to-Digital peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_AC |
Interrupt vector index for an Analog Comparator peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_DAC |
Interrupt vector index for a Digital-to-Analog peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_PTC |
Interrupt vector index for a Peripheral Touch Controller peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_I2S |
Interrupt vector index for a Inter-IC Sound Interface peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_AC1 |
Interrupt vector index for an Analog Comparator 1 peripheral interrupt.
|
Table of possible system interrupt/exception vector numbers.
Table of all possible interrupt and exception vector indexes within the SAM L21 device.
- Note
- The actual enumeration name is "system_interrupt_vector".
Enumerator |
---|
SYSTEM_INTERRUPT_NON_MASKABLE |
Interrupt vector index for a NMI interrupt.
|
SYSTEM_INTERRUPT_HARD_FAULT |
Interrupt vector index for a Hard Fault memory access exception.
|
SYSTEM_INTERRUPT_SV_CALL |
Interrupt vector index for a Supervisor Call exception.
|
SYSTEM_INTERRUPT_PENDING_SV |
Interrupt vector index for a Pending Supervisor interrupt.
|
SYSTEM_INTERRUPT_SYSTICK |
Interrupt vector index for a System Tick interrupt.
|
SYSTEM_INTERRUPT_MODULE_SYSTEM |
Interrupt vector index for MCLK, OSCCTRL, OSC32KCTRL, PAC, PM, SUPC, TAL peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_WDT |
Interrupt vector index for a Watch Dog peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_RTC |
Interrupt vector index for a Real Time Clock peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_EIC |
Interrupt vector index for an External Interrupt peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_NVMCTRL |
Interrupt vector index for a Non Volatile Memory Controller interrupt.
|
SYSTEM_INTERRUPT_MODULE_DMA |
Interrupt vector index for a Direct Memory Access interrupt.
|
SYSTEM_INTERRUPT_MODULE_USB |
Interrupt vector index for a Universal Serial Bus interrupt.
|
SYSTEM_INTERRUPT_MODULE_EVSYS |
Interrupt vector index for an Event System interrupt.
|
SYSTEM_INTERRUPT_MODULE_SERCOMn |
Interrupt vector index for a SERCOM peripheral interrupt.
Each specific device may contain several SERCOM peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_SERCOM0 ).
|
SYSTEM_INTERRUPT_MODULE_TCCn |
Interrupt vector index for a Timer/Counter Control peripheral interrupt.
Each specific device may contain several TCC peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_TCC0 ).
|
SYSTEM_INTERRUPT_MODULE_TCn |
Interrupt vector index for a Timer/Counter peripheral interrupt.
Each specific device may contain several TC peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_TC3 ).
|
SYSTEM_INTERRUPT_MODULE_AC |
Interrupt vector index for an Analog Comparator peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_ADC |
Interrupt vector index for an Analog-to-Digital peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_DAC |
Interrupt vector index for a Digital-to-Analog peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_PTC |
Interrupt vector index for a Peripheral Touch Controller peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_AES |
Interrupt vector index for a AES peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_TRNG |
Interrupt vector index for a TRNG peripheral interrupt.
|
Table of possible system interrupt/exception vector numbers.
Table of all possible interrupt and exception vector indexes within the SAM L22 device.
- Note
- The actual enumeration name is "system_interrupt_vector".
Enumerator |
---|
SYSTEM_INTERRUPT_NON_MASKABLE |
Interrupt vector index for a NMI interrupt.
|
SYSTEM_INTERRUPT_HARD_FAULT |
Interrupt vector index for a Hard Fault memory access exception.
|
SYSTEM_INTERRUPT_SV_CALL |
Interrupt vector index for a Supervisor Call exception.
|
SYSTEM_INTERRUPT_PENDING_SV |
Interrupt vector index for a Pending Supervisor interrupt.
|
SYSTEM_INTERRUPT_SYSTICK |
Interrupt vector index for a System Tick interrupt.
|
SYSTEM_INTERRUPT_MODULE_SYSTEM |
Interrupt vector index for MCLK, OSCCTRL, OSC32KCTRL, PAC, PM, SUPC, TAL peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_WDT |
Interrupt vector index for a Watch Dog peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_RTC |
Interrupt vector index for a Real Time Clock peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_EIC |
Interrupt vector index for an External Interrupt peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_FREQM |
Interrupt vector index for Frequency Meter peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_NVMCTRL |
Interrupt vector index for a Non Volatile Memory Controller interrupt.
|
SYSTEM_INTERRUPT_MODULE_DMA |
Interrupt vector index for a Direct Memory Access interrupt.
|
SYSTEM_INTERRUPT_MODULE_EVSYS |
Interrupt vector index for an Event System interrupt.
|
SYSTEM_INTERRUPT_MODULE_SERCOMn |
Interrupt vector index for a SERCOM peripheral interrupt.
Each specific device may contain several SERCOM peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_SERCOM0 ).
|
SYSTEM_INTERRUPT_MODULE_TCn |
Interrupt vector index for a Timer/Counter peripheral interrupt.
Each specific device may contain several TC peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_TC3 ).
|
SYSTEM_INTERRUPT_MODULE_TCC0 |
Interrupt vector index for a Timer/Counter Control peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_AC |
Interrupt vector index for an Analog Comparator peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_ADC |
Interrupt vector index for an Analog-to-Digital peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_SLCD |
Interrupt vector index for a Peripheral Touch Controller peripheral interrupt.
|
Table of possible system interrupt/exception vector numbers.
Table of all possible interrupt and exception vector indexes within the SAM R21 device.
- Note
- The actual enumeration name is "system_interrupt_vector".
Enumerator |
---|
SYSTEM_INTERRUPT_NON_MASKABLE |
Interrupt vector index for a NMI interrupt.
|
SYSTEM_INTERRUPT_HARD_FAULT |
Interrupt vector index for a Hard Fault memory access exception.
|
SYSTEM_INTERRUPT_SV_CALL |
Interrupt vector index for a Supervisor Call exception.
|
SYSTEM_INTERRUPT_PENDING_SV |
Interrupt vector index for a Pending Supervisor interrupt.
|
SYSTEM_INTERRUPT_SYSTICK |
Interrupt vector index for a System Tick interrupt.
|
SYSTEM_INTERRUPT_MODULE_PM |
Interrupt vector index for a Power Manager peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_SYSCTRL |
Interrupt vector index for a System Control peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_WDT |
Interrupt vector index for a Watch Dog peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_RTC |
Interrupt vector index for a Real Time Clock peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_EIC |
Interrupt vector index for an External Interrupt peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_NVMCTRL |
Interrupt vector index for a Non Volatile Memory Controller interrupt.
|
SYSTEM_INTERRUPT_MODULE_DMA |
Interrupt vector index for a Direct Memory Access interrupt.
|
SYSTEM_INTERRUPT_MODULE_USB |
Interrupt vector index for a Universal Serial Bus interrupt.
|
SYSTEM_INTERRUPT_MODULE_EVSYS |
Interrupt vector index for an Event System interrupt.
|
SYSTEM_INTERRUPT_MODULE_SERCOMn |
Interrupt vector index for a SERCOM peripheral interrupt.
Each specific device may contain several SERCOM peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_SERCOM0 ).
|
SYSTEM_INTERRUPT_MODULE_TCCn |
Interrupt vector index for a Timer/Counter Control peripheral interrupt.
Each specific device may contain several TCC peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_TCC0 ).
|
SYSTEM_INTERRUPT_MODULE_TCn |
Interrupt vector index for a Timer/Counter peripheral interrupt.
Each specific device may contain several TC peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_TC3 ).
|
SYSTEM_INTERRUPT_MODULE_AC |
Interrupt vector index for an Analog Comparator peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_ADC |
Interrupt vector index for an Analog-to-Digital peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_PTC |
Interrupt vector index for a Peripheral Touch Controller peripheral interrupt.
|
Table of possible system interrupt/exception vector numbers.
Table of all possible interrupt and exception vector indexes within the SAM L21 device.
- Note
- The actual enumeration name is "system_interrupt_vector".
Enumerator |
---|
SYSTEM_INTERRUPT_NON_MASKABLE |
Interrupt vector index for a NMI interrupt.
|
SYSTEM_INTERRUPT_HARD_FAULT |
Interrupt vector index for a Hard Fault memory access exception.
|
SYSTEM_INTERRUPT_SV_CALL |
Interrupt vector index for a Supervisor Call exception.
|
SYSTEM_INTERRUPT_PENDING_SV |
Interrupt vector index for a Pending Supervisor interrupt.
|
SYSTEM_INTERRUPT_SYSTICK |
Interrupt vector index for a System Tick interrupt.
|
SYSTEM_INTERRUPT_MODULE_SYSTEM |
Interrupt vector index for MCLK, OSCCTRL, OSC32KCTRL, PAC, PM, SUPC, TAL peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_WDT |
Interrupt vector index for a Watch Dog peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_RTC |
Interrupt vector index for a Real Time Clock peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_EIC |
Interrupt vector index for an External Interrupt peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_NVMCTRL |
Interrupt vector index for a Non Volatile Memory Controller interrupt.
|
SYSTEM_INTERRUPT_MODULE_DMA |
Interrupt vector index for a Direct Memory Access interrupt.
|
SYSTEM_INTERRUPT_MODULE_USB |
Interrupt vector index for a Universal Serial Bus interrupt.
|
SYSTEM_INTERRUPT_MODULE_EVSYS |
Interrupt vector index for an Event System interrupt.
|
SYSTEM_INTERRUPT_MODULE_SERCOMn |
Interrupt vector index for a SERCOM peripheral interrupt.
Each specific device may contain several SERCOM peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_SERCOM0 ).
|
SYSTEM_INTERRUPT_MODULE_TCCn |
Interrupt vector index for a Timer/Counter Control peripheral interrupt.
Each specific device may contain several TCC peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_TCC0 ).
|
SYSTEM_INTERRUPT_MODULE_TCn |
Interrupt vector index for a Timer/Counter peripheral interrupt.
Each specific device may contain several TC peripherals; each module instance will have its own entry in the table, with the instance number substituted for "n" in the entry name (e.g. SYSTEM_INTERRUPT_MODULE_TC3 ).
|
SYSTEM_INTERRUPT_MODULE_AC |
Interrupt vector index for an Analog Comparator peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_ADC |
Interrupt vector index for an Analog-to-Digital peripheral interrupt.
|
SYSTEM_INTERRUPT_MODULE_PTC |
Interrupt vector index for a Peripheral Touch Controller peripheral interrupt.
|
enum status_code system_interrupt_clear_pending |
( |
const enum system_interrupt_vector |
vector | ) |
|
static void system_interrupt_disable |
( |
const enum system_interrupt_vector |
vector | ) |
|
|
inlinestatic |
Disable interrupt vector.
Disables execution of the software handler for the requested interrupt vector.
- Parameters
-
[in] | vector | Interrupt vector to disable |
Referenced by _dac_interrupt_handler(), adc_disable(), freqm_disable_callback(), i2c_master_disable(), i2c_slave_disable(), rtc_calendar_disable(), rtc_count_disable(), sdadc_disable(), spi_disable(), spi_master_vec_disable(), tcc_disable_callback(), and usart_disable().
static void system_interrupt_disable_global |
( |
void |
| ) |
|
|
inlinestatic |
Disables global interrupts.
Disabled global interrupts in the device, preventing any enabled interrupt handlers from executing.
References cpu_irq_disable.
Referenced by dsu_crc32_cal().
static void system_interrupt_enable |
( |
const enum system_interrupt_vector |
vector | ) |
|
|
inlinestatic |
Enable interrupt vector.
Enables execution of the software handler for the requested interrupt vector.
- Parameters
-
[in] | vector | Interrupt vector to enable |
Referenced by _system_extint_init(), ac_enable_callback(), adc_enable(), configure_bod(), configure_can(), dac_chan_write_buffer_job(), dma_start_transfer_job(), events_add_hook(), freqm_enable_callback(), i2c_master_enable(), i2c_slave_enable(), main(), rtc_calendar_enable(), rtc_count_enable(), sdadc_enable(), spi_enable(), spi_master_vec_enable(), tc_enable_callback(), tcc_enable_callback(), usart_enable(), and wdt_enable_callback().
static void system_interrupt_enable_global |
( |
void |
| ) |
|
|
inlinestatic |
static void system_interrupt_enter_critical_section |
( |
void |
| ) |
|
|
inlinestatic |
Enters a critical section.
Disables global interrupts. To support nested critical sections, an internal count of the critical section nesting will be kept, so that global interrupts are only re-enabled upon leaving the outermost nested critical section.
References cpu_irq_enter_critical().
Referenced by _dma_find_first_free_channel_and_allocate(), _dma_set_config(), _events_find_first_free_channel_and_allocate(), _events_release_channel(), _usart_read_buffer(), _usart_write_buffer(), dma_abort_job(), dma_allocate(), dma_free(), dma_resume_job(), dma_start_transfer_job(), dma_suspend_job(), DMAC_Handler(), events_trigger(), i2c_master_lock(), i2c_master_reset(), i2c_slave_lock(), i2c_slave_reset(), main(), nvm_update_buffer(), spi_lock(), spi_master_vec_lock(), spi_master_vec_transceive_buffer_job(), system_gclk_chan_disable(), system_gclk_chan_enable(), system_gclk_chan_get_hz(), system_gclk_chan_is_enabled(), system_gclk_chan_is_locked(), system_gclk_chan_lock(), system_gclk_gen_disable(), system_gclk_gen_enable(), system_gclk_gen_get_hz(), system_gclk_gen_is_enabled(), system_gclk_gen_set_config(), and usart_lock().
static enum system_interrupt_vector system_interrupt_get_active |
( |
void |
| ) |
|
|
inlinestatic |
Get active interrupt (if any).
Return the vector number for the current executing software handler, if any.
- Returns
- Interrupt number that is currently executing.
Get interrupt vector priority level.
Retrieves the priority level of the requested external interrupt or exception.
- Parameters
-
[in] | vector | Interrupt vector of which the priority level will be read |
- Returns
- Currently configured interrupt priority level of the given interrupt vector.
References SYSTEM_INTERRUPT_PRIORITY_LEVEL_0, and SYSTEM_INTERRUPT_SYSTICK.
static bool system_interrupt_is_enabled |
( |
const enum system_interrupt_vector |
vector | ) |
|
|
inlinestatic |
Checks if an interrupt vector is enabled or not.
Checks if a specific interrupt vector is currently enabled.
- Parameters
-
[in] | vector | Interrupt vector number to check |
- Returns
- A variable identifying if the requested interrupt vector is enabled.
- Return values
-
true | Specified interrupt vector is currently enabled |
false | Specified interrupt vector is currently disabled |
Referenced by events_add_hook().
static bool system_interrupt_is_global_enabled |
( |
void |
| ) |
|
|
inlinestatic |
Check if global interrupts are enabled.
Checks if global interrupts are currently enabled.
- Returns
- A boolean that identifies if the global interrupts are enabled or not.
- Return values
-
true | Global interrupts are currently enabled |
false | Global interrupts are currently disabled |
References cpu_irq_is_enabled.
bool system_interrupt_is_pending |
( |
const enum system_interrupt_vector |
vector | ) |
|
Check if a interrupt line is pending.
Checks if the requested interrupt vector is pending.
- Parameters
-
[in] | vector | Interrupt vector number to check |
- Returns
- A boolean identifying if the requested interrupt vector is pending.
- Return values
-
true | Specified interrupt vector is pending |
false | Specified interrupt vector is not pending |
References Assert, result, and SYSTEM_INTERRUPT_SYSTICK.
static void system_interrupt_leave_critical_section |
( |
void |
| ) |
|
|
inlinestatic |
Leaves a critical section.
Enables global interrupts. To support nested critical sections, an internal count of the critical section nesting will be kept, so that global interrupts are only re-enabled upon leaving the outermost nested critical section.
References cpu_irq_leave_critical().
Referenced by _dma_find_first_free_channel_and_allocate(), _dma_set_config(), _events_find_first_free_channel_and_allocate(), _events_release_channel(), _usart_read_buffer(), _usart_write_buffer(), dma_abort_job(), dma_allocate(), dma_free(), dma_resume_job(), dma_start_transfer_job(), dma_suspend_job(), DMAC_Handler(), events_trigger(), i2c_master_lock(), i2c_master_reset(), i2c_slave_lock(), i2c_slave_reset(), main(), nvm_update_buffer(), spi_lock(), spi_master_vec_lock(), spi_master_vec_transceive_buffer_job(), system_gclk_chan_disable(), system_gclk_chan_enable(), system_gclk_chan_get_hz(), system_gclk_chan_is_enabled(), system_gclk_chan_is_locked(), system_gclk_chan_lock(), system_gclk_gen_disable(), system_gclk_gen_enable(), system_gclk_gen_get_hz(), system_gclk_gen_is_enabled(), system_gclk_gen_set_config(), and usart_lock().
enum status_code system_interrupt_set_pending |
( |
const enum system_interrupt_vector |
vector | ) |
|
Set a interrupt vector as pending.
Set the requested interrupt vector as pending (i.e. issues a software interrupt request for the specified vector). The software handler will be handled (if enabled) in a priority order based on vector number and configured priority settings.
- Parameters
-
[in] | vector | Interrupt vector number which is set as pending |
- Returns
- Status code identifying if the vector was successfully set as pending.
- Return values
-
STATUS_OK | If no error was detected |
STATUS_INVALID_ARG | If an unsupported interrupt vector number was given |
References Assert, STATUS_ERR_INVALID_ARG, STATUS_OK, SYSTEM_INTERRUPT_NON_MASKABLE, and SYSTEM_INTERRUPT_SYSTICK.
Set interrupt vector priority level.
Set the priority level of an external interrupt or exception.
- Parameters
-
[in] | vector | Interrupt vector to change |
[in] | priority_level | New vector priority level to set |
- Returns
- Status code indicating if the priority level of the interrupt was successfully set.
- Return values
-
STATUS_OK | If no error was detected |
STATUS_INVALID_ARG | If an unsupported interrupt vector number was given |
References Assert, STATUS_ERR_INVALID_ARG, STATUS_OK, and SYSTEM_INTERRUPT_SYSTICK.