#include <stdint.h>
#include <stdbool.h>
#include "stack_config.h"
#include "tal_generic.h"
#include "return_val.h"
#include "mac_api.h"
#include "qmm.h"
#include "mac_build_config.h"
Macros | |
#define | FCF_ADDR_MASK (3) |
#define | FCF_GET_DEST_ADDR_MODE(x) (((x) >> FCF_DEST_ADDR_OFFSET) & FCF_ADDR_MASK) |
#define | FCF_GET_SOURCE_ADDR_MODE(x) (((x) >> FCF_SOURCE_ADDR_OFFSET) & FCF_ADDR_MASK) |
Functions | |
uint8_t | mac_extract_mhr_addr_info (uint8_t *frame_ptr) |
retval_t | mac_init (void) |
Initializes the MAC sublayer. More... | |
bool | mac_task (void) |
Runs the MAC scheduler. More... | |
void | mcps_data_conf (uint8_t *m) |
Wrapper function for messages of type mcps_data_conf_t. More... | |
void | mcps_data_ind (uint8_t *m) |
Wrapper function for messages of type mcps_data_ind_t. More... | |
void | mcps_data_request (uint8_t *msg) |
Builds the data frame for transmission. More... | |
retval_t | mlme_get (uint8_t attribute, pib_value_t *attribute_value) |
void | mlme_gts_conf (uint8_t *m) |
void | mlme_gts_ind (uint8_t *m) |
void | mlme_gts_request (uint8_t *m) |
void | mlme_reset_conf (uint8_t *m) |
Wrapper function for messages of type mlme_reset_conf_t. More... | |
void | mlme_reset_request (uint8_t *m) |
Resets the MAC layer. More... | |
retval_t | mlme_set (uint8_t attribute, pib_value_t *attribute_value, bool set_trx_to_sleep) |
Setting of MAC PIB attributes via functional access. More... | |
void | mlme_set_conf (uint8_t *m) |
Wrapper function for messages of type mlme_set_conf_t. More... | |
void | mlme_set_request (uint8_t *m) |
Handles an MLME-SET.request primitive. More... | |
void | mlme_sync_loss_ind (uint8_t *m) |
Wrapper function for messages of type mlme_sync_loss_ind_t. More... | |
void | mlme_sync_request (uint8_t *m) |
Implements the MLME-SYNC request. More... | |
Variables | |
queue_t | mac_nhle_q |
Queue used by MAC for communication to next higher layer. More... | |
queue_t | nhle_mac_q |
NHLE to MAC queue in which NHLE pushes all the requests to the MAC layer. More... | |
#define FCF_ADDR_MASK (3) |
Referenced by mac_extract_mhr_addr_info().
#define FCF_GET_DEST_ADDR_MODE | ( | x | ) | (((x) >> FCF_DEST_ADDR_OFFSET) & FCF_ADDR_MASK) |
#define FCF_GET_SOURCE_ADDR_MODE | ( | x | ) | (((x) >> FCF_SOURCE_ADDR_OFFSET) & FCF_ADDR_MASK) |
uint8_t mac_extract_mhr_addr_info | ( | uint8_t * | frame_ptr | ) |
References convert_byte_array_to_16_bit(), convert_byte_array_to_64_bit(), parse_tag::dest_addr, parse_tag::dest_addr_mode, parse_tag::dest_panid, EXT_ADDR_LEN, parse_tag::fcf, FCF_ADDR_MASK, FCF_DEST_ADDR_OFFSET, FCF_LEN, FCF_LONG_ADDR, FCF_PAN_ID_COMPRESSION, FCF_SHORT_ADDR, FCF_SOURCE_ADDR_OFFSET, FCS_LEN, address_field_t::long_address, mac_parse_data, parse_tag::mac_payload_length, parse_tag::mpdu_length, PAN_ID_LEN, SEQ_NUM_LEN, SHORT_ADDR_LEN, address_field_t::short_address, parse_tag::src_addr, parse_tag::src_addr_mode, and parse_tag::src_panid.
Referenced by parse_mpdu().
retval_t mlme_get | ( | uint8_t | attribute, |
pib_value_t * | attribute_value | ||
) |
References ADDR_COPY_DST_SRC_16, ADDR_COPY_DST_SRC_64, mac_pib_tag::mac_AutoRequest, mac_pib_tag::mac_BattLifeExtPeriods, mac_pib_tag::mac_CoordExtendedAddress, mac_pib_tag::mac_CoordShortAddress, mac_pib_tag::mac_DSN, MAC_INVALID_INDEX, mac_pib_tag::mac_MaxFrameTotalWaitTime, mac_pib, mac_pib_tag::mac_ResponseWaitTime, mac_pib_tag::mac_RxOnWhenIdle, mac_pib_tag::mac_SecurityEnabled, mac_state, MAC_SUCCESS, mac_sync_state, MAC_UNSUPPORTED_ATTRIBUTE, macAssociatedPANCoord, macAssociationPermit, macAutoRequest, macBattLifeExt, macBattLifeExtPeriods, macBeaconOrder, macBeaconPayload, macBeaconPayloadLength, macBeaconTxTime, macBSN, macCoordExtendedAddress, macCoordShortAddress, macDSN, macIeeeAddress, macMaxBE, macMaxCSMABackoffs, macMaxFrameRetries, macMaxFrameTotalWaitTime, macMinBE, macPANId, macPrivateIllegalFrameType, macPrivateMACState, macPrivateMACSyncState, macPrivateNoDataAfterAssocReq, macPrivateVirtualPANs, macPromiscuousMode, macResponseWaitTime, macRxOnWhenIdle, macSecurityEnabled, macShortAddress, macSuperframeOrder, macTransactionPersistenceTime, MEMCPY_ENDIAN, phyCCAMode, phyChannelsSupported, phyCurrentChannel, phyCurrentPage, phyMaxFrameDuration, phySHRDuration, phySymbolsPerOctet, phyTransmitPower, mac_pib_tag::privateIllegalFrameType, mac_pib_tag::privateNoDataAfterAssocReq, mac_pib_tag::privateVirtualPANs, status, and tal_pib.
void mlme_gts_conf | ( | uint8_t * | m | ) |
References mlme_gts_conf_tag::GtsChar, mlme_gts_conf_tag::status, and usr_mlme_gts_conf().
void mlme_gts_ind | ( | uint8_t * | m | ) |
References mlme_gts_ind_tag::DeviceAddr, mlme_gts_ind_tag::GtsChar, and usr_mlme_gts_ind().
void mlme_gts_request | ( | uint8_t * | m | ) |
References aGTSDescPersistenceTime, frame_info_tag::buffer_header, convert_16_bit_to_byte_array(), convert_spec_16_bit_to_byte_array(), CSMA_SLOTTED, mlme_gts_req_tag::DeviceShortAddr, FCF_ACK_REQUEST, FCF_FRAMETYPE_MAC_CMD, FCF_PAN_ID_COMPRESSION, FCF_SET_DEST_ADDR_MODE, FCF_SET_FRAMETYPE, FCF_SET_SOURCE_ADDR_MODE, FCF_SHORT_ADDR, GTS_ALLOCATE, GTS_DEALLOCATE, GTS_REQ_PAYLOAD_LEN, GTS_STATE_IDLE, GTS_STATE_REQ_SENT, mlme_gts_req_tag::GtsChar, gts_char_tag::GtsCharType, gts_char_tag::GtsDirection, gts_char_tag::GtsLength, GTSREQUEST, MAC_ASSOCIATED, mac_pib_tag::mac_CoordShortAddress, mac_dev_gts_table, mac_pib_tag::mac_DSN, mac_gen_mlme_gts_conf(), mac_gts_allocate(), mac_gts_deallocate(), mac_pib_tag::mac_GTSPermit, MAC_INVALID_PARAMETER, MAC_NO_DATA, MAC_NO_SHORT_ADDR_VALUE, MAC_NO_SHORT_ADDRESS, MAC_PAN_COORD_STARTED, mac_pib, mac_state, MAC_SUCCESS, mac_sync_state, MAC_SYNC_TRACKING_BEACON, mac_trx_wakeup(), MAKE_MAC_BUSY, frame_info_tag::mpdu, frame_info_tag::msg_type, tal_pib, tal_tx_frame(), and transmit_frame().
Setting of MAC PIB attributes via functional access.
In case the highest stack layer is above MAC (e.g. NWK or even higher), it is not efficient to change PIB attributes using the standard request / confirm primitive concept via the NHLE_MAC queue. In order to allow a more efficient way to change PIB attributes residing in MAC or TAL, this function replaces the standard primitive access via a functional interface.
An additional parameter allows for forcing the transceiver back to sleep after PIB setting. Otherwise the transceiver will stay awake (if it has been woken up before). This enables the higher layer to change several PIB attributes without waking up the transceiver and putting it back to sleep several times.
attribute | PIB attribute to be set |
attribute_index | Index of the PIB attribute to be set |
attribute_value | Attribute value to be set |
set_trx_to_sleep | Set TRX back to sleep after this PIB access if it was before starting this TRX access. Otherwise the transceiver state will remain as it is, i.e. in case the transceiver was woken up, it will stay awake. The default value for just changing one variable is true, i.e. the transceiver will be put back to sleep if it has been woken up. |
References aMaxBeaconPayloadLength, mac_pib_tag::mac_AutoRequest, mac_pib_tag::mac_BattLifeExtPeriods, mac_pib_tag::mac_CoordExtendedAddress, mac_pib_tag::mac_CoordShortAddress, mac_pib_tag::mac_DSN, mac_pib_tag::mac_GTSPermit, MAC_INVALID_INDEX, MAC_INVALID_PARAMETER, mac_pib_tag::mac_MaxFrameTotalWaitTime, mac_pib, mac_pib_tag::mac_ResponseWaitTime, mac_pib_tag::mac_RxOnWhenIdle, mac_pib_tag::mac_SecurityEnabled, mac_sleep_trans(), MAC_SUCCESS, mac_trx_wakeup(), MAC_UNSUPPORTED_ATTRIBUTE, macAckWaitDuration, macAssociatedPANCoord, macAssociationPermit, macAutoRequest, macBattLifeExt, macBattLifeExtPeriods, macBeaconOrder, macBeaconPayload, macBeaconPayloadLength, macBSN, macCoordExtendedAddress, macCoordShortAddress, macDSN, macGTSPermit, macIeeeAddress, macMaxBE, macMaxCSMABackoffs, macMaxFrameRetries, macMaxFrameTotalWaitTime, macMinBE, macPANCoordExtendedAddress, macPANCoordShortAddress, macPANId, macPrivateCCAFailure, macPrivateDisableACK, macPrivateIllegalFrameType, macPrivateNoDataAfterAssocReq, macPrivateVirtualPANs, macPromiscuousMode, macResponseWaitTime, macRxOnWhenIdle, macSecurityEnabled, macShortAddress, macSuperframeOrder, macTransactionPersistenceTime, PHY_RX_ON, phyCCAMode, phyCurrentChannel, phyCurrentPage, phyTransmitPower, mac_pib_tag::privateIllegalFrameType, mac_pib_tag::privateNoDataAfterAssocReq, mac_pib_tag::privateVirtualPANs, recalc_macMaxFrameTotalWaitTime(), SLEEP_MODE_1, status, tal_pib_set(), tal_rx_enable(), TAL_TRX_ASLEEP, tal_trx_sleep(), and tal_trx_wakeup().
Referenced by mlme_set_request().
queue_t mac_nhle_q |
Queue used by MAC for communication to next higher layer.
Referenced by flush_queues(), gen_mlme_start_conf(), mac_gen_mcps_data_conf(), mac_gen_mlme_gts_conf(), mac_gts_table_update(), mac_process_data_frame(), mac_process_gts_request(), mac_process_tal_tx_status(), mac_ready_to_sleep(), mac_send_gts_ind(), mlme_set_request(), parse_mpdu(), send_reset_conf(), wpan_init(), and wpan_task().
queue_t nhle_mac_q |
NHLE to MAC queue in which NHLE pushes all the requests to the MAC layer.
Referenced by flush_queues(), mac_init(), mac_ready_to_sleep(), mac_task(), wpan_mcps_data_req(), wpan_mlme_reset_req(), and wpan_mlme_set_req().