This module provides implementation of MQTT wrapper for Paho MQTT.
MQ Telemetry Transport (MQTT) is a lightweight broker-based publish/subscribe messaging protocol designed to be open, simple, lightweight and easy to implement.
Revision history 2014/10/07 : Initial draft. (v1.0)
Data Structures | |
struct | mqtt_client_pool |
struct | mqtt_config |
MQTT configuration structure. More... | |
union | mqtt_data |
Structure of the MQTT callback. More... | |
struct | mqtt_data_connected |
Structure of the MQTT_CALLBACK_CONNECTED callback. More... | |
struct | mqtt_data_disconnected |
Structure of the MQTT_CALLBACK_DISCONNECTED callback. More... | |
struct | mqtt_data_ping |
Structure of the MQTT_CALLBACK_SENT_PING callback. More... | |
struct | mqtt_data_published |
Structure of the MQTT_CALLBACK_PUBLISHED callback. More... | |
struct | mqtt_data_sock_connected |
Structure of the MQTT_CALLBACK_SOCK_CONNECTED callback. More... | |
struct | mqtt_data_subscribed |
Structure of the MQTT_CALLBACK_SUBSCRIBED callback. More... | |
struct | mqtt_data_unsubscribed |
Structure of the MQTT_CALLBACK_UNSUBSCRIBED callback. More... | |
struct | mqtt_module |
Structure of MQTT connection instance. More... | |
Typedefs | |
typedef void(* | mqtt_callback_t )(struct mqtt_module *module_inst, int type, union mqtt_data *data) |
Callback interface of MQTT service. More... | |
Enumerations | |
enum | mqtt_callback_type { MQTT_CALLBACK_SOCK_CONNECTED, MQTT_CALLBACK_CONNECTED, MQTT_CALLBACK_PUBLISHED, MQTT_CALLBACK_SUBSCRIBED, MQTT_CALLBACK_UNSUBSCRIBED, MQTT_CALLBACK_DISCONNECTED, MQTT_CALLBACK_SENT_PING } |
A type of MQTT callback. More... | |
enum | mqtt_conn_result { MQTT_CONN_RESULT_ACCEPT = 0, MQTT_CONN_RESULT_UNACCEPTABLE_VERSION, MQTT_CONN_RESULT_ID_REJECTED, MQTT_CONN_RESULT_SERVER_UNAVAILABLE, MQTT_CONN_RESULT_BAD_USER_NAME, MQTT_CONN_RESULT_NOT_AUTHORIZED } |
Connect return code. More... | |
Functions | |
int | mqtt_connect (struct mqtt_module *const module, const char *host) |
Connect to specific MQTT broker server. More... | |
int | mqtt_connect_broker (struct mqtt_module *const module, uint8_t clean_session, const char *id, const char *password, const char *client_id, const char *will_topic, const char *will_msg, uint32_t will_msg_len, uint8_t will_qos, uint8_t will_retain) |
Send MQTT connect message to broker server with MQTT parameter. More... | |
int | mqtt_deinit (struct mqtt_module *const module) |
Termivate MQTT service. More... | |
int | mqtt_disconnect (struct mqtt_module *const module, int force_close) |
Send disconnect message to MQTT broker server and closing socket. More... | |
void | mqtt_get_config_defaults (struct mqtt_config *const config) |
Get default configuration of SW timer. More... | |
int | mqtt_init (struct mqtt_module *module, struct mqtt_config *config) |
Initialize MQTT service. More... | |
int | mqtt_publish (struct mqtt_module *const module, const char *topic, const char *msg, uint32_t msg_len, uint8_t qos, uint8_t retain) |
Send publish message to MQTT broker server. More... | |
int | mqtt_register_callback (struct mqtt_module *const module, mqtt_callback_t callback) |
Register and enable the callback. More... | |
void | mqtt_socket_event_handler (SOCKET sock, uint8_t msg_type, void *msg_data) |
Event handler of socket event. More... | |
void | mqtt_socket_resolve_handler (uint8_t *doamin_name, uint32_t server_ip) |
Event handler of gethostbyname. More... | |
int | mqtt_subscribe (struct mqtt_module *const module, const char *topic, uint8_t qos, messageHandler msgHandler) |
Send subscribe message to MQTT broker server. More... | |
int | mqtt_unregister_callback (struct mqtt_module *const module) |
Unregister callback. More... | |
int | mqtt_unsubscribe (struct mqtt_module *const module, const char *topic) |
Send unsubscribe message to MQTT broker server. More... | |
int | mqtt_yield (struct mqtt_module *module, int timeout_ms) |
Poll for published frames. More... | |
Variables | |
struct mqtt_client_pool | mqttClientPool [MQTT_MAX_CLIENTS] |
Static Client Pool Allocation. More... | |
typedef void(* mqtt_callback_t)(struct mqtt_module *module_inst, int type, union mqtt_data *data) |
Callback interface of MQTT service.
enum mqtt_callback_type |
A type of MQTT callback.
enum mqtt_conn_result |
Connect return code.
The connect return code is sent in the variable header of a CONNACK message.
int mqtt_connect | ( | struct mqtt_module *const | module, |
const char * | host | ||
) |
Connect to specific MQTT broker server.
This function is responsible only connect the socket. If operation of this function is complete, MQTT_CALLBACK_SOCK_CONNECTED event will be sent through MQTT callback.
[in] | module_inst | Instance of MQTT module. |
[in] | host | URL of MQTT broker server. |
References mqtt_module::callback, mqtt_module::config, ConnectNetwork(), MQTT_CALLBACK_SOCK_CONNECTED, mqtt_module::network, mqtt_config::port, mqtt_data_sock_connected::result, mqtt_data::sock_connected, and mqtt_config::tls.
Referenced by mqtt_callback(), PROCESS_THREAD(), and wifi_callback().
int mqtt_connect_broker | ( | struct mqtt_module *const | module, |
uint8_t | clean_session, | ||
const char * | id, | ||
const char * | password, | ||
const char * | client_id, | ||
const char * | will_topic, | ||
const char * | will_msg, | ||
uint32_t | will_msg_len, | ||
uint8_t | will_qos, | ||
uint8_t | will_retain | ||
) |
Send MQTT connect message to broker server with MQTT parameter.
If operation of this function is complete, MQTT_CALLBACK_CONNECTED event will be sent through MQTT callback.
[in] | module_inst | Instance of MQTT module. |
[in] | clean_session | If this value set to 1, Broker server store the previous subscribed informations after disconnected. |
[in] | id | ID of user. |
[in] | password | Password of user. |
[in] | client_id | Client ID of this connection. |
[in] | will_topic | A MQTT topic that will be sent to subscribers when this connection is disconnected. |
[in] | will_msg | A MQTT payload that will be sent to subscribers when this connection is disconnected. |
[in] | will_qos | QOS level of will message. |
[in] | will_retain | Whether broker server will be store MQTT will message or not. |
References mqtt_module::callback, mqtt_module::client, mqtt_data::connected, mqtt_module::isConnected, MQTT_CALLBACK_CONNECTED, MQTTConnect(), MQTTPacket_connectData_initializer, and mqtt_data_connected::result.
Referenced by mqtt_callback().
int mqtt_deinit | ( | struct mqtt_module *const | module | ) |
Termivate MQTT service.
[in] | module | Module instance of MQTT. |
References deAllocateClient(), FAILURE, mqtt_module::isConnected, mqtt_disconnect(), and SUCCESS.
int mqtt_disconnect | ( | struct mqtt_module *const | module, |
int | force_close | ||
) |
Send disconnect message to MQTT broker server and closing socket.
If operation of this function is complete, MQTT_CALLBACK_DISCONNECTED event will be sent through MQTT callback.
[in] | module_inst | Instance of MQTT module. |
[in] | force_close | If this flag is set, MQTT service will be close the socket immediately. |
References mqtt_module::callback, mqtt_module::client, mqtt_data::disconnected, mqtt_module::isConnected, MQTT_CALLBACK_DISCONNECTED, MQTTDisconnect(), and mqtt_data_disconnected::reason.
Referenced by mqtt_deinit(), PROCESS_THREAD(), and wifi_callback().
void mqtt_get_config_defaults | ( | struct mqtt_config *const | config | ) |
Get default configuration of SW timer.
[in] | config | Pointer of configuration structure which will be used in the module. |
References mqtt_config::keep_alive, NULL, mqtt_config::port, mqtt_config::read_buffer, mqtt_config::read_buffer_size, mqtt_config::send_buffer, mqtt_config::send_buffer_size, and mqtt_config::tls.
Referenced by configure_mqtt().
int mqtt_init | ( | struct mqtt_module * | module, |
struct mqtt_config * | config | ||
) |
Initialize MQTT service.
[in] | module | Module instance of MQTT. |
[in] | config | Pointer of configuration structure which will be used in the module. |
References allocateClient(), mqtt_module::client, mqtt_module::config, FAILURE, mqtt_config::keep_alive, MQTTClientInit(), mqtt_module::network, NetworkInit(), NULL, mqtt_config::read_buffer, mqtt_config::read_buffer_size, mqtt_config::send_buffer, mqtt_config::send_buffer_size, and SUCCESS.
Referenced by configure_mqtt().
int mqtt_publish | ( | struct mqtt_module *const | module, |
const char * | topic, | ||
const char * | msg, | ||
uint32_t | msg_len, | ||
uint8_t | qos, | ||
uint8_t | retain | ||
) |
Send publish message to MQTT broker server.
If operation of this function is complete, MQTT_CALLBACK_PUBLISHED event will be sent through MQTT callback.
[in] | module_inst | Instance of MQTT module. |
[in] | topic | Topic of this MQTT message. |
[in] | msg | Payload of this MQTT message. |
[in] | msg_len | Payload size of this MQTT message. |
[in] | qos | QOS level of this MQTT message. (0 <= qos <= 2) |
[in] | retain | Whether broker server will be store this MQTT message or not. |
References mqtt_module::callback, mqtt_module::client, MQTT_CALLBACK_PUBLISHED, MQTTPublish(), NULL, MQTTMessage::payload, MQTTMessage::payloadlen, MQTTMessage::qos, and MQTTMessage::retained.
Referenced by check_usart_buffer(), and PROCESS_THREAD().
int mqtt_register_callback | ( | struct mqtt_module *const | module, |
mqtt_callback_t | callback | ||
) |
Register and enable the callback.
[in] | module_inst | Instance of MQTT module. |
[in] | callback | Callback entry for the MQTT module. |
References callback, mqtt_module::callback, FAILURE, and SUCCESS.
Referenced by configure_mqtt().
void mqtt_socket_event_handler | ( | SOCKET | sock, |
uint8_t | msg_type, | ||
void * | msg_data | ||
) |
Event handler of socket event.
[in] | sock | Socket descriptor. |
[in] | msg_type | Event type. |
[in] | msg_data | Structure of socket event. |
References tcpClientSocketEventHandler().
Referenced by socket_event_handler().
void mqtt_socket_resolve_handler | ( | uint8_t * | doamin_name, |
uint32_t | server_ip | ||
) |
Event handler of gethostbyname.
[in] | doamin_name | Domain name. |
[in] | server_ip | Server IP. |
References dnsResolveCallback().
Referenced by socket_resolve_handler().
int mqtt_subscribe | ( | struct mqtt_module *const | module, |
const char * | topic, | ||
uint8_t | qos, | ||
messageHandler | msgHandler | ||
) |
Send subscribe message to MQTT broker server.
If operation of this function is complete, MQTT_CALLBACK_SUBSCRIBED event will be sent through MQTT callback.
[in] | module_inst | Instance of MQTT module. |
[in] | topic | A topic which will be received. |
[in] | qos | QOS level of received publish message. |
References mqtt_module::callback, mqtt_module::client, MQTT_CALLBACK_SUBSCRIBED, MQTTSubscribe(), and NULL.
Referenced by mqtt_callback(), and PROCESS_THREAD().
int mqtt_unregister_callback | ( | struct mqtt_module *const | module | ) |
Unregister callback.
[in] | module_inst | Instance of MQTT module. |
References mqtt_module::callback, FAILURE, NULL, and SUCCESS.
int mqtt_unsubscribe | ( | struct mqtt_module *const | module, |
const char * | topic | ||
) |
Send unsubscribe message to MQTT broker server.
If operation of this function is complete, MQTT_CALLBACK_UNSUBSCRIBED event will be sent through MQTT callback.
[in] | module_inst | Instance of MQTT module. |
[in] | topic | A topic that want to be removed. |
References mqtt_module::callback, mqtt_module::client, MQTT_CALLBACK_SUBSCRIBED, MQTTUnsubscribe(), and NULL.
int mqtt_yield | ( | struct mqtt_module * | module, |
int | timeout_ms | ||
) |
Poll for published frames.
[in] | module_inst | Instance of MQTT module. |
[in] | timeout_ms | time limit for polling. |
References mqtt_module::client, and MQTTYield().
Referenced by main().
struct mqtt_client_pool mqttClientPool[MQTT_MAX_CLIENTS] |
Static Client Pool Allocation.
Static Client Pool Allocation.
and its subsidiaries (Microchip). All rights reserved.
You are permitted to use the software and its derivatives with Microchip products.
SOFTWARE AND DOCUMENTATION ARE PROVIDED “AS IS” WITHOUT WARRANTY OF ANY KIND, EITHER EXPRESS OR IMPLIED, INCLUDING WITHOUT LIMITATION, ANY WARRANTY OF MERCHANTABILITY, TITLE, NON-INFRINGEMENT AND FITNESS FOR A PARTICULAR PURPOSE. IN NO EVENT SHALL MICROCHIP OR ITS LICENSORS BE LIABLE OR OBLIGATED UNDER CONTRACT, NEGLIGENCE, STRICT LIABILITY, CONTRIBUTION, BREACH OF WARRANTY, OR OTHER LEGAL OR EQUITABLE THEORY FOR ANY DIRECT OR INDIRECT DAMAGES OR EXPENSES INCLUDING BUT NOT LIMITED TO ANY INCIDENTAL, SPECIAL, INDIRECT OR CONSEQUENTIAL DAMAGES, OR OTHER SIMILAR COSTS. TO THE FULLEST EXTENT ALLOWED BY LAW, MICROCHIP AND ITS LICENSORS LIABILITY WILL NOT EXCEED THE AMOUNT OF FEES, IF ANY, THAT YOU PAID DIRECTLY TO MICROCHIP TO USE THIS SOFTWARE. MICROCHIP PROVIDES THIS SOFTWARE CONDITIONALLY UPON YOUR ACCEPTANCE OF THESE TERMS.
THIRD PARTY SOFTWARE: Notwithstanding anything to the contrary, any third party software accompanying this software is subject to the terms and conditions of the third party’s license agreement or open source software license. To the extent required by third party or open source licenses covering such third party software, the terms of such license will apply in lieu of the terms provided herein. To the extent the terms of such third party licenses prohibit any of the restrictions described herein, such restrictions will not apply to such third party software. THIRD PARTY SOFTWARE IS SUBJECT TO THE FOREGOING WARRANTY DISCLAIMER AND LIMIT ON LIABILITY PROVIDED IN THE PARAGRAPH ABOVE.
Referenced by isMQTTSocket().