Macros | |
#define | WIFI_1X_TLS_HS_FLAGS_DEFAULT |
#define | WIFI_1X_TLS_HS_FLAGS_PEER_AUTH NBIT1 |
#define | WIFI_1X_TLS_HS_FLAGS_PEER_CERTTIMECHECK NBIT2 |
#define | WIFI_1X_TLS_HS_FLAGS_REQUIRE_TIME NBIT3 |
#define | WIFI_1X_TLS_HS_FLAGS_SESSION_CACHING NBIT4 |
#define | WIFI_1X_TLS_HS_FLAGS_SPECIFY_ROOTCERT NBIT6 |
Functions | |
static sint8 | legacy_connect_prepare_msg (tstrM2mWifiConnHdr *pstrConnHdr, tstrM2mWifiConnectLegacy_1_2 *pstrConnect) |
static sint8 | m2m_validate_ap_parameters (CONST tstrM2MAPModeConfig *pstrM2MAPModeConfig) |
static sint8 | m2m_validate_scan_options (tstrM2MScanOption *ptstrM2MScanOption) |
static void | m2m_wifi_cb (uint8 u8OpCode, uint16 u16DataSize, uint32 u32Addr) |
static sint8 | m2m_wifi_connect_prepare_msg (tenuCredStoreOption enuCredStoreOption, tenuM2mSecType enuAuthType, uint16 u16AuthSize, tstrNetworkId *pstrNetworkId, tstrM2mWifiConnHdr *pstrWifiConn) |
uint32 | m2m_wifi_get_chipId (void) |
Get the WINC Chip ID. More... | |
sint8 | m2m_wifi_p2p (uint8 u8Channel) |
sint8 | m2m_wifi_p2p_disconnect (void) |
sint8 | m2m_wifi_wps (uint8 u8TriggerType, const char *pcPinNumber) |
Asynchronous API to engage the WINC Wi-Fi Protected Setup (enrollee) function. More... | |
sint8 | m2m_wifi_wps_disable (void) |
Asynchronous API that disables Wi-Fi Protected Setup mode in the WINC. More... | |
Variables | |
static uint8 | gau81xRootSha1 [20] = {0} |
static tpfAppWifiCb | gpfAppWifiCb = NULL |
static uint32 | gu321xTlsHsFlags = WIFI_1X_TLS_HS_FLAGS_DEFAULT |
static volatile uint8 | gu8ChNum |
#define WIFI_1X_TLS_HS_FLAGS_DEFAULT |
#define WIFI_1X_TLS_HS_FLAGS_PEER_AUTH NBIT1 |
Referenced by m2m_wifi_1x_get_option(), and m2m_wifi_1x_set_option().
#define WIFI_1X_TLS_HS_FLAGS_PEER_CERTTIMECHECK NBIT2 |
Referenced by m2m_wifi_1x_get_option(), and m2m_wifi_1x_set_option().
#define WIFI_1X_TLS_HS_FLAGS_REQUIRE_TIME NBIT3 |
Referenced by m2m_wifi_1x_get_option(), and m2m_wifi_1x_set_option().
#define WIFI_1X_TLS_HS_FLAGS_SESSION_CACHING NBIT4 |
Referenced by m2m_wifi_1x_get_option(), and m2m_wifi_1x_set_option().
#define WIFI_1X_TLS_HS_FLAGS_SPECIFY_ROOTCERT NBIT6 |
Referenced by m2m_wifi_1x_get_option(), and m2m_wifi_1x_set_option().
|
static |
References tstrM2mConnCredCmn::au8Ssid, tstrM2mWifiConnectLegacy_1_2::au8SSID, M2M_CRED_ENCRYPT_FLAG, M2M_CRED_STORE_FLAG, M2M_ERR_FAIL, m2m_memcpy(), m2m_memset(), M2M_SUCCESS, M2M_WIFI_CONN_BSSID_FLAG, tstrM2mWifiConnHdr::strConnCredCmn, tstrM2mWifiConnHdr::strConnCredHdr, tstrM2mWifiConnectLegacy_1_2::strSec, tstrM2mWifiConnectLegacy_1_2::u16Ch, tstrM2mConnCredCmn::u8AuthType, tstrM2mConnCredHdr::u8Channel, tstrM2mConnCredHdr::u8CredStoreFlags, tstrM2mWifiConnectLegacy_1_2::u8NoSaveCred, tstrM2mConnCredCmn::u8Options, tstrM2MWifiSecInfoLegacy_1_2::u8SecType, and tstrM2mConnCredCmn::u8SsidLen.
Referenced by m2m_wifi_connect_open(), m2m_wifi_connect_psk(), and m2m_wifi_connect_wep().
|
static |
References M2M_ERR, M2M_ERR_FAIL, M2M_MAX_SSID_LEN, m2m_strlen(), M2M_SUCCESS, M2M_WIFI_CH_1, M2M_WIFI_CH_14, M2M_WIFI_SEC_OPEN, M2M_WIFI_SEC_WEP, NULL, WEP_104_KEY_STRING_SIZE, WEP_40_KEY_STRING_SIZE, and WEP_KEY_MAX_INDEX.
Referenced by m2m_wifi_enable_ap_ext(), and m2m_wifi_start_provision_mode_ext().
|
static |
References BYTE_0, BYTE_1, BYTE_2, BYTE_3, tstrM2mBleApiMsg::data, gpfAppWifiCb, gu8ChNum, hif_receive(), M2M_ERR, M2M_INFO, m2m_memcpy(), m2m_memset(), M2M_SUCCESS, M2M_WIFI_REQ_DHCP_CONF, M2M_WIFI_REQ_WPS, M2M_WIFI_REQRSP_DELETE_APID, M2M_WIFI_RESP_BLE_API_RECV, M2M_WIFI_RESP_CLIENT_INFO, M2M_WIFI_RESP_CON_STATE_CHANGED, M2M_WIFI_RESP_CONN_INFO, M2M_WIFI_RESP_CURRENT_RSSI, M2M_WIFI_RESP_DEFAULT_CONNECT, M2M_WIFI_RESP_ETHERNET_RX_PACKET, M2M_WIFI_RESP_GET_PRNG, M2M_WIFI_RESP_GET_SYS_TIME, M2M_WIFI_RESP_IP_CONFLICT, M2M_WIFI_RESP_MEMORY_RECOVER, M2M_WIFI_RESP_PROVISION_INFO, M2M_WIFI_RESP_SCAN_DONE, M2M_WIFI_RESP_SCAN_RESULT, M2M_WIFI_RESP_SET_GAIN_TABLE, NULL, tstrPrng::pu8RngBuff, rx_buf, tstrM2mIpCtrlBuf::u16DataSize, tstrM2mBleApiMsg::u16Len, tstrM2mIpRsvdPkt::u16PktOffset, tstrM2mIpRsvdPkt::u16PktSz, tstrPrng::u16PrngSize, tstrM2mIpCtrlBuf::u16RemainingDataSize, tstrM2mWifiStateChanged::u8CurrState, and tstrM2mScanDone::u8NumofCh.
Referenced by m2m_wifi_init_start().
|
static |
References tstrM2mConnCredCmn::au8Bssid, tstrM2mConnCredCmn::au8Ssid, tstrNetworkId::enuChannel, M2M_CRED_ENCRYPT_FLAG, M2M_CRED_STORE_FLAG, M2M_ERR_FAIL, M2M_ERR_INVALID_ARG, M2M_MAC_ADDRES_LEN, M2M_MAX_SSID_LEN, m2m_memcpy(), m2m_memset(), M2M_SUCCESS, M2M_WIFI_CH_1, M2M_WIFI_CH_14, M2M_WIFI_CH_ALL, M2M_WIFI_CONN_BSSID_FLAG, M2M_WIFI_NUM_AUTH_TYPES, M2M_WIFI_SEC_INVALID, NULL, tstrNetworkId::pu8Bssid, tstrNetworkId::pu8Ssid, ret, tstrM2mWifiConnHdr::strConnCredCmn, tstrM2mWifiConnHdr::strConnCredHdr, tstrM2mConnCredHdr::u16CredSize, tstrM2mConnCredCmn::u8AuthType, tstrM2mConnCredHdr::u8Channel, tstrM2mConnCredHdr::u8CredStoreFlags, tstrM2mConnCredCmn::u8Options, tstrNetworkId::u8SsidLen, tstrM2mConnCredCmn::u8SsidLen, WIFI_CRED_DONTSAVE, WIFI_CRED_SAVE_ENCRYPTED, and WIFI_CRED_SAVE_UNENCRYPTED.
Referenced by m2m_wifi_connect_1x_mschap2(), m2m_wifi_connect_1x_tls(), m2m_wifi_connect_open(), m2m_wifi_connect_psk(), and m2m_wifi_connect_wep().
uint32 m2m_wifi_get_chipId | ( | void | ) |
Get the WINC Chip ID.
Synchronous API to obtain the firmware WINC chip ID.
References nmi_get_chipid().
sint8 m2m_wifi_p2p_disconnect | ( | void | ) |
References hif_send(), M2M_REQ_GROUP_WIFI, M2M_SUCCESS, M2M_WIFI_REQ_DISABLE_P2P, NULL, and ret.
Asynchronous API to engage the WINC Wi-Fi Protected Setup (enrollee) function.
Asynchronous API to engage the WINC IC's Wi-Fi Protected Setup (enrollee) function.
This function can be called to make the WINC enter WPS (Wi-Fi Protected Setup) mode. The result is passed to the Wi-Fi notification callback with the event @ref M2M_WIFI_REQ_WPS.
[in] | u8TriggerType | WPS Trigger method. This may be:
|
[in] | pcPinNumber | Valid only if the u8TriggerType is WPS_PIN_TRIGGER, this parameter contains the PIN number. The number must follow the format as given in the WSC1.0 specification. |
The code snippet shows an example of how wi-fi WPS is triggered .
This function is called for the WINC to enter the WPS (Wi-Fi Protected Setup) mode. The result is passed to the Wi-Fi notification callback with the event @ref M2M_WIFI_REQ_WPS.
[in] | u8TriggerType | WPS Trigger method. This may be:
|
[in] | pcPinNumber | PIN number for WPS PIN method. It is not used if the trigger type is WPS_PBC_TRIGGER. It must follow the rules stated by the WPS standard. |
The code snippet shows an example of how wi-fi WPS is triggered .
Referenced by btn_press(), and main().
Asynchronous API that disables Wi-Fi Protected Setup mode in the WINC.
Stops the ongoing WPS session.
|
static |
|
static |
Referenced by m2m_wifi_cb(), and m2m_wifi_init_start().
|
static |
|
static |
Referenced by m2m_wifi_cb(), and m2m_wifi_get_num_ap_found().