Httpd server.
Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.
Data Structures | |
struct | HttpCGI |
Macros | |
#define | CGI_LED_CMD_KEY "set" |
#define | CGI_LED_ID_KEY "n" |
#define | CGI_MATCH_EXT 2 |
Select item in table if the extention match. More... | |
#define | CGI_MATCH_NAME 3 |
Select item in table if the string is content. More... | |
#define | CGI_MATCH_NONE 0 |
#define | CGI_MATCH_WORD 1 |
Select item in table only if string match. More... | |
#define | CONFIG_AFSK_TX_BUFLEN 1024 |
FIFO tx buffer. More... | |
#define | HTTP_DEFAULT_PAGE "index.html" |
Typedefs | |
typedef int(* | http_handler_t )(const char *name, char *revc_buf, size_t revc_len) |
typedef struct HttpCGI | HttpCGI |
Enumerations | |
enum | { HTTP_CONTENT_JSON = 0, HTTP_CONTENT_HTML, HTTP_CONTENT_CSS, HTTP_CONTENT_JS, HTTP_CONTENT_PNG, HTTP_CONTENT_JPEG, HTTP_CONTENT_GIF, HTTP_CONTENT_PLAIN, HTTP_CONTENT_CNT } |
HTTP content type enum. More... | |
Functions | |
void | httpd_init (void) |
HTTP server init. More... | |
#define CGI_LED_CMD_KEY "set" |
Referenced by cgi_SetLed().
#define CGI_LED_ID_KEY "n" |
Referenced by cgi_SetLed().
#define CGI_MATCH_EXT 2 |
Select item in table if the extention match.
Referenced by cgi_search().
#define CGI_MATCH_NAME 3 |
Select item in table if the string is content.
Referenced by cgi_search().
#define CGI_MATCH_NONE 0 |
#define CGI_MATCH_WORD 1 |
Select item in table only if string match.
#define CONFIG_AFSK_TX_BUFLEN 1024 |
FIFO tx buffer.
#define HTTP_DEFAULT_PAGE "index.html" |
Referenced by http_recv().
typedef int(* http_handler_t)(const char *name, char *revc_buf, size_t revc_len) |
anonymous enum |
void httpd_init | ( | void | ) |
HTTP server init.
References http_accept(), httpd_cgi_init(), led_socket, led_socket_callback(), memb_init(), NULL, tcp_listen(), udp_socket_bind(), udp_socket_register(), and UIP_HTONS.
Referenced by main(), and PROCESS_THREAD().