Microchip® Advanced Software Framework

oled1_event_groups_xpro_example/demotasks.c File Reference

FreeRTOS demo task implementations.

Copyright (c) 2014-2018 Microchip Technology Inc. and its subsidiaries.

#include <asf.h>
#include <conf_demo.h>
#include "demotasks.h"

Macros

Task configuration
#define UART_TASK_PRIORITY   (tskIDLE_PRIORITY + 3)
 
#define UART_TASK_DELAY   (10 / portTICK_RATE_MS)
 
#define MAIN_TASK_PRIORITY   (tskIDLE_PRIORITY + 2)
 
#define MAIN_TASK_DELAY   (100 / portTICK_RATE_MS)
 
#define GRAPH_TASK_PRIORITY   (tskIDLE_PRIORITY + 1)
 
#define GRAPH_TASK_DELAY   (50 / portTICK_RATE_MS)
 
#define TERMINAL_TASK_PRIORITY   (tskIDLE_PRIORITY + 1)
 
#define TERMINAL_TASK_DELAY   (1000 / portTICK_RATE_MS)
 
#define ABOUT_TASK_PRIORITY   (tskIDLE_PRIORITY + 1)
 
#define ABOUT_TASK_DELAY   (33 / portTICK_RATE_MS)
 
Event bits definition
#define EVENT_DISPLAY_INIT   (0x01UL)
 
#define EVENT_DISPLAY_GRAPH   (0x02UL)
 
#define EVENT_DISPLAY_TERMINAL   (0x04UL)
 
#define EVENT_DISPLAY_ABOUT   (0x08UL)
 
#define EVENT_ALL_BITS   (0x0FUL)
 

Functions

static void cdc_rx_handler (uint8_t instance)
 Interrupt handler for reception from EDBG Virtual COM Port. More...
 
void demotasks_init (void)
 Initialize tasks and resources for demo. More...
 
Tasks for demo
static void main_task (void *params)
 Main demo task. More...
 
static void graph_task (void *params)
 Graph task. More...
 
static void terminal_task (void *params)
 Terminal task. More...
 
static void about_task (void *params)
 About task. More...
 
static void uart_task (void *params)
 UART task. More...
 

Menu and display configuration

#define MENU_HEIGHT   8
 Height of menu bar. More...
 
#define MENU_ITEM_WIDTH   (((GFX_MONO_LCD_WIDTH - (MENU_NUM_ITEMS - 1))) / MENU_NUM_ITEMS)
 Width per menu item. More...
 
#define CANVAS_HEIGHT   ((GFX_MONO_LCD_HEIGHT / 2) - (MENU_HEIGHT + 1))
 Height of area in which to draw content. More...
 
#define CANVAS_WIDTH   (GFX_MONO_LCD_WIDTH)
 Width of area in which to draw content. More...
 
#define CANVAS_GRAPH_Y_OFFSET   (GFX_MONO_LCD_HEIGHT / 2)
 Offset of Y-coordinate for display buffer of graph. More...
 
#define TERMINAL_LINES   (1 + ((CANVAS_HEIGHT - SYSFONT_HEIGHT) / (SYSFONT_HEIGHT + 1)))
 Character lines on display. More...
 
#define TERMINAL_COLUMNS   (CANVAS_WIDTH / SYSFONT_WIDTH)
 Character columns on display. More...
 
#define TERMINAL_BUFFER_LINES   (1 + TERMINAL_LINES)
 Character lines in terminal buffer. More...
 
#define TERMINAL_BUFFER_COLUMNS   (1 + TERMINAL_COLUMNS)
 Character columns in terminal buffer. More...
 
enum  menu_items {
  MENU_ITEM_GRAPH,
  MENU_ITEM_TERMINAL,
  MENU_ITEM_ABOUT,
  MENU_NUM_ITEMS,
  MENU_ITEM_GRAPH,
  MENU_ITEM_TERMINAL,
  MENU_ITEM_ABOUT,
  MENU_NUM_ITEMS,
  MENU_ITEM_GRAPH,
  MENU_ITEM_TERMINAL,
  MENU_ITEM_ABOUT,
  MENU_NUM_ITEMS,
  MENU_ITEM_GRAPH,
  MENU_ITEM_TERMINAL,
  MENU_ITEM_ABOUT,
  MENU_NUM_ITEMS
}
 Available selections in menu. More...
 

Global constants and variables

static const char menu_items_text [MENU_NUM_ITEMS][6]
 Labels for menu items. More...
 
static const char about_text []
 Text to display on about screen. More...
 
static struct usart_module cdc_usart
 Instance for Embedded Debugger (EDBG) Virtual COM Port driver. More...
 
static uint8_t graph_noise = 128
 Pseudo-random noise for graph task. More...
 
static uint8_t terminal_buffer [TERMINAL_BUFFER_LINES][TERMINAL_BUFFER_COLUMNS]
 Buffer for terminal text. More...
 
static uint8_t terminal_line_offset
 Index of latest terminal line (first to be printed) More...
 
static xQueueHandle terminal_in_queue
 Queue for incoming terminal characters. More...
 
static xSemaphoreHandle display_mutex
 Semaphore to signal busy display. More...
 
static xSemaphoreHandle terminal_mutex
 Semaphore to signal busy terminal buffer. More...
 
static EventGroupHandle_t event_group = NULL
 The event group used. More...
 
static OLED1_CREATE_INSTANCE (oled1, OLED1_EXT_HEADER)
 Instance for OLED1 Xplained Pro LED and button driver. More...
 

static void about_task ( void *  params)
static

About task.

This task prints a short text about the demo, with a simple zooming animation.

Parameters
paramsParameters for the task. (Not used.)

References ABOUT_TASK_DELAY, about_text, c, CANVAS_HEIGHT, CANVAS_WIDTH, display_mutex, EVENT_DISPLAY_ABOUT, event_group, gfx_mono_draw_char(), i, OLED1_LED2_ID, oled1_set_led_state(), pdFALSE, sysfont, TERMINAL_COLUMNS, vTaskDelay(), xEventGroupClearBits(), xEventGroupWaitBits(), xSemaphoreGive, and xSemaphoreTake.

static void cdc_rx_handler ( uint8_t  instance)
static

Interrupt handler for reception from EDBG Virtual COM Port.

UART interrupt handler for reception on EDBG CDC UART.

This function is based on the interrupt handler of the SERCOM USART callback driver (_usart_interrupt_handler()). It has been modified to only handle the receive interrupt and to push the received data directly into the queue for terminal characters (terminal_in_queue), and echo the character back to the sender.

Parameters
instanceInstance number of SERCOM that generated interrupt.

References data, NULL, terminal_in_queue, and xQueueSendFromISR.

static void graph_task ( void *  params)
static

Graph task.

This task runs in the background to draw a pseudo-random graph to a dedicated display buffer. If the user selects a different screen than the graph, it will continue to update even though it is not visible until the graph screen is selected again.

Parameters
paramsParameters for the task. (Not used.)

References CANVAS_GRAPH_Y_OFFSET, CANVAS_HEIGHT, CANVAS_WIDTH, display_mutex, EVENT_DISPLAY_GRAPH, EVENT_DISPLAY_INIT, event_group, gfx_mono_draw_line, gfx_mono_draw_pixel, gfx_mono_draw_vertical_line, GFX_PIXEL_CLR, GFX_PIXEL_SET, graph_noise, GRAPH_TASK_DELAY, OLED1_LED1_ID, oled1_set_led_state(), pdFALSE, vTaskDelay(), xEventGroupWaitBits(), xSemaphoreGive, and xSemaphoreTake.

static void main_task ( void *  params)
static
static void terminal_task ( void *  params)
static
static void uart_task ( void *  params)
static

UART task.

This task runs in the background to handle the queued, incoming terminal characters and write them to the terminal text buffer. It does not print anything to the display – that is done by terminal_task().

Parameters
paramsParameters for the task. (Not used.)

References OLED1_LED1_ID, oled1_set_led_state(), terminal_buffer, TERMINAL_BUFFER_LINES, TERMINAL_COLUMNS, terminal_in_queue, terminal_line_offset, terminal_mutex, UART_TASK_DELAY, vTaskDelay(), xQueueReceive, xSemaphoreGive, and xSemaphoreTake.