Microchip® Advanced Software Framework

tstrM2MAPConfigExt Struct Reference

AP Configuration Extension.

This structure holds additional configuration parameters for the M2M AP mode. If modification of the extended parameters in AP mode is desired then tstrM2MAPModeConfig should be set by the application, which contains the main AP configuration structure as well as this extended parameters structure. When configuring provisioning mode then tstrM2MProvisionModeConfig should be used, which also contains the main AP configuration structure, this extended parameters structure and additional provisioning parameters.

#include <m2m_types.h>

Data Fields

uint8 au8DefRouterIP [4]
 
uint8 au8DNSServerIP [4]
 
uint8 au8SubnetMask [4]
 

uint8 tstrM2MAPConfigExt::au8DefRouterIP

Ap Default Router address

Referenced by m2m_wifi_enable_ap(), and m2m_wifi_start_provision_mode().

uint8 tstrM2MAPConfigExt::au8DNSServerIP

Ap DNS server address

Referenced by m2m_wifi_enable_ap(), and m2m_wifi_start_provision_mode().

uint8 tstrM2MAPConfigExt::au8SubnetMask