BLE Result.
This struct is passed to the application in response to a BLE request. If the BLE session is completed successfully, the structure will have Non-ZERO authentication type. If the BLE Session fails (due to error or timeout) the authentication type is set to ZERO.
#include <m2m_types.h>
Data Fields | |
uint8 | __PAD__ [__PADDING_tstrM2MBLEInfo_] |
uint8 | au8PSK [M2M_MAX_PSK_LEN] |
uint8 | au8SSID [M2M_MAX_SSID_LEN] |
uint8 | u8AuthType |
uint8 | u8Ch |
uint8 tstrM2MBLEInfo::__PAD__[__PADDING_tstrM2MBLEInfo_] |
uint8 tstrM2MBLEInfo::au8PSK[M2M_MAX_PSK_LEN] |
PSK for the network obtained from BLE provisioning.
uint8 tstrM2MBLEInfo::au8SSID[M2M_MAX_SSID_LEN] |
SSID obtained from BLE provisioning.
uint8 tstrM2MBLEInfo::u8Ch |
RF Channel for the AP.