Microchip® Advanced Software Framework

winc1500/host_drv/driver/source/m2m_hif.c File Reference

This module contains M2M host interface APIs implementation.

Copyright (c) 2016-2018 Microchip Technology Inc. and its subsidiaries.

#include "common/include/nm_common.h"
#include "driver/source/nmbus.h"
#include "bsp/include/nm_bsp.h"
#include "m2m_hif.h"
#include "driver/include/m2m_types.h"
#include "driver/source/nmasic.h"
#include "driver/include/m2m_periph.h"

Data Structures

struct  tstrHifContext
 

Macros

#define NMI_AHB_DATA_MEM_BASE   0x30000
 
#define NMI_AHB_SHARE_MEM_BASE   0xd0000
 
#define WIFI_HOST_RCV_CTRL_0   (0x1070)
 
#define WIFI_HOST_RCV_CTRL_1   (0x1084)
 
#define WIFI_HOST_RCV_CTRL_2   (0x1078)
 
#define WIFI_HOST_RCV_CTRL_3   (0x106c)
 
#define WIFI_HOST_RCV_CTRL_4   (0x150400)
 
#define WIFI_HOST_RCV_CTRL_5   (0x1088)
 

Functions

sint8 hif_chip_sleep (void)
 To make the chip sleep. More...
 
sint8 hif_chip_sleep_sc (void)
 To clear the chip sleep but keep the chip sleep. More...
 
sint8 hif_chip_wake (void)
 To Wakeup the chip. More...
 
sint8 hif_deinit (void *arg)
 To Deinitialize HIF layer. More...
 
uint8 hif_get_sleep_mode (void)
 Get the sleep mode of the HIF layer. More...
 
sint8 hif_handle_isr (void)
 
    Handle interrupt received from NMC1500 firmware.
More...
 
sint8 hif_init (void *arg)
 To initialize HIF layer. More...
 
static sint8 hif_isr (void)
 Host interface interrupt service routine. More...
 
sint8 hif_receive (uint32 u32Addr, uint8 *pu8Buf, uint16 u16Sz, uint8 isDone)
 
sint8 hif_register_cb (uint8 u8Grp, tpfHifCallBack fn)
 
sint8 hif_send (uint8 u8Gid, uint8 u8Opcode, uint8 *pu8CtrlBuf, uint16 u16CtrlBufSize, uint8 *pu8DataBuf, uint16 u16DataSize, uint16 u16DataOffset)
 Send packet using host interface. More...
 
static sint8 hif_set_rx_done (void)
 
void hif_set_sleep_mode (uint8 u8Pstype)
 Set the sleep mode of the HIF layer. More...
 
void hif_yield (void)
 Yields control from interrupt event handler. More...
 
static void isr (void)
 
static void m2m_hif_cb (uint8 u8OpCode, uint16 u16DataSize, uint32 u32Addr)
 WiFi call back function. More...
 

Variables

volatile tstrHifContext gstrHifCxt
 

#define NMI_AHB_DATA_MEM_BASE   0x30000
#define NMI_AHB_SHARE_MEM_BASE   0xd0000
#define WIFI_HOST_RCV_CTRL_0   (0x1070)

Referenced by hif_isr(), and hif_set_rx_done().

#define WIFI_HOST_RCV_CTRL_1   (0x1084)

Referenced by hif_isr().

#define WIFI_HOST_RCV_CTRL_2   (0x1078)

Referenced by hif_send().

#define WIFI_HOST_RCV_CTRL_3   (0x106c)

Referenced by hif_send().

#define WIFI_HOST_RCV_CTRL_4   (0x150400)

Referenced by hif_send().

#define WIFI_HOST_RCV_CTRL_5   (0x1088)

sint8 hif_chip_sleep ( void  )

To make the chip sleep.

        To make the chip sleep.
Returns
The function shall return ZERO for successful operation and a negative value otherwise.

References chip_sleep(), M2M_NO_PS, M2M_SUCCESS, ret, tstrHifContext::u8ChipMode, and tstrHifContext::u8ChipSleep.

NMI_API sint8 hif_chip_sleep_sc ( void  )

To clear the chip sleep but keep the chip sleep.

        To clear the chip count only but keep the chip awake
Returns
The function shall return ZERO for successful operation and a negative value otherwise.

References M2M_SUCCESS, and tstrHifContext::u8ChipSleep.

sint8 hif_chip_wake ( void  )

To Wakeup the chip.

    To Wakeup the chip.
Returns
The function shall return ZERO for successful operation and a negative value otherwise.

References chip_wake(), M2M_NO_PS, M2M_SUCCESS, ret, tstrHifContext::u8ChipMode, tstrHifContext::u8ChipSleep, and tstrHifContext::u8HifRXDone.

sint8 hif_deinit ( void *  arg)

To Deinitialize HIF layer.

To De-initialize HIF layer.

        To Deinitialize HIF layer.
Parameters
[in]argPointer to the arguments.
Returns
The function shall return ZERO for successful operation and a negative value otherwise.
Parameters
[in]argPointer to the arguments.
Returns
The function shall return ZERO for successful operation and a negative value otherwise.

References hif_chip_wake(), m2m_memset(), M2M_SUCCESS, and ret.

uint8 hif_get_sleep_mode ( void  )

Get the sleep mode of the HIF layer.

Returns
The function SHALL return the sleep mode of the HIF layer.

References tstrHifContext::u8ChipMode.

sint8 hif_handle_isr ( void  )

    Handle interrupt received from NMC1500 firmware.

Handle interrupt received from NMC1500 firmware.

Returns
The function SHALL return 0 for success and a negative value otherwise.

References hif_isr(), M2M_ERR, M2M_SUCCESS, nm_bsp_interrupt_ctrl(), ret, tstrHifContext::u8Interrupt, and tstrHifContext::u8Yield.

sint8 hif_init ( void *  arg)

To initialize HIF layer.

        To initialize HIF layer.
Parameters
[in]argPointer to the arguments.
Returns
The function shall return ZERO for successful operation and a negative value otherwise.
Parameters
[in]argPointer to the arguments.
Returns
The function shall return ZERO for successful operation and a negative value otherwise.

References hif_chip_sleep(), hif_register_cb(), isr(), m2m_hif_cb(), m2m_memset(), M2M_REQ_GROUP_HIF, M2M_SUCCESS, nm_bsp_register_isr(), and ret.

sint8 hif_receive ( uint32  u32Addr,
uint8 pu8Buf,
uint16  u16Sz,
uint8  isDone 
)
sint8 hif_send ( uint8  u8Gid,
uint8  u8Opcode,
uint8 pu8CtrlBuf,
uint16  u16CtrlBufSize,
uint8 pu8DataBuf,
uint16  u16DataSize,
uint16  u16DataOffset 
)

Send packet using host interface.

Parameters
[in]u8GidGroup ID.
[in]u8OpcodeOperation ID.
[in]pu8CtrlBufPointer to the Control buffer.
[in]u16CtrlBufSizeControl buffer size.
[in]u16DataOffsetPacket Data offset.
[in]pu8DataBufPacket buffer Allocated by the caller.
[in]u16DataSizePacket buffer size (including the HIF header).
Returns
The function shall return M2M_SUCCESS for successful operation and a negative value otherwise.
Parameters
[in]u8GidGroup ID.
[in]u8OpcodeOperation ID.
[in]pu8CtrlBufPointer to the Control buffer.
[in]u16CtrlBufSizeControl buffer size.
[in]u16DataOffsetPacket Data offset.
[in]pu8DataBufPacket buffer Allocated by the caller.
[in]u16DataSizePacket buffer size (including the HIF header).
Returns
The function shall return ZERO for successful operation and a negative value otherwise.

References cnt, hif_check_code(), hif_chip_sleep(), hif_chip_sleep_sc(), hif_chip_wake(), INTERRUPT_CORTUS_1_3000D0, INTERRUPT_CORTUS_2_3000D0, ISNMC3400, M2M_DBG, M2M_ERR, M2M_ERR_MEM_ALLOC, M2M_ERR_SEND, M2M_HIF_HDR_OFFSET, M2M_HIF_MAX_PACKET_SIZE, M2M_INFO, M2M_REQ_GROUP_IP, M2M_SUCCESS, NBIT1, NBIT2, NBIT3, NBIT7, NM_BSP_B_L_16, nm_bsp_sleep(), nm_read_reg_with_ret(), nm_write_block(), nm_write_reg(), nmi_get_chipid(), NMI_STATE_REG, NULL, ret, tstrHifHdr::u16Length, tstrHifHdr::u8Gid, tstrHifHdr::u8Opcode, WIFI_HOST_RCV_CTRL_2, WIFI_HOST_RCV_CTRL_3, and WIFI_HOST_RCV_CTRL_4.

void hif_set_sleep_mode ( uint8  u8Pstype)

Set the sleep mode of the HIF layer.

Parameters
[in]u8PstypeSleep mode.
Returns
The function SHALL return 0 for success and a negative value otherwise.

References tstrHifContext::u8ChipMode.

void hif_yield ( void  )

Yields control from interrupt event handler.

    Yields control from interrupt event handler.

References tstrHifContext::u8Yield.

static void isr ( void  )
static
static void m2m_hif_cb ( uint8  u8OpCode,
uint16  u16DataSize,
uint32  u32Addr 
)
static

WiFi call back function.

Parameters
[in]u8OpCodeHIF Opcode type.
[in]u16DataSizeHIF data length.
[in]u32AddrHIF address.
[in]grpHIF group type.
Author
Date
Version
1.0

Referenced by hif_init().

volatile tstrHifContext gstrHifCxt