void vStreamBufferDelete( StreamBufferHandle_t xStreamBuffer );
Deletes a stream buffer that was previously created using a call to xStreamBufferCreate() or xStreamBufferCreateStatic(). If the stream buffer was created using dynamic memory (that is, by xStreamBufferCreate()), then the allocated memory is freed.
A stream buffer handle must not be used after the stream buffer has been deleted.
xStreamBuffer | The handle of the stream buffer to be deleted. |