croutine.
h
portBASE_TYPE xCoRoutineCreate( crCOROUTINE_CODE pxCoRoutineCode, unsigned portBASE_TYPE uxPriority, unsigned portBASE_TYPE uxIndex );
Create a new co-routine and add it to the list of co-routines that are ready to run.
pxCoRoutineCode | Pointer to the co-routine function. Co-routine functions require special syntax - see the co-routine section of the WEB documentation for more information. |
uxPriority | The priority with respect to other co-routines at which the co-routine will run. |
uxIndex | Used to distinguish between different co-routines that execute the same function. See the example below and the co-routine section of the WEB documentation for further information. |
Example usage:
Co-routine to be created. void vFlashCoRoutine( xCoRoutineHandle xHandle, unsigned portBASE_TYPE uxIndex ) { Variables in co-routines must be declared static if they must maintain value across a blocking call. This may not be necessary for const variables. static const char cLedToFlash[ 2 ] = { 5, 6 }; static const portTickType uxFlashRates[ 2 ] = { 200, 400 };
Must start every co-routine with a call to crSTART(); crSTART( xHandle );
for( ;; ) { This co-routine just delays for a fixed period, then toggles an LED. Two co-routines are created using this function, so the uxIndex parameter is used to tell the co-routine which LED to flash and how long to delay. This assumes xQueue has already been created. vParTestToggleLED( cLedToFlash[ uxIndex ] ); crDELAY( xHandle, uxFlashRates[ uxIndex ] ); }
Must end every co-routine with a call to crEND(); crEND(); }
Function that creates two co-routines. void vOtherFunction( void ) { unsigned char ucParameterToPass; xTaskHandle xHandle;
Create two co-routines at priority 0. The first is given index 0 so (from the code above) toggles LED 5 every 200 ticks. The second is given index 1 so toggles LED 6 every 400 ticks. for( uxIndex = 0; uxIndex < 2; uxIndex++ ) { xCoRoutineCreate( vFlashCoRoutine, 0, uxIndex ); } }
h
BaseType_t xCoRoutineCreate( crCOROUTINE_CODE pxCoRoutineCode, UBaseType_t uxPriority, UBaseType_t uxIndex );
Create a new co-routine and add it to the list of co-routines that are ready to run.
pxCoRoutineCode | Pointer to the co-routine function. Co-routine functions require special syntax - see the co-routine section of the WEB documentation for more information. |
uxPriority | The priority with respect to other co-routines at which the co-routine will run. |
uxIndex | Used to distinguish between different co-routines that execute the same function. See the example below and the co-routine section of the WEB documentation for further information. |
Example usage:
Co-routine to be created. void vFlashCoRoutine( CoRoutineHandle_t xHandle, UBaseType_t uxIndex ) { Variables in co-routines must be declared static if they must maintain value across a blocking call. This may not be necessary for const variables. static const char cLedToFlash[ 2 ] = { 5, 6 }; static const TickType_t uxFlashRates[ 2 ] = { 200, 400 };
Must start every co-routine with a call to crSTART(); crSTART( xHandle );
for( ;; ) { This co-routine just delays for a fixed period, then toggles an LED. Two co-routines are created using this function, so the uxIndex parameter is used to tell the co-routine which LED to flash and how int32_t to delay. This assumes xQueue has already been created. vParTestToggleLED( cLedToFlash[ uxIndex ] ); crDELAY( xHandle, uxFlashRates[ uxIndex ] ); }
Must end every co-routine with a call to crEND(); crEND(); }
Function that creates two co-routines. void vOtherFunction( void ) { uint8_t ucParameterToPass; TaskHandle_t xHandle;
Create two co-routines at priority 0. The first is given index 0 so (from the code above) toggles LED 5 every 200 ticks. The second is given index 1 so toggles LED 6 every 400 ticks. for( uxIndex = 0; uxIndex < 2; uxIndex++ ) { xCoRoutineCreate( vFlashCoRoutine, 0, uxIndex ); } }