Two-Wire Interface (TWIHS) driver for SAM.
Copyright (c) 2013-2018 Microchip Technology Inc. and its subsidiaries.
#include "twihs.h"
Macros | |
#define | I2C_FAST_MODE_SPEED 400000 |
#define | LOW_LEVEL_TIME_LIMIT 384000 |
#define | TWIHS_CLK_CALC_ARGU 3 |
#define | TWIHS_CLK_DIV_MAX 0xFF |
#define | TWIHS_CLK_DIV_MIN 7 |
#define | TWIHS_CLK_DIVIDER 2 |
Functions | |
void | twihs_disable_interrupt (Twihs *p_twihs, uint32_t ul_sources) |
Disable TWIHS interrupts. More... | |
void | twihs_disable_master_mode (Twihs *p_twihs) |
Disable TWIHS master mode. More... | |
void | twihs_disable_slave_mode (Twihs *p_twihs) |
Disable TWIHS slave mode. More... | |
void | twihs_enable_interrupt (Twihs *p_twihs, uint32_t ul_sources) |
Enable TWIHS interrupts. More... | |
void | twihs_enable_master_mode (Twihs *p_twihs) |
Enable TWIHS master mode. More... | |
void | twihs_enable_slave_mode (Twihs *p_twihs) |
Enable TWIHS slave mode. More... | |
uint32_t | twihs_get_interrupt_mask (Twihs *p_twihs) |
Read TWIHS interrupt mask. More... | |
uint32_t | twihs_get_interrupt_status (Twihs *p_twihs) |
Get TWIHS interrupt status. More... | |
Pdc * | twihs_get_pdc_base (Twihs *p_twihs) |
Get TWIHS PDC base address. More... | |
void | twihs_mask_slave_addr (Twihs *p_twihs, uint32_t ul_mask) |
A mask can be applied on the slave device address in slave mode in order to allow multiple address answer. More... | |
uint32_t | twihs_master_init (Twihs *p_twihs, const twihs_options_t *p_opt) |
Initialize TWIHS master mode. More... | |
uint32_t | twihs_master_read (Twihs *p_twihs, twihs_packet_t *p_packet) |
Read multiple bytes from a TWIHS compatible slave device. More... | |
uint32_t | twihs_master_write (Twihs *p_twihs, twihs_packet_t *p_packet) |
Write multiple bytes to a TWIHS compatible slave device. More... | |
static uint32_t | twihs_mk_addr (const uint8_t *addr, int len) |
Construct the TWIHS module address register field. More... | |
uint32_t | twihs_probe (Twihs *p_twihs, uint8_t uc_slave_addr) |
Test if a chip answers a given I2C address. More... | |
uint8_t | twihs_read_byte (Twihs *p_twihs) |
Reads a byte from the TWIHS bus. More... | |
void | twihs_read_write_protection_status (Twihs *p_twihs, uint32_t *p_status) |
Read the write protection status. More... | |
void | twihs_reset (Twihs *p_twihs) |
Reset TWIHS. More... | |
void | twihs_set_alternative_command (Twihs *p_twihs, uint32_t ul_alt_cmd) |
Set length/direction/PEC for alternative command mode. More... | |
void | twihs_set_filter (Twihs *p_twihs, uint32_t ul_filter) |
Set the filter for TWIHS. More... | |
void | twihs_set_slave_addr (Twihs *p_twihs, uint32_t ul_device_addr) |
Set TWIHS slave address. More... | |
uint32_t | twihs_set_speed (Twihs *p_twihs, uint32_t ul_speed, uint32_t ul_mck) |
Set the I2C bus speed in conjunction with the clock frequency. More... | |
void | twihs_set_write_protection (Twihs *p_twihs, bool flag) |
Enables/Disables write protection mode. More... | |
void | twihs_slave_init (Twihs *p_twihs, uint32_t ul_device_addr) |
Initialize TWIHS slave mode. More... | |
uint32_t | twihs_slave_read (Twihs *p_twihs, uint8_t *p_data) |
Read data from master. More... | |
uint32_t | twihs_slave_write (Twihs *p_twihs, uint8_t *p_data) |
Write data to TWIHS bus. More... | |
void | twihs_smbus_set_timing (Twihs *p_twihs, uint32_t ul_timing) |
Set the prescaler, TLOW:SEXT, TLOW:MEXT and clock high max cycles for SMBUS mode. More... | |
void | twihs_write_byte (Twihs *p_twihs, uint8_t uc_byte) |
Sends a byte of data to one of the TWIHS slaves on the bus. More... | |