Microchip® Advanced Software Framework

write.c File Reference

System-specific implementation of the _write function used by the standard library.

Copyright (c) 2009-2018 Microchip Technology Inc. and its subsidiaries.

#include "compiler.h"

Functions

int _write (int file, const char *ptr, int len)
 

Variables

int(* ptr_put )(void volatile *, char)
 Pointer to the external low level write function. More...
 
volatile void *volatile stdio_base
 Pointer to the base of the USART module instance to use for stdio. More...