This file for Persistent Data Storage management.
Copyright (c) 2018 Microchip Technology Inc. and its subsidiaries.
#include "pds_nvm.h"
Functions | |
uint16_t | pds_calc_crc (uint8_t *buf, uint16_t len) |
Calculate crc of the given buffer. More... | |
pds_status_t | pds_compact_sector (pds_env_t *pds_instance) |
PDS Sector compact operation involves moving of valid item from one sector to another sector (new sector). More... | |
pds_status_t | pds_delete (pds_env_t *pds_instance, uint16_t item_id) |
Delete PDS item from active sector. More... | |
pds_status_t | pds_delete_all (pds_env_t *pds_instance) |
Delete all the PDS sector and initialize the sector's again. More... | |
pds_status_t | pds_init (pds_env_t *pds_instance) |
Initialize the PDS sectors and NVM memory controller. More... | |
pds_status_t | pds_item_exist (pds_env_t *pds_instance, uint16_t item_id) |
Check item id exists in the active sector. More... | |
uint16_t | pds_list_item (pds_env_t *pds_instance, uint16_t item_id, uint16_t *item_id_buf, uint16_t len) |
List PDS similar Major item ID's from active sector. More... | |
pds_status_t | pds_read (pds_env_t *pds_instance, uint16_t item_id, uint8_t *buf, uint16_t buf_len, uint16_t *read_size) |
Read the PDS item from active sector. More... | |
pds_status_t | pds_write (pds_env_t *pds_instance, uint16_t item_id, uint8_t *buf, uint16_t len) |
Write PDS item into active sector. More... | |
uint16_t pds_calc_crc | ( | uint8_t * | buf, |
uint16_t | len | ||
) |
Calculate crc of the given buffer.
[in] | buf | The pointer to uint8_t size buffer to calculate crc |
[in] | len | The length of the buffer |
pds_status_t pds_compact_sector | ( | pds_env_t * | pds_instance | ) |
PDS Sector compact operation involves moving of valid item from one sector to another sector (new sector).
This requires erase of new sector and writing new sector header and copying all the valid items into new sector one by one. Once the old sector items are copied into new sector, then new sector will be activated at the end of the compact operation.
[in] | pds_instance | Initialized PDS environment structure, |
PDS_SUCCESS | PDS Compact operation successfully completed. |
for | other return values, check pds_status_t enum values |
pds_status_t pds_delete | ( | pds_env_t * | pds_instance, |
uint16_t | item_id | ||
) |
Delete PDS item from active sector.
Scan the Item id from PDS active sector and if the item is valid, update the status deletion flag.
[in] | pds_instance | Initialized PDS environment structure, |
[in] | item_id | 16-bit item Identifier |
PDS_SUCCESS | PDS Item id found and deleted successfully |
for | other return values, check pds_status_t enum values |
pds_status_t pds_delete_all | ( | pds_env_t * | pds_instance | ) |
Delete all the PDS sector and initialize the sector's again.
Delete the PDS sectors and erase it's contents. Also initialize the PDS sector as the new device. The sector header number set to lowest valid value.
[in] | pds_instance | Initialized PDS environment structure, |
PDS_SUCCESS | PDS sector's and contents are erased and initialized |
for | other return values, check pds_status_t enum values |
pds_status_t pds_init | ( | pds_env_t * | pds_instance | ) |
Initialize the PDS sectors and NVM memory controller.
If the device is new and not initialized, then need to initialize the sector by erasing the complete sector and writing the sector header. Also the sector header status is set to valid status, Initial sector number will be set to 1. If sector's are initialized then all sector's of the PDS must be scanned and the active sector is decided based on the higher value of the sector header number.
[in] | pds_instance | Initialized PDS environment structure |
PDS_SUCCESS | PDS Initialize procedure is completed |
PDS_INIT_ERROR | PDS initialization failed, due to inactive sector or NVM Init failures |
for | other return values check pds_status_t enum values |
pds_status_t pds_item_exist | ( | pds_env_t * | pds_instance, |
uint16_t | item_id | ||
) |
Check item id exists in the active sector.
Scan the Item id from PDS active sector and if the item is valid return the status as item found
[in] | pds_instance | Initialized PDS environment structure, |
[in] | item_id | 16-bit item Identifier |
PDS_SUCCESS | PDS Item id found in the PDS |
for | other return values, check pds_status_t enum values |
uint16_t pds_list_item | ( | pds_env_t * | pds_instance, |
uint16_t | item_id, | ||
uint16_t * | item_id_buf, | ||
uint16_t | len | ||
) |
List PDS similar Major item ID's from active sector.
Scan the major (MSB) Item id's from PDS active sector & ignore the minor id's (Sub ID or LSB of Item ID) and if the item is valid and matched copy the entire item id's into buffer and update the matched item counts
[in] | pds_instance | Initialized PDS environment structure, |
[in] | item_id | 16-bit item Identifier |
[in] | item_id_buf | buffer to store the item id that's matched |
[in] | len | maximum length of the buffer to store the complete item id's |
pds_status_t pds_read | ( | pds_env_t * | pds_instance, |
uint16_t | item_id, | ||
uint8_t * | buf, | ||
uint16_t | buf_len, | ||
uint16_t * | read_size | ||
) |
Read the PDS item from active sector.
Read the item id value from the active sector. Which will scan the entire sector to find the valid block header of the item. If the item id in the block header matches, further it checks for non deletion and CRC matches.
[in] | pds_instance | Initialized PDS environment structure, |
[in] | item_id | 16-bit item Identifier |
[out] | buf | buffer to store the item values that's matched |
[in] | buf_len | maximum length of the buffer to store the valid value |
[out] | read_size | Actual valid size of the item read into buffer, This helps the application to retrieve and identify the variable size of similar item category. Where application can store variable size of data items into PDS and reduces wastage of PDS memory. The read size set 0 in case valid item not found. otherwise a valid item matched then the item size will be set to read_size referenced variable pointer. |
PDS_SUCCESS | PDS Item id found and item read success |
for | other return values, check pds_status_t enum values |
pds_status_t pds_write | ( | pds_env_t * | pds_instance, |
uint16_t | item_id, | ||
uint8_t * | buf, | ||
uint16_t | len | ||
) |
Write PDS item into active sector.
Scan the empty space in active sector. If the empty space is found the item of the block header will be written with calculated CRC. once the item is written the block is activated.
[in] | pds_instance | Initialized PDS environment structure, |
[in] | item_id | 16-bit item Identifier |
[in] | buf | buffer to write the item values in to NVM |
[in] | len | item buffer length |
PDS_SUCCESS | PDS Item id and it's values are written successfully |
for | other return values, check pds_status_t enum values |