This is the implementation of to read EUI value from EDBG.
Copyright (c) 2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | edbg_eui_read_eui64 (uint8_t *eui) |
Reads back the device MAC address stored in User page of EDBG. More... | |
void edbg_eui_read_eui64 | ( | uint8_t * | eui | ) |
Reads back the device MAC address stored in User page of EDBG.
[in] | eui | - Device EUI read back from EDBG(8 bytes) |
Referenced by dev_eui_read().