This group includes GAP address APIs.
Functions | |
at_ble_status_t | at_ble_addr_get (at_ble_addr_t *address) |
Get device BT Address. More... | |
at_ble_status_t | at_ble_addr_set (at_ble_addr_t *address) |
Set device BT Address. More... | |
at_ble_status_t | at_ble_random_address_resolve (uint8_t nb_key, at_ble_addr_t *rand_addr, uint8_t *irk_key) |
Handles request of resolving a resolvable random address ,AT_BLE_RESOLV_RAND_ADDR_STATUS event is used to inform which key has been used to perform resolution for the returned address. More... | |
at_ble_status_t at_ble_addr_get | ( | at_ble_addr_t * | address | ) |
Get device BT Address.
[out] | address | pointer to save returned BT Address |
Referenced by app_init(), ble_device_config(), ble_set_address(), and ble_set_dev_config().
at_ble_status_t at_ble_addr_set | ( | at_ble_addr_t * | address | ) |
Set device BT Address.
[in] | address | the new BT address |
Referenced by app_init(), ble_device_config(), ble_set_address(), and ble_set_dev_config().
at_ble_status_t at_ble_random_address_resolve | ( | uint8_t | nb_key, |
at_ble_addr_t * | rand_addr, | ||
uint8_t * | irk_key | ||
) |
Handles request of resolving a resolvable random address ,AT_BLE_RESOLV_RAND_ADDR_STATUS event is used to inform which key has been used to perform resolution for the returned address.
[in] | nb_key | number of provided IRK |
[in] | rand_addr | pointer to the random address |
[in] | irk_key | array of IRK used for address resolution |
Referenced by ble_connected_state_handler().