Microchip® Advanced Software Framework

radio_lbt.h File Reference

This is the Radio LBT header file which contains listen before talk specific Radio functions declarations and defines for SX1276.

Copyright (c) 2018 Microchip Technology Inc. and its subsidiaries.

#include "system_task_manager.h"
#include "stdint.h"

Functions

void Radio_LBTScanTimeout (uint8_t time)
 This function is the callback function for LBT scan timer timeout. More...
 
SYSTEM_TaskStatus_t radioScanDoneHandler (void)
 This function is triggered by the scan done event and it sets up the radio for scanning. More...
 

void Radio_LBTScanTimeout ( uint8_t  time)

This function is the callback function for LBT scan timer timeout.

Parameters
time- not used.
Returns
- none
SYSTEM_TaskStatus_t radioScanDoneHandler ( void  )

This function is triggered by the scan done event and it sets up the radio for scanning.

Parameters
-none
Returns
- returns the success or failure of a task