Main functions.
Copyright (c) 2016-2018 Microchip Technology Inc. and its subsidiaries.
#include "usb_protocol_cdc.h"
Functions | |
void | main_cdc_disable (uint8_t port) |
Closes the communication port This is called by CDC interface when USB Host disable it. More... | |
bool | main_cdc_enable (uint8_t port) |
Opens the communication port This is called by CDC interface when USB Host enable it. More... | |
void | main_cdc_rx_notify (uint8_t port) |
Called by CDC interface Callback running when CDC device have received data. More... | |
void | main_cdc_set_coding (uint8_t port, usb_cdc_line_coding_t *cfg) |
Configures communication line. More... | |
void | main_cdc_set_dtr (uint8_t port, bool b_enable) |
Save new DTR state to change led behavior. The DTR notify that the terminal have open or close the communication port. More... | |
void | main_remotewakeup_lpm_disable (void) |
Called by UDC when USB Host request to disable LPM remote wakeup. More... | |
void | main_remotewakeup_lpm_enable (void) |
Called by UDC when USB Host request to enable LPM remote wakeup. More... | |
void | main_suspend_lpm_action (void) |
Enters the application in low power mode Callback called when USB host sets LPM suspend state. More... | |
void main_cdc_disable | ( | uint8_t | port | ) |
Closes the communication port This is called by CDC interface when USB Host disable it.
bool main_cdc_enable | ( | uint8_t | port | ) |
Opens the communication port This is called by CDC interface when USB Host enable it.
true | if cdc startup is successfully done |
void main_cdc_rx_notify | ( | uint8_t | port | ) |
Called by CDC interface Callback running when CDC device have received data.
void main_cdc_set_coding | ( | uint8_t | port, |
usb_cdc_line_coding_t * | cfg | ||
) |
Configures communication line.
cfg | line configuration |
void main_cdc_set_dtr | ( | uint8_t | port, |
bool | b_enable | ||
) |
Save new DTR state to change led behavior. The DTR notify that the terminal have open or close the communication port.
void main_remotewakeup_lpm_disable | ( | void | ) |
Called by UDC when USB Host request to disable LPM remote wakeup.
void main_remotewakeup_lpm_enable | ( | void | ) |
Called by UDC when USB Host request to enable LPM remote wakeup.
void main_suspend_lpm_action | ( | void | ) |
Enters the application in low power mode Callback called when USB host sets LPM suspend state.