A structure for storing all the attributes of the radio and the transceiver.
#include <radio_interface.h>
Data Fields | |
RadioFSKBandWidth_t | afcBw |
RadioLoRaBandWidth_t | bandWidth |
uint32_t | bitRate |
uint8_t | clockSource |
uint8_t | clockStabilizationDelay |
uint8_t | crcOn |
uint8_t * | dataBuffer |
uint8_t volatile | dataBufferLen |
RadioDataRate_t | dataRate |
RadioErrorCodingRate_t | errorCodingRate |
uint32_t | frequency |
uint32_t | frequencyDeviation |
uint16_t | frequencyHopPeriod |
RadioFSKShaping_t | fskDataShaping |
uint8_t volatile | fskPayloadIndex |
uint8_t | fskRxWindowTimerId |
uint8_t | implicitHeaderMode |
uint8_t | initialized |
uint8_t | iqInverted |
RadioLBT_t | lbt |
RadioModulation_t | modulation |
int8_t | outputPower |
uint8_t | paBoost |
int16_t | packetRSSI |
int8_t | packetSNR |
uint16_t | preambleLen |
RadioCallback_t | radioCallback |
uint8_t | regVersion |
RadioFSKBandWidth_t | rxBw |
uint8_t | syncWord [8] |
uint8_t | syncWordLen |
uint8_t | syncWordLoRa |
uint8_t | timeOnAirTimerId |
uint8_t | watchdogTimerId |
uint32_t | watchdogTimerTimeout |
RadioFSKBandWidth_t _RadioConfiguration_t::afcBw |
RadioLoRaBandWidth_t _RadioConfiguration_t::bandWidth |
uint32_t _RadioConfiguration_t::bitRate |
uint8_t _RadioConfiguration_t::clockSource |
uint8_t _RadioConfiguration_t::clockStabilizationDelay |
uint8_t _RadioConfiguration_t::crcOn |
uint8_t* _RadioConfiguration_t::dataBuffer |
uint8_t volatile _RadioConfiguration_t::dataBufferLen |
RadioDataRate_t _RadioConfiguration_t::dataRate |
RadioErrorCodingRate_t _RadioConfiguration_t::errorCodingRate |
uint32_t _RadioConfiguration_t::frequency |
Referenced by Radio_ReadLoraRssi().
uint32_t _RadioConfiguration_t::frequencyDeviation |
uint16_t _RadioConfiguration_t::frequencyHopPeriod |
Referenced by RADIO_FHSSChangeChannel().
RadioFSKShaping_t _RadioConfiguration_t::fskDataShaping |
uint8_t volatile _RadioConfiguration_t::fskPayloadIndex |
uint8_t _RadioConfiguration_t::fskRxWindowTimerId |
uint8_t _RadioConfiguration_t::implicitHeaderMode |
uint8_t _RadioConfiguration_t::initialized |
uint8_t _RadioConfiguration_t::iqInverted |
RadioLBT_t _RadioConfiguration_t::lbt |
RadioModulation_t _RadioConfiguration_t::modulation |
int8_t _RadioConfiguration_t::outputPower |
uint8_t _RadioConfiguration_t::paBoost |
int16_t _RadioConfiguration_t::packetRSSI |
int8_t _RadioConfiguration_t::packetSNR |
uint16_t _RadioConfiguration_t::preambleLen |
RadioCallback_t _RadioConfiguration_t::radioCallback |
Referenced by RADIO_FHSSChangeChannel().
uint8_t _RadioConfiguration_t::regVersion |
RadioFSKBandWidth_t _RadioConfiguration_t::rxBw |
uint8_t _RadioConfiguration_t::syncWord[8] |
uint8_t _RadioConfiguration_t::syncWordLen |
uint8_t _RadioConfiguration_t::syncWordLoRa |
uint8_t _RadioConfiguration_t::timeOnAirTimerId |
uint8_t _RadioConfiguration_t::watchdogTimerId |
uint32_t _RadioConfiguration_t::watchdogTimerTimeout |