#include <MCMPackageCore.h>
Data Fields | |
struct { | |
uint32_t DataRate:8 | |
uint32_t DLFrequency:24 | |
}; | |
uint8_t | McGroupIDHeader |
uint32_t | SessionTime |
uint8_t | TimeOut |
struct { ... } |
uint32_t McClassSessionParams_s::DataRate |
datarate of the current class c session
uint32_t McClassSessionParams_s::DLFrequency |
reception frequency
uint8_t McClassSessionParams_s::McGroupIDHeader |
is the identifier of the multicast group being used.
uint32_t McClassSessionParams_s::SessionTime |
uint8_t McClassSessionParams_s::TimeOut |