#include <at_ble_api.h>
Data Fields | |
uint8_t | irk [AT_BLE_MAX_KEY_LEN] |
IRK that correctly solved the random address. More... | |
uint8_t | resolved_addr [AT_BLE_ADDR_LEN] |
returned address More... | |
at_ble_status_t | status |
uint8_t at_ble_resolv_rand_addr_status_t::irk[AT_BLE_MAX_KEY_LEN] |
IRK that correctly solved the random address.
Referenced by ble_resolv_rand_addr_handler().
uint8_t at_ble_resolv_rand_addr_status_t::resolved_addr[AT_BLE_ADDR_LEN] |
returned address
at_ble_status_t at_ble_resolv_rand_addr_status_t::status |
Referenced by ble_resolv_rand_addr_handler().