#include <atca_host.h>
Data Fields | |
const uint8_t * | digest |
Plaintext digest as input. More... | |
uint8_t * | digest_enc |
Encrypted (ciphertext) digest is return here (32 bytes) More... | |
uint8_t * | hashed_key |
Calculated key is returned here (32 bytes) More... | |
const uint8_t * | io_key |
IO protection key value (32 bytes) More... | |
struct atca_temp_key * | temp_key |
Current value of TempKey. More... | |
const uint8_t* atca_secureboot_enc_in_out::digest |
Plaintext digest as input.
Referenced by atcah_secureboot_enc().
uint8_t* atca_secureboot_enc_in_out::digest_enc |
Encrypted (ciphertext) digest is return here (32 bytes)
Referenced by atcah_secureboot_enc().
uint8_t* atca_secureboot_enc_in_out::hashed_key |
Calculated key is returned here (32 bytes)
Referenced by atcah_secureboot_enc().
const uint8_t* atca_secureboot_enc_in_out::io_key |
IO protection key value (32 bytes)
Referenced by atcah_secureboot_enc().
struct atca_temp_key* atca_secureboot_enc_in_out::temp_key |
Current value of TempKey.
Referenced by atcah_secureboot_enc().