#include <atca_host.h>
Data Fields | |
const uint8_t * | io_key |
IO protection key value (32 bytes). More... | |
uint16_t | key_id |
KeyID (Param2) used in Verify command. More... | |
uint8_t * | mac |
Calculated verification MAC is returned here (32 bytes). More... | |
uint8_t | mode |
Mode (Param1) parameter used in Verify command. More... | |
const uint8_t * | msg_dig_buf |
Message digest buffer (64 bytes). More... | |
const uint8_t * | other_data |
OtherData used in Verify command (19 bytes). More... | |
const uint8_t * | signature |
Signature used in Verify command (64 bytes). More... | |
const uint8_t * | sn |
Serial number (9 bytes). More... | |
const atca_temp_key_t * | temp_key |
TempKey. More... | |
const uint8_t* atca_verify_mac::io_key |
IO protection key value (32 bytes).
Referenced by atcah_verify_mac().
uint16_t atca_verify_mac::key_id |
KeyID (Param2) used in Verify command.
Referenced by atcah_verify_mac().
uint8_t* atca_verify_mac::mac |
Calculated verification MAC is returned here (32 bytes).
Referenced by atcah_verify_mac().
uint8_t atca_verify_mac::mode |
Mode (Param1) parameter used in Verify command.
Referenced by atcah_verify_mac().
const uint8_t* atca_verify_mac::msg_dig_buf |
Message digest buffer (64 bytes).
Referenced by atcah_verify_mac().
const uint8_t* atca_verify_mac::other_data |
OtherData used in Verify command (19 bytes).
Referenced by atcah_verify_mac().
const uint8_t* atca_verify_mac::signature |
Signature used in Verify command (64 bytes).
Referenced by atcah_verify_mac().
const uint8_t* atca_verify_mac::sn |
Serial number (9 bytes).
Referenced by atcah_verify_mac().
const atca_temp_key_t* atca_verify_mac::temp_key |
TempKey.
Referenced by atcah_verify_mac().