#include <atca_crypto_sw_sha1.h>
Data Fields | |
uint32_t | pad [32] |
Filler value to make sure the actual implementation has enough room to store its context. uint32_t is used to remove some alignment warnings. More... | |
uint32_t atcac_sha1_ctx::pad[32] |
Filler value to make sure the actual implementation has enough room to store its context. uint32_t is used to remove some alignment warnings.