Global FTMPackage parameters
#include <FTMPackageCore.h>
Data Fields | |
uint16_t | BlockAckDelay |
uint32_t | Descriptor |
uint8_t | Encoding |
uint8_t | FragIndex |
uint8_t | FragSession |
uint8_t | FragSize |
uint8_t | McGroupBitMask |
uint16_t | NbFrag |
uint8_t | Padding |
uint16_t | Redundancy |
uint16_t sFTMPackageParams::BlockAckDelay |
Specifies random delay between request and device reply for multicast requests in seconds
uint32_t sFTMPackageParams::Descriptor |
32bit number describing the file that is going to be transported through the fragmentation session. The encoding of this field is application specific.
uint8_t sFTMPackageParams::Encoding |
uint8_t sFTMPackageParams::FragIndex |
uint8_t sFTMPackageParams::FragSession |
uint8_t sFTMPackageParams::FragSize |
is the size in byte of each fragment.
uint8_t sFTMPackageParams::McGroupBitMask |
specifies which multicast group addresses are allowed as input to this defragmentation session
uint16_t sFTMPackageParams::NbFrag |
uint8_t sFTMPackageParams::Padding |
specifies number of padding bytes
uint16_t sFTMPackageParams::Redundancy |
specifies the total number of Redundancy fragments of the data block to be transported during the coming multicast fragmentation session