This is the implementation of LoRaWAN system initialization.
Copyright (c) 2018 Microchip Technology Inc. and its subsidiaries.
Functions | |
void | Stack_Init (void) |
Initializes the system. More... | |
void Stack_Init | ( | void | ) |
Initializes the system.
This is the first stack function to be called by the application in the main() function.
References APP_TASK_ID, and SYSTEM_PostTask().