#include <miwi_api.h>
Data Fields | |
uint8_t | bloomFilterValue [BLOOM_FILTER_SIZE] |
bloom filter value More... | |
uint8_t | connectionPermit |
connection permit More... | |
uint8_t | coordinatorHop |
coordinator hop More... | |
uint8_t | enddeviceCapacity |
End device Capacity percentage. More... | |
uint8_t | LinkQuality |
LQI at which the beacon was received. More... | |
uint8_t | logicalChannel |
The current logical channel used by the network. More... | |
uint16_t | panId |
PANID. More... | |
uint16_t | shortAddress |
Short Address. More... | |
uint8_t | sleepEnddeviceCapacity |
Sleeping End device Capacity percentage. More... | |
uint8_t beaconDescriptor_t::bloomFilterValue[BLOOM_FILTER_SIZE] |
bloom filter value
uint8_t beaconDescriptor_t::connectionPermit |
connection permit
uint8_t beaconDescriptor_t::coordinatorHop |
coordinator hop
uint8_t beaconDescriptor_t::enddeviceCapacity |
End device Capacity percentage.
uint8_t beaconDescriptor_t::LinkQuality |
LQI at which the beacon was received.
uint8_t beaconDescriptor_t::logicalChannel |
The current logical channel used by the network.
uint16_t beaconDescriptor_t::panId |
PANID.
uint16_t beaconDescriptor_t::shortAddress |
Short Address.
uint8_t beaconDescriptor_t::sleepEnddeviceCapacity |
Sleeping End device Capacity percentage.