Microchip® Advanced Software Framework

usart_config Struct Reference

USART configuration struct.

Configuration options for USART.

#include <usart.h>

Data Fields

uint32_t baudrate
 USART baudrate. More...
 
enum usart_character_size character_size
 USART character size. More...
 
bool clock_polarity_inverted
 USART Clock Polarity. More...
 
bool collision_detection_enable
 Enable collision dection. More...
 
enum usart_dataorder data_order
 USART bit order (MSB or LSB first) More...
 
bool encoding_format_enable
 Enable IrDA encoding format. More...
 
uint32_t ext_clock_freq
 External clock frequency in synchronous mode. More...
 
enum gclk_generator generator_source
 GCLK generator source. More...
 
bool immediate_buffer_overflow_notification
 Controls when the buffer overflow status bit is asserted when a buffer overflow occurs. More...
 
struct iso7816_config_t iso7816_config
 Enable ISO7816 for smart card interfacing. More...
 
enum lin_master_break_length lin_break_length
 LIN Master Break Length. More...
 
enum lin_master_header_delay lin_header_delay
 LIN master header delay. More...
 
enum lin_node_type lin_node
 LIN node type. More...
 
bool lin_slave_enable
 Enable LIN Slave Support. More...
 
enum usart_signal_mux_settings mux_setting
 USART pin out. More...
 
enum usart_parity parity
 USART parity. More...
 
uint32_t pinmux_pad0
 PAD0 pinmux. More...
 
uint32_t pinmux_pad1
 PAD1 pinmux. More...
 
uint32_t pinmux_pad2
 PAD2 pinmux. More...
 
uint32_t pinmux_pad3
 PAD3 pinmux. More...
 
uint8_t receive_pulse_length
 The minimum pulse length required for a pulse to be accepted by the IrDA receiver. More...
 
bool receiver_enable
 Enable receiver. More...
 
enum rs485_guard_time rs485_guard_time
 RS485 guard time. More...
 
bool run_in_standby
 If true the USART will be kept running in Standby sleep mode. More...
 
enum usart_sample_adjustment sample_adjustment
 USART sample adjustment. More...
 
enum usart_sample_rate sample_rate
 USART sample rate. More...
 
bool start_frame_detection_enable
 Enable start of frame dection. More...
 
enum usart_stopbits stopbits
 Number of stop bits. More...
 
enum usart_transfer_mode transfer_mode
 USART in asynchronous or synchronous mode. More...
 
bool transmitter_enable
 Enable transmitter. More...
 
bool use_external_clock
 States whether to use the external clock applied to the XCK pin. More...
 

enum usart_character_size usart_config::character_size
bool usart_config::clock_polarity_inverted

USART Clock Polarity.

If true, data changes on falling XCK edge and is sampled at rising edge. If false, data changes on rising XCK edge and is sampled at falling edge.

Referenced by _usart_set_config(), and usart_get_config_defaults().

bool usart_config::collision_detection_enable

Enable collision dection.

Referenced by _usart_set_config(), and usart_get_config_defaults().

enum usart_dataorder usart_config::data_order

USART bit order (MSB or LSB first)

Referenced by _usart_set_config(), and usart_get_config_defaults().

bool usart_config::encoding_format_enable

Enable IrDA encoding format.

Referenced by _usart_set_config(), and usart_get_config_defaults().

uint32_t usart_config::ext_clock_freq

External clock frequency in synchronous mode.

This must be set if use_external_clock is true.

Referenced by _usart_set_config(), and usart_get_config_defaults().

enum gclk_generator usart_config::generator_source

GCLK generator source.

Referenced by main(), uart_config(), usart_get_config_defaults(), and usart_init().

bool usart_config::immediate_buffer_overflow_notification

Controls when the buffer overflow status bit is asserted when a buffer overflow occurs.

Referenced by _usart_set_config(), and usart_get_config_defaults().

struct iso7816_config_t usart_config::iso7816_config

Enable ISO7816 for smart card interfacing.

Referenced by _usart_set_config(), usart_get_config_defaults(), and usart_init().

enum lin_master_break_length usart_config::lin_break_length

LIN Master Break Length.

Referenced by _usart_set_config(), and usart_get_config_defaults().

enum lin_master_header_delay usart_config::lin_header_delay

LIN master header delay.

Referenced by _usart_set_config(), and usart_get_config_defaults().

enum lin_node_type usart_config::lin_node

LIN node type.

Referenced by _usart_set_config(), and usart_get_config_defaults().

bool usart_config::lin_slave_enable

Enable LIN Slave Support.

Referenced by _usart_set_config(), usart_get_config_defaults(), and usart_init().

enum usart_parity usart_config::parity
uint32_t usart_config::pinmux_pad0

PAD0 pinmux.

If current USARTx has several alternative multiplexing I/O pins for PAD0, then only one peripheral multiplexing I/O can be enabled for current USARTx PAD0 function. Make sure that no other alternative multiplexing I/O is associated with the same USARTx PAD0.

Referenced by cdc_rx_init(), cdc_uart_init(), configure_console(), configure_usart(), main(), sio2host_init(), test_system_init(), uart_config(), usart_get_config_defaults(), and usart_init().

uint32_t usart_config::pinmux_pad1

PAD1 pinmux.

If current USARTx has several alternative multiplexing I/O pins for PAD1, then only one peripheral multiplexing I/O can be enabled for current USARTx PAD1 function. Make sure that no other alternative multiplexing I/O is associated with the same USARTx PAD1.

Referenced by cdc_rx_init(), cdc_uart_init(), configure_console(), configure_usart(), main(), sio2host_init(), test_system_init(), uart_config(), usart_get_config_defaults(), and usart_init().

uint32_t usart_config::pinmux_pad2

PAD2 pinmux.

If current USARTx has several alternative multiplexing I/O pins for PAD2, then only one peripheral multiplexing I/O can be enabled for current USARTx PAD2 function. Make sure that no other alternative multiplexing I/O is associated with the same USARTx PAD2.

Referenced by cdc_rx_init(), cdc_uart_init(), configure_console(), configure_usart(), main(), sio2host_init(), test_system_init(), uart_config(), usart_get_config_defaults(), and usart_init().

uint32_t usart_config::pinmux_pad3

PAD3 pinmux.

If current USARTx has several alternative multiplexing I/O pins for PAD3, then only one peripheral multiplexing I/O can be enabled for current USARTx PAD3 function. Make sure that no other alternative multiplexing I/O is associated with the same USARTx PAD3.

Referenced by cdc_rx_init(), cdc_uart_init(), configure_console(), configure_usart(), main(), sio2host_init(), test_system_init(), uart_config(), usart_get_config_defaults(), and usart_init().

uint8_t usart_config::receive_pulse_length

The minimum pulse length required for a pulse to be accepted by the IrDA receiver.

Referenced by _usart_set_config(), and usart_get_config_defaults().

bool usart_config::receiver_enable

Enable receiver.

Referenced by _usart_set_config(), usart_get_config_defaults(), and usart_init().

enum rs485_guard_time usart_config::rs485_guard_time

RS485 guard time.

Referenced by _usart_set_config(), and usart_get_config_defaults().

bool usart_config::run_in_standby

If true the USART will be kept running in Standby sleep mode.

Referenced by _usart_set_config(), and usart_get_config_defaults().

enum usart_sample_adjustment usart_config::sample_adjustment

USART sample adjustment.

Referenced by _usart_set_config(), and usart_get_config_defaults().

enum usart_sample_rate usart_config::sample_rate

USART sample rate.

Referenced by _usart_set_config(), and usart_get_config_defaults().

bool usart_config::start_frame_detection_enable

Enable start of frame dection.

Referenced by _usart_set_config(), usart_get_config_defaults(), and usart_init().

enum usart_stopbits usart_config::stopbits

Number of stop bits.

Referenced by _usart_set_config(), uart_config(), and usart_get_config_defaults().

enum usart_transfer_mode usart_config::transfer_mode

USART in asynchronous or synchronous mode.

Referenced by _usart_set_config(), and usart_get_config_defaults().

bool usart_config::transmitter_enable

Enable transmitter.

Referenced by _usart_set_config(), usart_get_config_defaults(), and usart_init().

bool usart_config::use_external_clock

States whether to use the external clock applied to the XCK pin.

In synchronous mode the shift register will act directly on the XCK clock. In asynchronous mode the XCK will be the input to the USART hardware module.

Referenced by _usart_set_config(), and usart_get_config_defaults().