Microchip® Advanced Software Framework

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Macros Groups Pages
maXTouch low-level component

See Quick start guide for the maXTouch component.

This component provides low-level read/write access to the configuration and data registers on a maXTouch device. It has only been tested on mxt143E parts, but it should be easy to add support for other maXTouch devices. This is a common API for all supported architectures in ASF.

The component is not interrupt driven and the maXTouch device has to be polled to see if there are any pending messages, and the mxt_read_message function reads out the messages pending. For reading out only touch events, the mxt_read_touch_event function can be used. As mentioned the component is not interrupt driven, but by configuring a pin change interrupt on the CHG pin, the application can receive interrupts when there are messages pending.

Modules

 Quick Start Guide(s)
 In this section you can find a list of all Quick Start guides related to the maXTouch low-level component.
 

Data Structures

struct  mxt_conf_messageprocessor_t5
 Object message. More...
 
struct  mxt_device
 maXTouch device information data container struct More...
 
struct  mxt_gen_commandprocessor_t6
 Commandprocessor T6 object. More...
 
struct  mxt_info_object
 Identification header. More...
 
struct  mxt_object
 Object table entry. More...
 
struct  mxt_report_id_map
 Map of the report ID vs object type and instance. More...
 
struct  mxt_touch_event
 Touch event struct. More...
 

Typedefs

typedef void(* mxt_message_handler_t )(struct mxt_device *device, struct mxt_conf_messageprocessor_t5 *message)
 Message handler prototype. More...
 

Enumerations

enum  mxt_object_type {
  MXT_GEN_MESSAGEPROCESSOR_T5 = 5,
  MXT_GEN_COMMANDPROCESSOR_T6 = 6,
  MXT_GEN_POWERCONFIG_T7 = 7,
  MXT_GEN_ACQUISITIONCONFIG_T8 = 8,
  MXT_TOUCH_MULTITOUCHSCREEN_T9 = 9,
  MXT_SPT_COMMSCONFIG_T18 = 18,
  MXT_SPT_MESSAGECOUNT_T44 = 44,
  MXT_SPT_CTE_CONFIGURATION_T46 = 46,
  MXT_PROCG_TOUCHSUPPRESSION_T48 = 48,
  MXT_PROCI_SHIELDLESS_T56 = 56
}
 Object types. More...
 

Functions

status_code_t mxt_close_device (struct mxt_device *device)
 Closes the twi connection and frees memory. More...
 
int8_t mxt_get_message_count (struct mxt_device *device)
 Get pending message count. More...
 
uint16_t mxt_get_object_address (struct mxt_device *device, uint8_t object_id, uint8_t instance)
 Get memory address to object. More...
 
enum mxt_object_type mxt_get_object_type (struct mxt_device *device, struct mxt_conf_messageprocessor_t5 *message)
 Get object type from message. More...
 
status_code_t mxt_init_device (struct mxt_device *device, twihs_master_t interface, uint8_t chip_adr, uint32_t chgpin)
 Initialize maXTouch device connected to TWIx module. More...
 
bool mxt_is_message_pending (struct mxt_device *device)
 Report if there is any pending messages in the queue. More...
 
status_code_t mxt_load_configuration (struct mxt_device *device, void *configuration_data)
 
status_code_t mxt_probe_device (twihs_master_t interface, uint8_t chip_adr)
 Probe for a maXTouch connected to a specific TWI line. More...
 
status_code_t mxt_process_messages (struct mxt_device *device)
 Process message queue on maXTouch device. More...
 
status_code_t mxt_read_config_object (struct mxt_device *device, mxt_memory_adr memory_adr, void *obj_data)
 Read object configuration. More...
 
status_code_t mxt_read_config_reg (struct mxt_device *device, mxt_memory_adr memory_adr, uint8_t *value)
 Read object register. More...
 
status_code_t mxt_read_message (struct mxt_device *device, struct mxt_conf_messageprocessor_t5 *message)
 Get next message in queue. More...
 
status_code_t mxt_read_touch_event (struct mxt_device *device, struct mxt_touch_event *touch_event)
 Read next touch event in queue, skip other events (other events are lost) More...
 
void mxt_set_message_handler (struct mxt_device *device, mxt_message_handler_t handler)
 Set message handler. More...
 
status_code_t mxt_write_config_object (struct mxt_device *device, mxt_memory_adr memory_adr, void *obj_data)
 Write object configuration. More...
 
status_code_t mxt_write_config_reg (struct mxt_device *device, mxt_memory_adr memory_adr, uint8_t value)
 Write object register. More...
 

COMMSCONFIG T18 object control register bit positions

#define MXT_COMMSCONFIG_T18_CHG_MODE_bp   2
 
#define MXT_COMMSCONFIG_T18_DISMNTR_bp   7
 

COMMANDPROCESSOR T6 object register offset

#define MXT_GEN_COMMANDPROCESSOR_RESET   0
 
#define MXT_GEN_COMMANDPROCESSOR_BACKUPNV   1
 
#define MXT_GEN_COMMANDPROCESSOR_CALIBRATE   2
 
#define MXT_GEN_COMMANDPROCESSOR_REPORTALL   3
 
#define MXT_GEN_COMMANDPROCESSOR_DIAGNOSTIC   5
 

Touch event types

#define MXT_UNGRIP_EVENT   1
 
#define MXT_SUPPRESS_EVENT   2
 
#define MXT_AMP_EVENT   4
 
#define MXT_VECTOR_EVENT   8
 
#define MXT_MOVE_EVENT   16
 
#define MXT_RELEASE_EVENT   32
 
#define MXT_PRESS_EVENT   64
 
#define MXT_DETECT_EVENT   128
 

#define MXT_AMP_EVENT   4
#define MXT_COMMSCONFIG_T18_CHG_MODE_bp   2
#define MXT_COMMSCONFIG_T18_DISMNTR_bp   7
#define MXT_DETECT_EVENT   128
#define MXT_GEN_COMMANDPROCESSOR_BACKUPNV   1
#define MXT_GEN_COMMANDPROCESSOR_CALIBRATE   2
#define MXT_GEN_COMMANDPROCESSOR_DIAGNOSTIC   5
#define MXT_GEN_COMMANDPROCESSOR_REPORTALL   3
#define MXT_GEN_COMMANDPROCESSOR_RESET   0
#define MXT_MOVE_EVENT   16
#define MXT_PRESS_EVENT   64
#define MXT_RELEASE_EVENT   32
#define MXT_SUPPRESS_EVENT   2
#define MXT_UNGRIP_EVENT   1
#define MXT_VECTOR_EVENT   8

typedef void(* mxt_message_handler_t)(struct mxt_device *device, struct mxt_conf_messageprocessor_t5 *message)

Message handler prototype.

Parameters
*devicePointer to mxt_device struct
*messagePointer to mxt_message struct

Object types.

Enumerator
MXT_GEN_MESSAGEPROCESSOR_T5 
MXT_GEN_COMMANDPROCESSOR_T6 
MXT_GEN_POWERCONFIG_T7 
MXT_GEN_ACQUISITIONCONFIG_T8 
MXT_TOUCH_MULTITOUCHSCREEN_T9 
MXT_SPT_COMMSCONFIG_T18 
MXT_SPT_MESSAGECOUNT_T44 
MXT_SPT_CTE_CONFIGURATION_T46 
MXT_PROCG_TOUCHSUPPRESSION_T48 
MXT_PROCI_SHIELDLESS_T56 

status_code_t mxt_close_device ( struct mxt_device device)

Closes the twi connection and frees memory.

Parameters
*devicePointer to mxt_device instance
Returns
Operation result status code

References mxt_device::info_object, mxt_device::object_list, mxt_device::report_id_map, and STATUS_OK.

int8_t mxt_get_message_count ( struct mxt_device device)

Get pending message count.

Parameters
*devicePointer to mxt_device instance
Returns
Number of pending messages in the queue

References twihs_packet::addr, ERR_IO_ERROR, mxt_device::interface, mxt_device::mxt_chip_adr, mxt_get_object_address(), MXT_SPT_MESSAGECOUNT_T44, STATUS_OK, and twihs_master_read().

uint16_t mxt_get_object_address ( struct mxt_device device,
uint8_t  object_id,
uint8_t  instance 
)

Get memory address to object.

Parameters
*devicePointer to mxt_device instance
object_idObject ID
instanceObject instance
Returns
Object memory address on maXTouch device. 0 if object not found

References mxt_device::info_object, mxt_info_object::obj_count, mxt_device::object_list, mxt_object::start_address, and mxt_object::type.

Referenced by mxt_get_message_count(), and mxt_read_message().

enum mxt_object_type mxt_get_object_type ( struct mxt_device device,
struct mxt_conf_messageprocessor_t5 message 
)

Get object type from message.

Parameters
*devicePointer to mxt_device instance
*messageMessage buffer
Returns
Operation

References mxt_report_id_map::object_type, mxt_device::report_id_map, and mxt_conf_messageprocessor_t5::reportid.

Referenced by mxt_read_touch_event().

status_code_t mxt_init_device ( struct mxt_device device,
twihs_master_t  interface,
uint8_t  chip_adr,
uint32_t  chgpin 
)

Initialize maXTouch device connected to TWIx module.

Parameters
*interfacePointer to TWI register set
*devicePointer to mxt_device instance
chip_adrI2C address to maXTouch device
chgpinIOPORT pin instance attached to the maXTouch device's /CHG pin
Returns
Operation result status code

References mxt_device::chgpin, ERR_BAD_DATA, mxt_device::handler, mxt_device::interface, mxt_device::multitouch_report_offset, mxt_device::mxt_chip_adr, mxt_create_report_id_map(), mxt_get_report_id_offset(), mxt_info_le_to_cpu(), mxt_read_info_block(), MXT_TOUCH_MULTITOUCHSCREEN_T9, mxt_validate_info_block(), NULL, status, and STATUS_OK.

bool mxt_is_message_pending ( struct mxt_device device)

Report if there is any pending messages in the queue.

Parameters
*devicePointer to mxt_device instance
Returns
Return /CHG pin status

References mxt_device::chgpin, and ioport_get_pin_level().

Referenced by mxt_process_messages(), and mxt_read_touch_event().

status_code_t mxt_load_configuration ( struct mxt_device device,
void *  configuration_data 
)
status_code_t mxt_probe_device ( twihs_master_t  interface,
uint8_t  chip_adr 
)

Probe for a maXTouch connected to a specific TWI line.

Parameters
interfacePointer to TWI register set
*chip_adrI2C address to maXTouch device
Returns
Operation result status code

References twihs_packet::addr, buffer, ERR_BAD_ADDRESS, mxt_info_object::family_ID, MXT_FAMILY_143E, MXT_MEM_ADDR, MXT_VARIANT_143E, status, STATUS_OK, twihs_master_read(), TWIHS_SUCCESS, and mxt_info_object::variant_ID.

status_code_t mxt_process_messages ( struct mxt_device device)

Process message queue on maXTouch device.

Parameters
*devicePointer to mxt_device instance
Returns
Operation result status code

References ERR_BAD_ADDRESS, mxt_device::handler, if(), mxt_is_message_pending(), mxt_read_message(), NULL, status, and STATUS_OK.

status_code_t mxt_read_config_object ( struct mxt_device device,
mxt_memory_adr  memory_adr,
void *  obj_data 
)

Read object configuration.

Parameters
*devicePointer to mxt_device instance
memory_adrMemory address to the object
*obj_dataPointer to a large enough memory buffer
Returns
Operation result status code

References twihs_packet::addr, ERR_IO_ERROR, mxt_device::interface, mxt_device::mxt_chip_adr, mxt_get_object_size(), STATUS_OK, and twihs_master_read().

status_code_t mxt_read_config_reg ( struct mxt_device device,
mxt_memory_adr  memory_adr,
uint8_t *  value 
)

Read object register.

Parameters
*devicePointer to mxt_device instance
memory_adrMemory address to the register
*valuePointer to a 1 byte buffer to store the data in
Returns
Operation result status code

References twihs_packet::addr, ERR_IO_ERROR, mxt_device::interface, mxt_device::mxt_chip_adr, STATUS_OK, and twihs_master_read().

status_code_t mxt_read_message ( struct mxt_device device,
struct mxt_conf_messageprocessor_t5 message 
)

Get next message in queue.

Parameters
*devicePointer to mxt_device instance
*messagePointer to mxt_message instance
Returns
Operation result status code

References twihs_packet::addr, ERR_IO_ERROR, mxt_device::interface, mxt_device::mxt_chip_adr, MXT_GEN_MESSAGEPROCESSOR_T5, mxt_get_object_address(), MXT_TWI_MSG_SIZE_T5, mxt_validate_message(), STATUS_OK, and twihs_master_read().

Referenced by mxt_process_messages(), and mxt_read_touch_event().

status_code_t mxt_read_touch_event ( struct mxt_device device,
struct mxt_touch_event touch_event 
)
void mxt_set_message_handler ( struct mxt_device device,
mxt_message_handler_t  handler 
)

Set message handler.

Parameters
*devicePointer to mxt_device instance
handlerMessage handler function

References mxt_device::handler.

status_code_t mxt_write_config_object ( struct mxt_device device,
mxt_memory_adr  memory_adr,
void *  obj_data 
)

Write object configuration.

Parameters
*devicePointer to mxt_device instance
memory_adrMemory address to the object
*obj_dataPointer to memory buffer containing object data
Returns
Operation result status code

References twihs_packet::addr, ERR_IO_ERROR, mxt_device::interface, mxt_device::mxt_chip_adr, mxt_get_object_size(), STATUS_OK, and twihs_master_write().

status_code_t mxt_write_config_reg ( struct mxt_device device,
mxt_memory_adr  memory_adr,
uint8_t  value 
)

Write object register.

Parameters
*devicePointer to mxt_device instance
memory_adrMemory address to register
valueValue to be written to register
Returns
Operation result status code

References twihs_packet::addr, ERR_IO_ERROR, mxt_device::interface, mxt_device::mxt_chip_adr, STATUS_OK, and twihs_master_write().