Driver for the TWIHS (High-Speed Two-Wire Interface).
This driver provides access to the main features of the TWIHS controller. The TWIHS interconnects components on a unique two-wire bus. The TWIHS is programmable as a master or a slave with sequential or single-byte access. Multiple master capability is supported. The High Speed of 3.4Mbits per second can be achieved in slave mode only.
Modules | |
Related Project(s) | |
In this section you can find all the projects related to the High-Speed Two-Wire Interface (TWIHS). | |
Macros | |
#define | I2C_FAST_MODE_SPEED 400000 |
#define | LOW_LEVEL_TIME_LIMIT 384000 |
#define | TWIHS_CLK_CALC_ARGU 3 |
#define | TWIHS_CLK_DIV_MAX 0xFF |
#define | TWIHS_CLK_DIV_MIN 7 |
#define | TWIHS_CLK_DIVIDER 2 |
Functions | |
void | twihs_disable_interrupt (Twihs *p_twihs, uint32_t ul_sources) |
Disable TWIHS interrupts. More... | |
void | twihs_disable_master_mode (Twihs *p_twihs) |
Disable TWIHS master mode. More... | |
void | twihs_disable_slave_mode (Twihs *p_twihs) |
Disable TWIHS slave mode. More... | |
void | twihs_enable_interrupt (Twihs *p_twihs, uint32_t ul_sources) |
Enable TWIHS interrupts. More... | |
void | twihs_enable_master_mode (Twihs *p_twihs) |
Enable TWIHS master mode. More... | |
void | twihs_enable_slave_mode (Twihs *p_twihs) |
Enable TWIHS slave mode. More... | |
uint32_t | twihs_get_interrupt_mask (Twihs *p_twihs) |
Read TWIHS interrupt mask. More... | |
uint32_t | twihs_get_interrupt_status (Twihs *p_twihs) |
Get TWIHS interrupt status. More... | |
Pdc * | twihs_get_pdc_base (Twihs *p_twihs) |
Get TWIHS PDC base address. More... | |
void | twihs_mask_slave_addr (Twihs *p_twihs, uint32_t ul_mask) |
A mask can be applied on the slave device address in slave mode in order to allow multiple address answer. More... | |
uint32_t | twihs_master_init (Twihs *p_twihs, const twihs_options_t *p_opt) |
Initialize TWIHS master mode. More... | |
uint32_t | twihs_master_read (Twihs *p_twihs, twihs_packet_t *p_packet) |
Read multiple bytes from a TWIHS compatible slave device. More... | |
uint32_t | twihs_master_write (Twihs *p_twihs, twihs_packet_t *p_packet) |
Write multiple bytes to a TWIHS compatible slave device. More... | |
static uint32_t | twihs_mk_addr (const uint8_t *addr, int len) |
Construct the TWIHS module address register field. More... | |
uint32_t | twihs_probe (Twihs *p_twihs, uint8_t uc_slave_addr) |
Test if a chip answers a given I2C address. More... | |
uint8_t | twihs_read_byte (Twihs *p_twihs) |
Reads a byte from the TWIHS bus. More... | |
void | twihs_read_write_protection_status (Twihs *p_twihs, uint32_t *p_status) |
Read the write protection status. More... | |
void | twihs_reset (Twihs *p_twihs) |
Reset TWIHS. More... | |
void | twihs_set_alternative_command (Twihs *p_twihs, uint32_t ul_alt_cmd) |
Set length/direction/PEC for alternative command mode. More... | |
void | twihs_set_filter (Twihs *p_twihs, uint32_t ul_filter) |
Set the filter for TWIHS. More... | |
void | twihs_set_slave_addr (Twihs *p_twihs, uint32_t ul_device_addr) |
Set TWIHS slave address. More... | |
uint32_t | twihs_set_speed (Twihs *p_twihs, uint32_t ul_speed, uint32_t ul_mck) |
Set the I2C bus speed in conjunction with the clock frequency. More... | |
void | twihs_set_write_protection (Twihs *p_twihs, bool flag) |
Enables/Disables write protection mode. More... | |
void | twihs_slave_init (Twihs *p_twihs, uint32_t ul_device_addr) |
Initialize TWIHS slave mode. More... | |
uint32_t | twihs_slave_read (Twihs *p_twihs, uint8_t *p_data) |
Read data from master. More... | |
uint32_t | twihs_slave_write (Twihs *p_twihs, uint8_t *p_data) |
Write data to TWIHS bus. More... | |
void | twihs_smbus_set_timing (Twihs *p_twihs, uint32_t ul_timing) |
Set the prescaler, TLOW:SEXT, TLOW:MEXT and clock high max cycles for SMBUS mode. More... | |
void | twihs_write_byte (Twihs *p_twihs, uint8_t uc_byte) |
Sends a byte of data to one of the TWIHS slaves on the bus. More... | |
#define I2C_FAST_MODE_SPEED 400000 |
Referenced by twihs_set_speed().
#define LOW_LEVEL_TIME_LIMIT 384000 |
Referenced by twihs_set_speed().
#define TWIHS_CLK_CALC_ARGU 3 |
Referenced by twihs_set_speed().
#define TWIHS_CLK_DIV_MAX 0xFF |
Referenced by twihs_set_speed().
#define TWIHS_CLK_DIV_MIN 7 |
Referenced by twihs_set_speed().
#define TWIHS_CLK_DIVIDER 2 |
Referenced by twihs_set_speed().
void twihs_disable_interrupt | ( | Twihs * | p_twihs, |
uint32_t | ul_sources | ||
) |
Disable TWIHS interrupts.
p_twihs | Pointer to a TWIHS instance. |
ul_sources | Interrupts to be disabled. |
Referenced by BOARD_TWIHS_Handler().
void twihs_disable_master_mode | ( | Twihs * | p_twihs | ) |
Disable TWIHS master mode.
p_twihs | Pointer to a TWIHS instance. |
void twihs_disable_slave_mode | ( | Twihs * | p_twihs | ) |
Disable TWIHS slave mode.
p_twihs | Pointer to a TWIHS instance. |
void twihs_enable_interrupt | ( | Twihs * | p_twihs, |
uint32_t | ul_sources | ||
) |
Enable TWIHS interrupts.
p_twihs | Pointer to a TWIHS instance. |
ul_sources | Interrupts to be enabled. |
Referenced by BOARD_TWIHS_Handler(), and main().
void twihs_enable_master_mode | ( | Twihs * | p_twihs | ) |
Enable TWIHS master mode.
p_twihs | Pointer to a TWIHS instance. |
Referenced by twihs_master_init().
void twihs_enable_slave_mode | ( | Twihs * | p_twihs | ) |
Enable TWIHS slave mode.
p_twihs | Pointer to a TWIHS instance. |
Referenced by twihs_slave_init().
uint32_t twihs_get_interrupt_mask | ( | Twihs * | p_twihs | ) |
Read TWIHS interrupt mask.
p_twihs | Pointer to a TWIHS instance. |
uint32_t twihs_get_interrupt_status | ( | Twihs * | p_twihs | ) |
Get TWIHS interrupt status.
p_twihs | Pointer to a TWIHS instance. |
TWIHS | interrupt status. |
Referenced by BOARD_TWIHS_Handler().
Pdc* twihs_get_pdc_base | ( | Twihs * | p_twihs | ) |
void twihs_mask_slave_addr | ( | Twihs * | p_twihs, |
uint32_t | ul_mask | ||
) |
A mask can be applied on the slave device address in slave mode in order to allow multiple address answer.
For each bit of the MASK field set to one the corresponding SADR bit will be masked.
p_twihs | Base address of the TWIHS instance. |
ul_mask | Mask value. |
uint32_t twihs_master_init | ( | Twihs * | p_twihs, |
const twihs_options_t * | p_opt | ||
) |
Initialize TWIHS master mode.
p_twihs | Pointer to a TWIHS instance. |
p_opt | Options for initializing the TWIHS module (see twihs_options_t). |
References FAIL, twihs_options::master_clk, twihs_options::speed, status, twihs_enable_master_mode(), TWIHS_INVALID_ARGUMENT, twihs_reset(), twihs_set_speed(), and TWIHS_SUCCESS.
Referenced by capture_init(), main(), and twihs_master_setup().
uint32_t twihs_master_read | ( | Twihs * | p_twihs, |
twihs_packet_t * | p_packet | ||
) |
Read multiple bytes from a TWIHS compatible slave device.
p_twihs | Pointer to a TWIHS instance. |
p_packet | Packet information and data (see twihs_packet_t). |
References twihs_packet::addr, twihs_packet::addr_length, buffer, twihs_packet::buffer, twihs_packet::chip, twihs_packet::length, status, TWIHS_ERROR_TIMEOUT, TWIHS_INVALID_ARGUMENT, twihs_mk_addr(), TWIHS_RECEIVE_NACK, TWIHS_SUCCESS, and TWIHS_TIMEOUT.
Referenced by at24macxx_read_byte(), at24macxx_read_continuous(), at24macxx_read_page(), main(), mxt_get_crc_value(), mxt_get_message_count(), mxt_probe_device(), mxt_read_config_object(), mxt_read_config_reg(), mxt_read_id_block(), mxt_read_message(), mxt_read_object_table(), ov_read_reg(), and wm8904_read_register().
uint32_t twihs_master_write | ( | Twihs * | p_twihs, |
twihs_packet_t * | p_packet | ||
) |
Write multiple bytes to a TWIHS compatible slave device.
p_twihs | Pointer to a TWIHS instance. |
p_packet | Packet information and data (see twihs_packet_t). |
References twihs_packet::addr, twihs_packet::addr_length, buffer, twihs_packet::buffer, twihs_packet::chip, twihs_packet::length, status, TWIHS_INVALID_ARGUMENT, twihs_mk_addr(), TWIHS_RECEIVE_NACK, and TWIHS_SUCCESS.
Referenced by at24macxx_acknowledge_polling(), at24macxx_write_byte(), at24macxx_write_page(), main(), mxt_write_config_object(), mxt_write_config_reg(), ov_write_reg(), twihs_probe(), and wm8904_write_register().
|
static |
Construct the TWIHS module address register field.
The TWIHS module address register is sent out MSB first. And the size controls which byte is the MSB to start with.
Please see the device datasheet for details on this.
Referenced by twihs_master_read(), and twihs_master_write().
uint32_t twihs_probe | ( | Twihs * | p_twihs, |
uint8_t | uc_slave_addr | ||
) |
Test if a chip answers a given I2C address.
p_twihs | Pointer to a TWIHS instance. |
uc_slave_addr | Address of the remote chip to search for. |
References twihs_packet::addr, twihs_packet::addr_length, twihs_packet::buffer, twihs_packet::chip, twihs_packet::length, and twihs_master_write().
uint8_t twihs_read_byte | ( | Twihs * | p_twihs | ) |
Reads a byte from the TWIHS bus.
p_twihs | Pointer to a TWIHS instance. |
Referenced by BOARD_TWIHS_Handler(), and main().
void twihs_read_write_protection_status | ( | Twihs * | p_twihs, |
uint32_t * | p_status | ||
) |
Read the write protection status.
p_twihs | Pointer to a TWIHS instance. |
p_status | Pointer to save the status. |
void twihs_reset | ( | Twihs * | p_twihs | ) |
Reset TWIHS.
p_twihs | Pointer to a TWIHS instance. |
Referenced by twihs_master_init(), and twihs_slave_init().
void twihs_set_alternative_command | ( | Twihs * | p_twihs, |
uint32_t | ul_alt_cmd | ||
) |
Set length/direction/PEC for alternative command mode.
p_twihs | Base address of the TWIHS instance. |
ul_alt_cmd | Alternative command parameters. |
void twihs_set_filter | ( | Twihs * | p_twihs, |
uint32_t | ul_filter | ||
) |
Set the filter for TWIHS.
p_twihs | Base address of the TWIHS instance. |
ul_filter | Filter value. |
void twihs_set_slave_addr | ( | Twihs * | p_twihs, |
uint32_t | ul_device_addr | ||
) |
Set TWIHS slave address.
p_twihs | Pointer to a TWIHS instance. |
ul_device_addr | Device address of the SAM slave device on the I2C bus. |
uint32_t twihs_set_speed | ( | Twihs * | p_twihs, |
uint32_t | ul_speed, | ||
uint32_t | ul_mck | ||
) |
Set the I2C bus speed in conjunction with the clock frequency.
p_twihs | Pointer to a TWIHS instance. |
ul_speed | The desired I2C bus speed (in Hz). |
ul_mck | Main clock of the device (in Hz). |
PASS | New speed setting is accepted. |
FAIL | New speed setting is rejected. |
References FAIL, I2C_FAST_MODE_SPEED, LOW_LEVEL_TIME_LIMIT, PASS, TWIHS_CLK_CALC_ARGU, TWIHS_CLK_DIV_MAX, TWIHS_CLK_DIV_MIN, and TWIHS_CLK_DIVIDER.
Referenced by twihs_master_init().
void twihs_set_write_protection | ( | Twihs * | p_twihs, |
bool | flag | ||
) |
Enables/Disables write protection mode.
p_twihs | Pointer to a TWIHS instance. |
flag | ture for enable, false for disable. |
void twihs_slave_init | ( | Twihs * | p_twihs, |
uint32_t | ul_device_addr | ||
) |
Initialize TWIHS slave mode.
p_twihs | Pointer to a TWIHS instance. |
ul_device_addr | Device address of the SAM slave device on the I2C bus. |
References twihs_enable_slave_mode(), and twihs_reset().
Referenced by main(), and twihs_slave_setup().
uint32_t twihs_slave_read | ( | Twihs * | p_twihs, |
uint8_t * | p_data | ||
) |
Read data from master.
p_twihs | Pointer to a TWIHS instance. |
p_data | Pointer to the data buffer where data received will be stored. |
References status.
uint32_t twihs_slave_write | ( | Twihs * | p_twihs, |
uint8_t * | p_data | ||
) |
Write data to TWIHS bus.
p_twihs | Pointer to a TWIHS instance. |
p_data | Pointer to the data buffer to be sent. |
References status.
void twihs_smbus_set_timing | ( | Twihs * | p_twihs, |
uint32_t | ul_timing | ||
) |
Set the prescaler, TLOW:SEXT, TLOW:MEXT and clock high max cycles for SMBUS mode.
p_twihs | Base address of the TWIHS instance. |
ul_timing | Parameter for prescaler, TLOW:SEXT, TLOW:MEXT and clock high max cycles. |
void twihs_write_byte | ( | Twihs * | p_twihs, |
uint8_t | uc_byte | ||
) |
Sends a byte of data to one of the TWIHS slaves on the bus.
p_twihs | Pointer to a TWIHS instance. |
byte | The byte to send. |
Referenced by BOARD_TWIHS_Handler().