Microchip® Advanced Software Framework

ip.c File Reference

This is the IPv4 layer implementation for incoming and outgoing IP traffic.

See Also
ip_frag.c
#include "lwip/opt.h"
#include "lwip/ip.h"
#include "lwip/def.h"
#include "lwip/mem.h"
#include "lwip/ip_frag.h"
#include "lwip/inet_chksum.h"
#include "lwip/netif.h"
#include "lwip/icmp.h"
#include "lwip/igmp.h"
#include "lwip/raw.h"
#include "lwip/udp.h"
#include "lwip/tcp_impl.h"
#include "lwip/snmp.h"
#include "lwip/dhcp.h"
#include "lwip/autoip.h"
#include "lwip/stats.h"
#include "arch/perf.h"
#include <string.h>

Macros

#define CHECKSUM_GEN_IP_INLINE   1
 
#define IP_ACCEPT_LINK_LAYER_ADDRESSED_PORT(port)   ((port) == PP_NTOHS(DHCP_CLIENT_PORT))
 Some defines for DHCP to let link-layer-addressed packets through while the netif is down. More...
 
#define IP_ACCEPT_LINK_LAYER_ADDRESSING   1
 
#define LWIP_INLINE_IP_CHKSUM   1
 Set this to 0 in the rare case of wanting to call an extra function to generate the IP checksum (in contrast to calculating it on-the-fly). More...
 

Functions

err_t ip_input (struct pbuf *p, struct netif *inp)
 This function is called by the network interface device driver when an IP packet is received. More...
 
err_t ip_output (struct pbuf *p, ip_addr_t *src, ip_addr_t *dest, u8_t ttl, u8_t tos, u8_t proto)
 Simple interface to ip_output_if. More...
 
err_t ip_output_if (struct pbuf *p, ip_addr_t *src, ip_addr_t *dest, u8_t ttl, u8_t tos, u8_t proto, struct netif *netif)
 Sends an IP packet on a network interface. More...
 
struct netifip_route (ip_addr_t *dest)
 Finds the appropriate network interface for a given IP address. More...
 

Variables

struct ip_hdrcurrent_header
 Header of the input packet currently being processed. More...
 
ip_addr_t current_iphdr_dest
 Destination IP address of current_header. More...
 
ip_addr_t current_iphdr_src
 Source IP address of current_header. More...
 
struct netifcurrent_netif
 The interface that provided the packet for the current callback invocation. More...
 
static u16_t ip_id
 The IP header ID of the next outgoing IP packet. More...
 

#define CHECKSUM_GEN_IP_INLINE   1
#define IP_ACCEPT_LINK_LAYER_ADDRESSED_PORT (   port)    ((port) == PP_NTOHS(DHCP_CLIENT_PORT))

Some defines for DHCP to let link-layer-addressed packets through while the netif is down.

To use this in your own application/protocol, define LWIP_IP_ACCEPT_UDP_PORT to return 1 if the port is accepted and 0 if the port is not accepted.

Referenced by ip_input().

#define IP_ACCEPT_LINK_LAYER_ADDRESSING   1
#define LWIP_INLINE_IP_CHKSUM   1

Set this to 0 in the rare case of wanting to call an extra function to generate the IP checksum (in contrast to calculating it on-the-fly).

err_t ip_input ( struct pbuf p,
struct netif inp 
)

This function is called by the network interface device driver when an IP packet is received.

The function does the basic checks of the IP header such as packet size being at least larger than the header size etc. If the packet was not destined for us, the packet is forwarded (using ip_forward). The IP checksum is always checked.

Finally, the packet is sent to the upper layer protocol input function.

Parameters
pthe received IP packet (p->payload points to IP header)
inpthe netif on which this packet was received
Returns
ERR_OK if the packet was processed (could return ERR_* if it wasn't processed, but currently always returns ERR_OK)

References current_iphdr_dest, current_iphdr_src, ERR_OK, netif::flags, icmp_dest_unreach(), ICMP_DUR_PROTO, icmp_input(), if(), inet_chksum(), ip4_addr_get_u32, IP_ACCEPT_LINK_LAYER_ADDRESSED_PORT, netif::ip_addr, ip_addr_cmp, ip_addr_copy, ip_addr_isany, ip_addr_isbroadcast, ip_addr_ismulticast, ip_addr_set_any, IP_DEBUG, ip_debug_print, IP_HLEN, IP_MF, IP_OFFMASK, IP_PROTO_ICMP, IP_PROTO_IGMP, IP_PROTO_TCP, IP_PROTO_UDP, IP_PROTO_UDPLITE, ip_reass(), IP_STATS_INC, IPH_HL, IPH_ID, IPH_LEN, IPH_OFFSET, IPH_PROTO, IPH_V, iphdr, pbuf::len, LWIP_DBG_LEVEL_SERIOUS, LWIP_DBG_LEVEL_WARNING, LWIP_DBG_TRACE, LWIP_DEBUGF, netif::name, NETIF_FLAG_IGMP, netif_is_up, netif_list, netif::netmask, netif::next, ntohs, NULL, pbuf::payload, pbuf_free(), pbuf_realloc(), PP_HTONS, snmp_inc_ipinaddrerrors, snmp_inc_ipindelivers, snmp_inc_ipindiscards, snmp_inc_ipinhdrerrors, snmp_inc_ipinreceives, snmp_inc_ipinunknownprotos, tcp_input(), pbuf::tot_len, udp_input(), X16_F, and X32_F.

Referenced by ethernet_input(), netif_init(), tcpip_input(), and tcpip_thread().

err_t ip_output ( struct pbuf p,
ip_addr_t src,
ip_addr_t dest,
u8_t  ttl,
u8_t  tos,
u8_t  proto 
)

Simple interface to ip_output_if.

It finds the outgoing network interface and calls upon ip_output_if to do the actual work.

Parameters
pthe packet to send (p->payload points to the data, e.g. next protocol header; if dest == IP_HDRINCL, p already includes an IP header and p->payload points to that IP header)
srcthe source IP address to send from (if src == IP_ADDR_ANY, the IP address of the netif used to send is used as source address)
destthe destination IP address to send the packet to
ttlthe TTL value to be set in the IP header
tosthe TOS value to be set in the IP header
protothe PROTOCOL to be set in the IP header
Returns
ERR_RTE if no route is found see ip_output_if() for more return values

References ERR_RTE, ip4_addr1_16, ip4_addr2_16, ip4_addr3_16, ip4_addr4_16, IP_DEBUG, ip_output_if(), ip_route(), IP_STATS_INC, LWIP_ASSERT, LWIP_DEBUGF, NULL, and pbuf::ref.

Referenced by icmp_send_response(), tcp_keepalive(), tcp_output_segment(), tcp_rst(), tcp_send_empty_ack(), and tcp_zero_window_probe().

err_t ip_output_if ( struct pbuf p,
ip_addr_t src,
ip_addr_t dest,
u8_t  ttl,
u8_t  tos,
u8_t  proto,
struct netif netif 
)

Sends an IP packet on a network interface.

This function constructs the IP header and calculates the IP header checksum. If the source IP address is NULL, the IP address of the outgoing network interface is filled in as source address. If the destination IP address is IP_HDRINCL, p is assumed to already include an IP header and p->payload points to it instead of the data.

Parameters
pthe packet to send (p->payload points to the data, e.g. next protocol header; if dest == IP_HDRINCL, p already includes an IP header and p->payload points to that IP header)
srcthe source IP address to send from (if src == IP_ADDR_ANY, the IP address of the netif used to send is used as source address)
destthe destination IP address to send the packet to
ttlthe TTL value to be set in the IP header
tosthe TOS value to be set in the IP header
protothe PROTOCOL to be set in the IP header
netifthe netif on which to send this packet
Returns
ERR_OK if the packet was sent OK ERR_BUF if p doesn't have enough space for IP/LINK headers returns errors returned by netif->output
Note
ip_id: RFC791 "some host may be able to simply use unique identifiers independent of destination"

References NULL.

Referenced by icmp_input(), and ip_output().

struct netif* ip_route ( ip_addr_t dest)

Finds the appropriate network interface for a given IP address.

It searches the list of network interfaces linearly. A match is found if the masked IP address of the network interface equals the masked IP address given to the function.

Parameters
destthe destination IP address for which to find the route
Returns
the netif on which to send to reach dest

References ip4_addr1_16, ip4_addr2_16, ip4_addr3_16, ip4_addr4_16, netif::ip_addr, ip_addr_netcmp, IP_DEBUG, IP_STATS_INC, LWIP_DBG_LEVEL_SERIOUS, LWIP_DEBUGF, netif_default, netif_is_up, netif_list, netif::netmask, netif::next, NULL, snmp_inc_ipoutnoroutes, and U16_F.

Referenced by etharp_update_arp_entry(), ip_output(), tcp_connect(), tcp_eff_send_mss(), tcp_output_segment(), and udp_connect().

struct ip_hdr* current_header

Header of the input packet currently being processed.

ip_addr_t current_iphdr_dest

Destination IP address of current_header.

Referenced by icmp_input(), ip_input(), tcp_input(), tcp_listen_input(), and udp_input().

ip_addr_t current_iphdr_src

Source IP address of current_header.

Referenced by ip_input(), tcp_input(), tcp_listen_input(), and udp_input().

struct netif* current_netif

The interface that provided the packet for the current callback invocation.

u16_t ip_id
static

The IP header ID of the next outgoing IP packet.